6. HEALTH & SAFETY FEATURES ON TOOLS
Just as more sustainable materials are being considered when designing new tools, so are a range of health and safety features to help protect and prevent workers from injuring themselves. Our Hilti Active Vibration Reduction (AVR) technology, for example, minimises exposure to tool vibration by up to two-thirds – lowering the risk of damage to nerves, tendons, muscles, bones and joints. There’s added productivity benefits too, as workers can use tools – such as the TE 1000-AVR concrete breaker – for a full 8-hour day before reaching HSE exposure limits. Similarly, our Hilti Active Torque Control (ATC) technology stops the tool body from spinning uncontrollably if the drill bit jams, making the tool much safer to use. As health and safety continues to be a top priority throughout the construction industry, there’s no doubt that these types of features will become the norm in 2022 and beyond.