Please note, the order volume has been updated. This is due to package and minimum order quantities.
Please note, the order volume has been updated to {0}. This is due to package and minimum order quantities.. This is due to package and minimum order quantities.
Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
Observe the safety instructions and warnings in this documentation and on the product.
Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
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
General symbol for "must do"
Wear eye protection
Wear hearing protection
Wear a hard hat
Direct current (DC)
The power tool supports near-field communication (NFC) technology, which is compatible with iOS and Android platforms.
Hilti Li-ion battery type series used. Observe the information given in the section headed Intended use .
Never use the battery as a striking tool.
Do not drop the battery. Never use a battery that has suffered an impact or is damaged in any other way.
If applied on the product, the product has been certified by this certification body for the US and Canadian markets according to the applicable standards.
Product information
products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
The type designation and serial number are printed on the rating plate.
Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product. Product information
Type:
BX 3-SCT
Generation:
02
Serial number:
Declaration of conformity
The manufacturer declares, on his sole responsibility, that the product described here complies with the applicable legislation and standards. A copy of the declaration of conformity can be found at the end of this documentation.
The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | D-86916 Kaufering, Germany
Safety
General power tool safety warnings
WARNING
Read all safety warnings and all instructions. Failure to follow the warnings and instructions may result in electric shock, fire and/or serious injury.
Save all warnings and instructions for future reference. Work area safety
Keep work area clean and well lit. Cluttered or dark areas invite accidents.
Do not operate power tools in explosive atmospheres, such as in the presence of flammable liquids, gases or dust. Power tools create sparks which may ignite the dust or fumes.
Keep children and bystanders away while operating a power tool. Distractions can cause you to lose control.
Electrical safety
Avoid body contact with earthed or grounded surfaces, such as pipes, radiators, ranges and refrigerators. There is an increased risk of electric shock if your body is earthed or grounded.
Do not expose power tools to rain or wet conditions. Water entering a power tool will increase the risk of electric shock.
Personal safety
Stay alert, watch what you are doing and use common sense when operating a power tool. Do not use a power tool while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating power tools may result in serious personal injury.
Use personal protective equipment. Always wear eye protection. Protective equipment such as dust mask, non-skid safety shoes, hard hat, or hearing protection used for appropriate conditions will reduce personal injuries.
Prevent unintentional starting. Ensure the switch is in the off‐position before connecting to battery pack, picking up or carrying the tool. Carrying power tools with your finger on the switch or energising power tools that have the switch on invites accidents.
Remove any adjusting key or wrench before turning the power tool on. A wrench or a key left attached to a rotating part of the power tool may result in personal injury.
Do not overreach. Keep proper footing and balance at all times. This enables better control of the power tool in unexpected situations.
Dress properly. Do not wear loose clothing or jewellery. Keep your hair, clothing and gloves away from moving parts. Loose clothes, jewellery or long hair can be caught in moving parts.
If devices are provided for the connection of dust extraction and collection facilities, ensure these are connected and properly used. Use of dust collection can reduce dust-related hazards.
Power tool use and care
Do not force the power tool. Use the correct power tool for your application. The correct power tool will do the job better and safer at the rate for which it was designed.
Do not use the power tool if the switch does not turn it on and off. Any power tool that cannot be controlled with the switch is dangerous and must be repaired.
Disconnect the battery pack from the power tool before making any adjustments, changing accessories, or storing power tools. Such preventive safety measures reduce the risk of starting the power tool accidentally.
Store idle power tools out of the reach of children and do not allow persons unfamiliar with the power tool or these instructions to operate the power tool. Power tools are dangerous in the hands of untrained users.
Maintain power tools. Check for misalignment or binding of moving parts, breakage of parts and any other condition that may affect the power tool’s operation. If damaged, have the power tool repaired before use. Many accidents are caused by poorly maintained power tools.
Keep cutting tools sharp and clean. Properly maintained cutting tools with sharp cutting edges are less likely to bind and are easier to control.
Use the power tool, accessories and tool bits etc. in accordance with these instructions, taking into account the working conditions and the work to be performed. Use of the power tool for operations different from those intended could result in a hazardous situation.
Battery tool use and care
Recharge only with the charger specified by the manufacturer. A charger that is suitable for one type of battery pack may create a risk of fire when used with another battery pack.
Use power tools only with specifically designated battery packs. Use of any other battery packs may create a risk of injury and fire.
When battery pack is not in use, keep it away from other metal objects, like paper clips, coins, keys, nails, screws or other small metal objects, that can make a connection from one terminal to another. Shorting the battery terminals together may cause burns or a fire.
Under abusive conditions, liquid may be ejected from the battery; avoid contact. If contact accidentally occurs, flush with water. If liquid contacts eyes, additionally seek medical help. Liquid ejected from the battery may cause irritation or burns.
Service
Have your power tool serviced by a qualified repair person using only identical replacement parts. This will ensure that the safety of the power tool is maintained.
Tacker safety warnings
Always assume that the tool contains fasteners. Careless handling of the tacker can result in unexpected firing of fasteners and personal injury.
Do not point the tool towards yourself or anyone nearby. Unexpected triggering will discharge the fastener causing an injury.
Do not actuate the tool unless the tool is placed firmly against the workpiece. If the tool is not in contact with the workpiece, the fastener may be deflected away from your target.
Disconnect the tool from the power source when the fastener jams in the tool. While removing a jammed fastener, the tacker may be accidentally activated if it is plugged in.
Use caution while removing a jammed fastener. The mechanism may be under compression and the fastener may be forcefully discharged while attempting to free a jammed condition.
When fastening electrical cables, make sure the cables are not energized. Hold the tacker only by insulated gripping surfaces. Use only fasteners designed for electrical cable installations. Inspect that the fastener has not damaged the insulation of the electrical cables. A fastener that damages the insulation of electric cables can lead to electric shock and fire hazards.
Safety instructions
Basic information concerning safetyWARNING!Read all safety precautions and other instructions. Failure to observe the safety precautions and other instructions may result in electric shock, fire and/or serious injury.
Keep all safety precautions and instructions for future reference.
Requirements to be met by users
Only authorized, appropriately trained persons may operate or service this tool.
Personal protective equipment
You and all other persons in the vicinity must wear suitable eye protection and a hard hat while the tool is in use.
Wear hearing protection.
Exposure to noise can cause hearing loss.
Personal safety
Observe the information printed in the operating instructions concerning operation, care and maintenance.
Stay alert, watch what you are doing and use common sense when operating a direct fastening tool. Do not use the tool when you are tired or under the influence of drugs, alcohol or medication. Take a break if you experience pain or feel unwell. A moment of inattention while operating tools may result in serious personal injury.
Avoid awkward postures. Make sure you work from a safe stance and stay in balance at all times.
Take breaks between working and do relaxation and finger exercises to improve the blood circulation in your fingers.
Wear non-skid shoes.
Keep the arms slightly bent while operating the tool (do not straighten the arms).
Keep other people away from the working area, especially children.
Risk of injury by falling tools and/or accessories. Before starting work, check that installed accessories are secure.
Use and care of direct fastening toolsWARNING!Danger of fastener penetrating right through! Before driving fasteners, check to make sure that no one is present behind or below the object into which the fastener is to be driven.
Use the right tool for the work you are carrying out. Do not use the tool for purposes for which it was not intended. Use it only as directed and when in faultless condition.
Never leave a loaded tool unattended.
Transport and store the tool in a secured toolbox.
Always switch the tool off before cleaning, maintenance, changing the fastener guide, before work breaks and before storing the tool.
When not in use, the tool should be unloaded and stored in a locked, dry place where it is inaccessible to children.
Check the tool and the accessories for any damage. Check that moving parts function faultlessly, without sticking, and that no parts are damaged.
All parts must be fitted correctly and fulfill all conditions necessary for correct operation of the tool. Damaged parts must be properly repaired or replaced by Hilti Service unless otherwise stated in the operating instructions.
Before beginning work, check the working area (e.g. using a metal detector) to ensure that no concealed electric cables or gas and water pipes are present. External metal parts of the power tool may become live, for example, when an electric cable is damaged accidentally.
Do not attempt to drive fasteners into unsuitable materials.
Unsuitable materials are glass, marble, plastic, bronze, brass, copper, insulating material, hollow brick, ceramic brick, thin sheet metal (< 4 mm) and cellular concrete. Driving a fastener into these materials may cause the fastener to break, splinter the material or to be driven right through.
Pull the trigger only when the tool is fully pressed against the working surface at right angles.
When driving fasteners, always hold the fastening tool at right angles to the working surface in order to prevent the fastener being deflected by the surface.
Keep the grips dry, clean and free from oil and grease.
Never drop the tool.
Do not use the tool in places where there is a risk of fire or explosion unless the tool is specially approved for this type of use.
Workplace
Keep the workplace tidy. Clear the work zone of objects that could cause injury.
Untidiness in the working area can lead to accidents.
Make sure that the working area is well lit and well ventilated.
Mechanical safety rules
Do not tamper with or modify the tool or parts of it, especially the piston.
Use only fasteners of a type approved for use with the tool.
Thermal safety rules
Do not exceed the recommended maximum fastener driving rate (see the section headed "Technical data").
If the tool has overheated, allow it to cool down.
Do not dismantle the tool while it is hot. Allow the tool to cool down.
Careful handling and use of batteries
Observe the special guidelines applicable to the transport, storage and use of lithium-ion batteries.
Do not expose batteries to high temperatures, direct sunlight or fire.
Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C (176 °F).
Do not use or charge batteries that have suffered mechanical impact, have been dropped from a height or show signs of damage. In this case, always contact your HiltiService .
If the battery is too hot to touch it may be defective. Put the battery in a place where it is clearly visible and where there is no risk of fire, at an adequate distance from flammable materials. Allow the battery to cool down. If it is still too hot to touch after an hour, the battery is faulty. Contact HiltiService .
Description
Product overview
Fastener guide
Fastener guide locking catch
Air vents
Belt hook
Trigger
Grip
Release buttons (also used to activate the charge status indicator)
Li‑ion battery
Status indicator
On/off button
Intended use
The product is a hand-held, cordless fastening tool. It is designed for driving fasteners into concrete. Use only approved fasteners in combination with the corresponding fastener guide.
CAUTION
Incorrect estimate of concrete strength Use of the wrong fastener guide or the wrong fastener can lead to poor-quality driving of the fastener and subsequently to misjudgment of concrete strength.
Always use the correct fastener guide!
Always use the right fastener!
The fastening tool, battery and fasteners together form a technical entity. Use the
Hilti fasteners specially manufactured for the tool and the batteries and chargers recommended by
Hilti . The fastening and application recommendations made by
Hilti apply only when these conditions are observed.
The fastening tool is for hand-held use only.
Misuse must be ruled out. Misuse includes triggering without a fastener inserted in the fastener guide.
Use only Hilti lithium‑ion batteries of the B 22 series with this product.
Use only Hilti -approved battery chargers to charge these batteries. More information is available from your Hilti Store or from www.hilti.group
Status indicator
The status indicator provides information about the status of the fastening tool.
Status
Meaning
Off
The fastening tool is switched off
The LED shows green.
The fastening tool is switched on and ready for use
The LED flashes green every 3 seconds.
The fastening tool is in stand-by mode. Press the nose of the tool against the working surface to switch it on
The LED flashes steadily green.
The fastening tool is too hot or the battery has insufficient power; see “Troubleshooting”
The LED flashes red.
Malfunction; see “Troubleshooting”
The LED shows red.
Malfunction; see “Troubleshooting”
The LED flashes yellow.
Bring the fastening tool to Hilti Service.
Indication of battery charge status
When one of the battery release buttons is pressed, the display indicates the battery’s state of charge.
Reliable indication of the charge status is not possible while a fastener is being driven or immediately after a fastener is driven.
Status
Meaning
All four LEDs show green.
Charge status is 75 % to 100 %.
Three LEDs show green.
Charge status is 50 % to 75 %.
Two LEDs show green.
Charge status is 25 % to 50 %.
One LED shows green.
Charge status is 10 % to 25 %.
One LED flashes green.
Charge status is below 10 %.
Items supplied
BX 3-SCT fastening tool, operating instructions.
Other system products approved for use with this product can be found at your local
Hilti Store or at:
www.hilti.group
Technical data
Fastening tool
Weight in accordance with EPTA Procedure 01 including battery B22⁄2.6
4.0 kg
Fastener guide
X‑FG B3‑SCT 02
Fasteners
X‑M6‑8‑52 DP7 SCT B3
X‑M6‑8‑62 DP7 SCT B3
X‑M6‑8‑87 DP7 SCT B3
Length, fastener
52 mm / 62 mm / 87 mm
Fastener diameter
6 mm
Compression stroke
12 mm
Contact pressure
50 N …70 N
Application temperature (ambient temperature)
−15 ℃ …50 ℃
Application temperature, fastener
−10 ℃ …50 ℃
Recommended maximum driving rate
650/h
Rated voltage
21.6 V
Frequency
2,400 MHz …2,483.5 MHz
Maximum emitted transmission power
−11.9 dBm
Battery
Battery operating voltage
21.6 V
Ambient temperature for operation
−17 ℃ …60 ℃
Storage temperature
−20 ℃ …40 ℃
Battery charging starting temperature
−10 ℃ …45 ℃
Noise information and vibration values
The sound pressure and vibration values given in these instructions have been measured in accordance with a standardized test and may be used to compare one power tool with another. They may be used for a preliminary assessment of exposure. The data given represents the main applications of the power tool. However, if the power tool is used for different applications, with different accessories or is poorly maintained, the data may vary. This may significantly increase exposure over the total working period. An accurate estimation of exposure should also take into account the times when the tool is switched off, or when it is running but not actually being used for a job. This may significantly reduce exposure over the total working period. Set out additional safety measures to protect the operator from the effects of noise and/or vibration, such as: Maintaining the power tool and accessories, keeping the hands warm, reorganization of work patterns.
Noise and vibration information (measured in accordance with EN 60745-2‑16)
Typical A-weighted sound power level, LWA (driving studs into concrete)
Slide the fastener guide locking catch as far as it will go in the direction of the arrow.
The fastener guide will be released.
Remove the fastener guide.
Inserting the fastener guide
Switch off the fastening tool.
Remove the battery.
Slide the fastener guide locking catch as far as it will go in the direction of the arrow and hold it in this position.
Slide the fastener guide into the nosepiece until it engages with an audible click.
Release the fastener guide locking catch.
The fastener guide jumps to the middle position.
Grip and pull the fastener guide to check that it is securely seated.
Fall arrest
WARNING
Risk of injury by falling tool and/or accessory!
Use only the Hilti tool tether recommended for your product.
Prior to each use, always check the attachment point of the tool tether for possible damage.
Do not secure a tool tether to the belt hook. Do not use a belt hook to lift the product.
Comply with the national regulations for working at heights.
As drop arrester for this product, use only the
Hilti tool tether #2261971.
Use the loop to secure the tool tether to the product as shown in the illustration. Check that it holds securely.
Secure the carabiner to a load-bearing structure. Check that the carabiner holds securely.
Comply with the operating instructions of the
Hilti tool tether.
Operation
Switching on the fastening tool
WARNING
Risk of injury! Pressing the nosepiece of the fastening tool against a part of the body may lead to serious injury due to inadvertent firing and release of a fastener.
Never press the nosepiece of the fastening tool against your hand or any other part of the body.
WARNING
Risk of injury! Under certain circumstances, pulling the fastener guide back by hand could make the tool ready to fire. When the tool is ready to fire, fasteners or the piston could be driven inadvertently into parts of the body.
Never attempt to pull the fastener guide back by hand.
Press the on/off button.
The spring mechanism audibly builds up tension and the status indicator shows green.
Battery performance drops at low temperatures.
When battery performance drops, tensioning of the spring mechanism takes longer than with a fully charged battery.
If you continue to operate the fastening tool after battery performance drops, the fastening tool will switch itself off automatically before damage to the battery cells occurs.
Switching off the fastening tool
Press the on/off button.
The spring mechanism audibly relieves its tension and the status indicator goes out.
Driving a fastener
WARNING
Risk of injury byincorrect handling and/or splintering material!
Risk of driving a nail through your hand! Always use both hands to operate the product! Always hold the product firmly with your second hand as illustrated.
Never press the nosepiece of the fastening tool against your hand or any other part of the body! By unintentionally triggering a driving operation, this can cause severe injury.
Wear personal protective equipment and always wear protective glasses and protective gloves. Other persons in the vicinity must also wear eye protection and a hard hat. When fasteners are being driven, there is a risk of injury to the body and eyes caused by material splintering off the working surface and also if there are foreign bodies in the area of the fastener guide.
Never attempt to clear malfunctions of the tool by continuing to trigger the tool!
CAUTION
Risk of injuryand damage to the fastening tool!
Never attempt to re-drive the fastener! This can lead to fastener breakages and jamming of the fastener.
Use only approved, genuine Hilti accessories with this tool. The use of unsuitable material and accessories can lead to injuries and damage the fastening tool.
Hold the fastening tool perpendicular to the working surface and press it against the surface, pushing the fastener guide in as far as it will go.
Drive the fastener by pulling the trigger.
After driving each fastener, use the test gauge to check that the stud has been driven to the correct preset depth.
Lift the fastening tool completely clear of the working surface after driving a fastener.
The fastening tool switches itself off automatically if the fastener guide is pressed against the working surface for longer than 6 seconds without a fastener being driven. The fastening tool can be switched on again by pressing the on/off button. Never attempt to re-drive the fastener!
The fastening tool switches itself off automatically if it is not used for 6 minutes.
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
Switch off the fastening tool.
Remove the battery.
Remove the fastener from the fastener guide.
Carefully remove any dirt that may be adhering to parts.
Clean the air vents carefully with a dry brush.
Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
Care of the lithium‑ion batteries
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
To help ensure safe and reliable operation, use only genuine Hilti spare parts and consumables. Spare parts, consumables and accessories approved by Hilti for use with the product can be found at your local
Hilti Store or online at:
www.hilti.group .
Transport and storage of cordless tools
Transport
Switch off the fastening tool.
CAUTION
Accidental starting during transport !
Always transport your products with the batteries removed!
Remove the battery.
Remove the fastener from the fastener guide.
Never transport batteries in bulk form (loose, unprotected).
Check the tool and batteries for damage before use after long periods of transport.
Storage
WARNING
Accidental damage caused by defective or leaking batteries !
Always store your products with the batteries removed!
Store the tool and batteries in a place that is as cool and dry as possible.
Never leave batteries in direct sunlight, near sources of heat or behind glass.
Store the tool and batteries in a place where they cannot be accessed by children or unauthorized persons.
Check the tool and batteries for damage before use after long periods of storage.
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
The spring element is not tensioned; no status indication.
Too much contact pressure applied through the grip to the fastening tool.
Apply less pressure to press the fastening tool against the surface.
Fastening tool was angled off the driving axis when pressed against the surface.
Press the fastening tool at right angles against the surface, applying pressure to the grip surface on the back of the fastening tool.
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
Dispose of the battery at your Hilti Store , or consult your local governmental garbage disposal or public health and safety resources for disposal instructions.
Most of the materials from which
Hilti products are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to
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
For more information on operation, technology, environment and recycling, follow this link:
qr.hilti.com/manual/?id=2338836&id=2338838 This link is also to be found at the end of the documentation, in the form of a QR code.