Please note, the order volume has been updated. This is due to package and minimum order quantities.
Please note, the order volume has been updated to {0}. This is due to package and minimum order quantities.. This is due to package and minimum order quantities.
Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
Observe the safety instructions and warnings in this documentation and on the product.
Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
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
The device supports near-field communication (NFC) technology, which is compatible with Android platforms.
Hilti Li-ion battery type series used. Observe the information given in the section headed Intended use .
Li-ion battery
Battery state of charge indicator
On/off button
Never use the battery as a striking tool.
Do not drop the battery. Never use a battery that has suffered an impact or is damaged in any other way.
Sticker on the product
Laser information
Laser class 2, based on the IEC/EN 60825-1:2014 standard and corresponding to CFR 21 Sec. 1040. Do not look straight into the laser beam.
Product information
products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
The type designation and serial number are printed on the rating plate.
Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product. Product information
Layout tool
PMD 200
Generation
01
Serial no.
Safety
General safety rules
WARNING!Read all safety precautions and other instructions. Failure to observe the safety instructions and other instructions can result in electric shock, fire and/or serious injury.
Keep all safety precautions and instructions for future reference.
Personal safety
Stay alert, watch what you are doing and use common sense when operating a measuring tool. Do not use a measuring tool while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating the measuring tool can result in serious injuries.
Do not allow yourself to be lulled into a false sense of security and do not flout the safety rules for tools, even if you are familiar with the tool after using it many times. Carelessness can result in serious injury within a fraction of a second.
Keep children and other persons away from the working area.
Electrical safety
Do not expose the product to rain or moisture. Water entering an electric device increases the risk of electric shock.
Using and handling the measuring tool
Due to the principle employed, the results of measurements may be negatively affected by the surrounding conditions. This includes, for example, close proximity to products that generate powerful magnetic or electromagnetic fields, taking measurements from unsuitable surfaces and the use of unsuitable reflectors.
When the product is brought into a warm environment from very cold conditions, or vice-versa, allow it to become acclimatized before use.
Check the accuracy of the product if it has been dropped or subjected to other mechanical stresses.
Do not use the product for purposes for which it was not intended. Use it only as directed and when in faultless condition.
Using and handling the cordless power tool
Use only the specified batteries in the measuring tools. Use of other batteries can result in injury and a risk of fire.
Recharge only with the charger specified by the manufacturer. A charger that is suitable for a certain type of battery may present a risk of fire when used with other types of battery.
Paper clips, coins, keys, nails, screws and other small metal objects that could short-circuit the electrical contacts must be kept away from batteries that are not in use and away from battery chargers. Short-circuiting the contacts on a battery or charger can cause burn injuries or start a fire.
Under abusive conditions, liquid may be ejected from the battery. Avoid contact with the liquid. Liquid leaking from the battery may cause skin irritation or burns.
Disconnect the plug from the power source and/or remove the battery before making any adjustments, changing accessories, or storing the appliance. This precaution reduces the risk of the power tool starting accidentally.
Remove the battery before storing or transporting the product. Store the product in a dry place where it cannot be accessed by children or unauthorized persons.
Product-specific safety instructions
Using and handling the measuring tool
Rapidly changing measuring conditions can falsify the result of measurement.
Keep the product clean and dry at all times.
Always check the device settings before using it.
Use the product only within its specified limits.
Additional safety instructions
Work area safety
Keep the work area clean and uncluttered and watch out for supply cords routed in the work area. Carelessly routed supply cords can constitute trip hazards and lead to injuries. Measuring tools mounted on tripods can topple and be damaged if a supply cord is accidentally pulled. Make sure you are aware of everything that is happening around you when you change position while using the remote control unit.
Personal safety
The product complies with Laser Class 2 in accordance with IEC/EN 60825-1:2014 in accordance with CFR 21 Sec. 1040 (FDA). This product may be used without need for further protective measures. Nevertheless, as with the sun, do not look directly into the light source. If you do inadvertently look into the laser beam, immediately close your eyes and move your head clear of the laser beam. Do not aim the laser beam at persons.
If the product falls from an elevated position there is a risk of injury to persons. Use only tripods recommended by Hilti .
Wear your personal protective equipment and always wear protective glasses. Depending on the type of product you are using and its purpose, wearing personal protective equipment such as a dust mask, non-slip safety shoes, hard hat, or hearing protection reduces the risk of injury.
Using and handling the measuring tool
Maintain the measuring tool carefully. Check that moving parts are in full working order and do not jam and make sure there are no parts that are broken or damaged in such a way as to impair operation of the measuring tool. Have damaged parts repaired before using the tool. Poor maintenance of measuring tools is the cause of many accidents.
Make sure that the scanning tool is standing firmly on all three of its rests or is correctly secured to the tripod recommended by Hilti .
To avoid inaccuracies, always make sure that the target plate is always perfectly plumb when points are marked. Use the adjusting screw and the bubble level for adjusting and checking.
Never use a damaged target plate. Risk of inaccurate measurement.
Check the accuracy of the product before use and several times during use.
Although the measuring tool complies with the strict requirements of the applicable directives, Hilti cannot entirely rule out the possibility of interference caused by powerful electromagnetic radiation, possibly leading to incorrect operation.
Battery use and care
Observe the special guidelines applicable to the transport, storage and use of Li-ion batteries.
Do not expose batteries to high temperatures, direct sunlight or fire.
Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C.
Do not use or charge batteries that have suffered mechanical impact, have been dropped from a height or show signs of damage. In this case, always contact your HiltiService .
If the battery is too hot to touch it may be defective. Put the battery in a place where it is clearly visible and where there is no risk of fire, at an adequate distance from flammable materials. Allow the battery to cool down. If it is still too hot to touch after an hour, the battery is faulty. Contact HiltiService .
Description
Product overview (PMD 200 layout tool)
Battery
Grip
Laser exit window
On/off button
Product overview (PMDA 200 target plate)
Grip
Bubble level
Adjusting screw
Target plate
Intended use
The product described is a layout tool that is controlled with the PMD 200 application pre-installed on the tablet (PMC 200 ). It is designed to enable the operator to transfer points from the drawing to the jobsite without the assistance of a second person. The layout tool has a green (vertical) laser line and a built-in laser range-finder module (red dot).
Documentation of the tablet (PMC 200 ): See the supplier's documentation (enclosed).
With this product, use only the Hilti Li‑ion batteries of the B 12 series stated at the end of this document.
Use only Hilti -approved battery chargers to charge these batteries. More information is available from your Hilti Store or from: www.hilti.group
Bluetooth®
This layout tool has Bluetooth.
Bluetooth is a wireless data transfer protocol with which two Bluetooth-enabled devices can communicate with each other over a certain distance. The layout tool pairs with the tablet by means of the pre-installed
PMD 200 application.
products are delivered with Bluetooth switched on by default.
Third-party wordmarks, trademarks and logos
The
Bluetooth® wordmark and the
logo are registered trademarks and the property of
Bluetooth SIG, Inc. and
Hilti has been granted a license to use these trademarks.
Google Play and
Android™ are trademarks of
Google LLC .
All other trademarks and wordmarks used, even when not expressly stated or marked as such, are the property of their applicable owners.
Items supplied
Layout tool, 2 batteries, charger, tablet with charger and protective cover, target plate, manufacturer's certificate, operating instructions and
Hilti case
Other system products approved for use with this product can be found at your local
Hilti Store or at:
www.hilti.group
Technical data
Conditions (with 2 σ standard deviation) * favorable conditions: moderate temperature range, no strong ambient light sources (e.g. direct sunlight), bright and diffusely reflective target background
** unfavorable conditions: temperatures at the low or high end of the tolerance range, strong or direct ambient light sources, target background with very low or very high reflection
PMD 200
Typical battery life with B 12/4.0 battery at 23 °C/73 °F
8 h
Weight in accordance with EPTA procedure 01
2.9 kg (6.4 lb)
Self-leveling range
±3.5°
Working range (radius) under favorable conditions*
25 m (85 ft)
Laser class
Line laser (green)
2
Range-finding laser (red)
2
Output power
Line laser (green)
< 1 mW
Range-finding laser (red)
< 1 mW
Pulse duration
Range-finding laser (red)
< 2 ns
Frequency
Range-finding laser (red)
< 100 MHz
Beam angle
Line laser (green)
90°
Wavelength
Line laser (green)
510 nm
Range-finding laser (red)
635 nm
Beam divergence
Line laser (green)
0.05 mrad …0.08 mrad
Range-finding laser (red)
0.2 mrad …0.45 mrad
Bluetooth version
Bluetooth Low Energy 5.0
Bluetooth power
6.31 mW
Bluetooth frequency
2,400 MHz …2,483.5 MHz
Degree of protection (IEC 60529) without battery
IP 54
Tripod mount (BSW)
5/8 in
System measuring accuracy under favorable conditions*
±3 mm (±0.1 in)
System measuring accuracy under unfavorable conditions**
±5 mm (±0.2 in)
Storage temperature
−20 ℃ …70 ℃ (−4 ℉ …158 ℉)
Ambient temperature for operation
−10 ℃ …40 ℃ (14 ℉ …104 ℉)
Rated voltage
10.8 V
Rated current
350 mA
Max. site elevation
2000 m / 6560 ft AMSL
Max. humidity
80 %
Tablet
The technical data below constitute the minimum requirements for running the PMD 200 application.
PMC 200
Operating system
Android 7.0
Bluetooth
BLE
Display resolution
1,920 x 1,200
Battery
Battery operating voltage
10.8 V
Ambient temperature for operation
−17 ℃ …60 ℃ (1 ℉ …140 ℉)
Storage temperature
−20 ℃ …40 ℃ (−4 ℉ …104 ℉)
Battery charging starting temperature
−10 ℃ …45 ℃ (14 ℉ …113 ℉)
Preparations at the workplace
Observe the safety instructions and warnings in this documentation and on the product.
Charging the battery
Before charging the battery, read the operating instructions for the charger.
Make sure that the contacts on the battery and the contacts on the charger are clean and dry.
Use an approved charger to charge the battery.
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
Push the battery into the battery holder until it engages with an audible click.
Check that the battery is seated securely.
Removing the battery
Press the battery release button.
Remove the battery from the device.
Operation
Observe the safety instructions and warnings in this documentation and on the product.
Preparing and pairing layout tool and tablet
The tablet has to be paired to the layout tool only once, when the two are used together for the first time.
Position the layout tool on the floor at a point with the best view of the working area.
Switch the layout tool on.
Switch the tablet on and open the "PMD 200" app.
Accept the End User License Agreement.
Accept the use of location services.
Pair the layout tool with the tablet by selecting the layout tool with the appropriate serial number in the app.
The product's serial number is on the rating plate affixed to the back of the head.
The settings are saved so that they can be retrieved the next time the layout tool is used. Tablet and layout tool pair with each other automatically.
Wait until the layout tool has leveled itself automatically.
Creating new layout
When you start a new layout, the data of the last layout are irrevocably deleted.
On the app's start screen, select New layout .
If you want to resume working on your last layout, select Current layout on the start screen.
Defining control line
You have to measure out a control line before you can start setting out your layout.
The ways in which you can define a control line are as follows:
Measure two points on a control line or on a building axis.
Measure two points on a building wall or on building columns.
The rule of thumb for the control line is: The radius of the working range is roughly twice the length of the measured control line.
On the app's start screen, select New layout .
Define the control line (e.g. building axis or building wall) on the jobsite.
Position the target plate precisely on the first control point (0/0 starting point).
Use the left/right buttons to move the green laser line to the exact center of the control point.
To measure the first control point, select Measure .
Position the target plate precisely on the second control point (direction point).
Use the left/right buttons to move the green laser line to the exact center of the control point.
To measure the second control point, select Measure .
Check the control line and confirm it.
If the control line is not right, select
Back and remeasure the control points.
Creating layout points
The layout points have to be entered manually in the app in accordance with the plan of the building.
To move the layout point in the direction of the blue arrow, enter the value in the blue input box.
To move the layout point in the direction of the yellow arrow, enter the value in the yellow input box.
Entering values
Select New point in the app.
Select the appropriate input box (yellow/blue).
A keypad appears in the app.
Enter the appropriate value in accordance with the building plan.
To add or subtract a value, select the appropriate button (+/-).
When you finish defining the values, select OK .
When you have defined the position of the layout point, select Confirm .
Changing direction of the layout points
To change the direction of the layout points relative to the 0/0 point, use the direction arrows (up/down or left/right) below the input boxes.
Changing/deleting layout points
Select a layout point you want to change or delete.
Select the menu symbol at the top right.
To change a layout point, select Change .
Change the value in the appropriate input box.
To save the change, select Confirm .
To exit the menu without saving the change, select
Cancel .
To delete the selected layout point, select Delete .
Adjusting control point (0/0)
By default, every time you create a new layout point the control point (0/0) changes to the most recently created point.
Select a layout point that you want to define as the new control point (0/0).
Select the Temporary 0/0 radio button.
The layout point you selected is now the new control point (0/0).
The next layout point is created relative to the new control point.
Transferring layout point to the jobsite
The layout tool rotates the green laser toward the selected layout point.
To enable the red range-finding laser to measure the distance, move the PMDA 200 target plate along the green laser.
The red laser dot must be on the target plate.
The app tells you whether the target plate has to be moved closer or farther away.
As soon as you come within 50 cm (20 in) of the layout point, an acoustic signal sounds to help you pinpoint the layout point.
When the app shows a reading of 0.0, you have reached the position of the layout point.
Mark the layout point on the floor at the position where the green laser line hits the target plate.
To avoid measuring errors, make sure that the target plate is always plumb. Use the adjusting screw and the bubble level on the target plate for this purpose.
Laying out angle
To create an angle, you must first create or define a layout point that represents the hinge point of the angle.
Select a layout point you want to use as the hinge of the angle.
Select the menu symbol at the top right.
To create an angle, select Angle .
In the top input box, enter the value of the distance to the hinge point.
In the bottom input box, enter the angle.
Select the orientation of the angle by selecting another layout point toward which the angle will orient itself.
Select Confirm to create the new layout point. The device directly shows you the direction of the new layout point.
Laying out radius
To lay out points on a radius, you must first create or define a layout point that represents the center point of the radius.
Select a layout point that will represent the center point of the radius.
Select the menu symbol at the top right.
To create a radius, select Radius .
In the top input box, enter the value of the radius.
In the bottom input box, enter the length of the segments on the radius.
On the screen, select the starting point and the end point of the arc.
Define the desired arc by selecting the appropriate page.
To create the points, select Confirm .
The layout tool directly shows you the direction of the first layout point on the radius.
Laying out an arc through 2 points
To lay out an arc through 2 points, you must first create or define two points that represent the starting point and the end point of the arc.
Select the layout point that defines the starting point of the arc.
Select the menu symbol at the top right.
To create an arc through 2 points, select Arc through 2 points .
The function initially creates a sample arc.
In the top input box, enter either the radius of the arc or the height of the arc above an imaginary axis joining starting point and end point.
In the bottom input box, enter the length of the segments on the arc.
Select the layout point that defines the end point of the arc.
Select the arc of your choice from the options.
To create the points, select Confirm .
The layout tool directly shows you the direction of the first layout point on the arc.
Settings
Units
You can choose between metric and imperial units of measure.
Pairing with the layout tool
Shows which layout tool the tablet is paired with. Other layout tools within range are listed here.
As soon as it is paired to a tablet, the layout tool no longer appears in the list. You have to unpair the layout tool before you can pair it with another tablet.
Acoustic signal
You can switch the acoustic signal on or off. In the as-delivered condition, the signal is switched on by default.
Show intro
You can switch this function on or off. When this function is switched on, the introduction is displayed when you start the app. In the as-delivered condition, this function is switched on by default.
Show point names
You can switch this function on or off. When this function is switched off, the point names are hidden. In the as-delivered condition, this function is switched on by default.
About us
Use this function to view information about the software version, the tool's firmware version, licenses and legal matters.
Care and maintenance
WARNING
Risk of injury with battery inserted !
Always remove the battery before carrying out care and maintenance tasks!
Care and maintenance of the tool
Carefully remove stubborn dirt from the tool.
Carefully remove dust with a dry brush or cloth.
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
Do not operate the cordless tool if signs of damage are found or if parts malfunction. Have the tool repaired by Hilti Service immediately.
After cleaning and maintenance, fit all guards or protective devices and check that they function correctly.
Cleaning the laser exit window
Blow dust off the laser exit window.
Do not touch the laser exit window with your fingers.
Coarse cleaning materials can scratch the glass, impairing the accuracy of the device. Use only pure alcohol or water for cleaning, as other liquids can attack the plastic parts.
Observe the temperature limits when drying the equipment.
Transport and storage of cordless tools
Transport
Remove the battery.
Never transport batteries in bulk form (loose, unprotected).
Check tools and batteries for damage before use after long periods of transport.
Storage
CAUTION
Accidental damage caused by defective or leaking batteries !
Always store your products with the batteries removed!
Store the tool and battery in a place that is as cool and dry as possible.
Never store batteries in direct sunlight, on heating units or behind a window pane.
Store the tool and batteries in a place where they cannot be accessed by children or unauthorized persons.
Check the tool and batteries for damage before use after long periods of storage.
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
Layout tool and/or tablet cannot be switched on.
The battery is low.
Charge the battery.
The PMD 200 app is not available.
The app is in a submenu on the tablet.
Look for the PMD 200 app in the tablet's submenu.
The app was uninstalled.
Download the PMD 200 app again from the Google Play store.
Wrong language in the app
Language setting of the tablet
Change the language in the tablet settings. If the language is not supported, English is used by default in the app.
The app is not working.
Software malfunction
Shut the app down completely and then restart it.
End User License Agreement not accepted
Accept the End User License Agreement.
Unexpected closure of the app.
Tablet's power saving mode is activated
Deactivate the power saving mode in the tablet settings.
Layout tool and tablet cannot be paired.
Layout tool is switched off.
Switch the layout tool on.
Layout tool is experiencing a fault.
Switch the layout tool off and then on again. If the problem persists, consult Hilti Service.
Most of the materials from which
Hilti tools and appliances are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to
Hilti for recycling. Ask
Hilti Service or your Hilti representative for further information.
Battery disposalImproper disposal of batteries can result in health hazards from leaking gases or fluids.
DO NOT send batteries through the mail!
Cover the terminals with a non-conductive material (such as electrical tape) to prevent short circuiting.
Dispose of your battery out of the reach of children.
Dispose of the battery at your Hilti Store , or consult your local governmental garbage disposal or public health and safety resources for disposal instructions.
Do not dispose of power tools, electronic equipment or batteries as household waste!
Declaration of conformity
Conditions : Not USA We declare, on our sole responsibility, that the product described here complies with the applicable directives and standards.
The technical documentation is filed and stored here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | 86916 Kaufering, Germany
FCC statement (applicable in US) / IC statement (applicable in Canada)
This device has been tested and found to comply with the limits for a class A digital device, pursuant to part 15 of the FCC rules. These limits are intended to ensure adequate protection against electromagnetic interference when the device is operated in areas used for commercial purposes. This equipment generates, uses, and can radiate radio frequency energy and, if not installed and used in accordance with the instructions, may cause interference to radio communications. The user must bear costs incurred due to interference that operation of this device in residential areas can cause.
This device is in compliance with paragraph 15 of the FCC rules and the RSS‑210 specifications of ISED.
Operation is subject to the following two conditions:
This device shall cause no harmful interference.
This device must accept any interference received, including interference that may cause undesired operation.
Changes or modifications not expressly approved by
Hilti may restrict the user’s authorization to operate the equipment.
Manufacturer’s warranty
Please contact your local Hilti representative if you have questions about the warranty conditions.
Hilti Li-ion batteries
Instructions for safety and useThis documentation uses the term battery to describe rechargeable Hilti Li-ion battery packs containing several Li-ion cells joined together. These batteries are to be used in Hilti power tools exclusively. When using Hilti power tools, use only genuine
Hilti battery packs!
Hilti batteries are state of the art and are equipped with cell management and cell protection systems.
DescriptionThe batteries are composed of cells that contain lithium-ion storage materials that are capable of providing high specific energy density. Unlike NiMH and NiCd batteries, Li-ion batteries have a minimal memory effect, but they are extremely susceptible to external impact, deep discharge, and high temperatures. See
Safety Find our battery-powered products at your
Hilti Store or at:
www.hilti.group | USA:
www.hilti.com Safety
Do not under any circumstances modify or tamper with batteries!
Never use recycled or repaired batteries not approved by Hilti Service.
Do not use or charge batteries that have suffered mechanical impact, have been dropped from a height of more than one meter or are otherwise damaged. Examine your batteries regularly for signs of damage, such as dents, cuts or punctures.
Never use the battery or a battery-operated power tool as a hammer.
Avoid eye or skin contact with leaking liquids!
See What to do in case of damaged batteries
Damaged batteries can leak fluid which may moisten adjacent objects. Clean these objects with warm soapy water and replace the damaged batteries.
See What to do in case of damaged batteries
Never expose batteries to elevated temperature, sparking, or an open flame because the battery may explode.
Do not touch the battery poles with your fingers, tools, jewelry, or other metallic objects because this may cause a short circuit, electric shock, burns or explosions.
Keep batteries away from rain and moisture. Penetrating moisture can cause short circuits, electric shock, burns or explosions.
Use only chargers and power tools approved for the specific battery type. Read and follow the instructions in the respective user manuals.
Do not store or use the battery in explosion-prone environments containing combustible liquids or gases. An unexpected battery malfunction can cause an explosion under those conditions.
What to do in case of damaged batteries
If a Hilti battery is found to be damaged, contact your Hilti service partner.
If a battery is leaking, use safety goggles and gloves to avoid direct eye or skin contact.
To store a damaged battery, place the battery in a non-flammable container and cover the battery with dry sand, chalk powder (CaCO3) or silicate (Vermiculite). Then, close the lid air-tight and store the container away from flammable gases, liquids or objects.
Dispose of the container at your Hilti Store , or consult your local governmental garbage disposal or public health and safety resources for disposal instructions. Do not ship or mail damaged batteries!
Use a chemical spill cleanup kit to remove leaked battery fluid.
What to do in case of dysfunctional batteries
Watch for abnormal battery behavior, such as faulty charging or unusually long charging times, noticeable power loss, unusual charger LED activity, or leaking fluids. These are signs of an internal problem.
If you suspect an internal battery problem, contact your Hilti service partner.
A battery that no longer works, cannot be recharged or leaks fluid has to be disposed of as described above.
See What to do in case of damaged batteries .
What to do in case of a battery fire
WARNING
Battery fire hazard! A burning battery will release hazardous and potentially explosive liquids and fumes which may result in a corrosion injury, burns or explosion.
Wear your personal protective equipment when you tackle a battery fire.
Provide sufficient venting to permit hazardous and potentially explosive fumes to escape.
Leave the room immediately in case of intense smoke emission.
Consult a doctor in case of any skin or respiratory irritation.
Use only water to tackle a battery fire. Powder fire extinguishers and fire blankets are ineffective with Li-Ion batteries. Fires started by a lithium-ion battery in nearby materials can be extinguished with any appropriate extinguishing agent.
Do not try to move large quantities of damaged, burning or leaking batteries. Instead, remove surrounding materials and isolate the batteries. If the scale of the fire is larger than can be extinguished with available methods, contact the nearest firefighting authority.
In the case of a single burning battery:
Scoop the battery up with a shovel and drop it into a bucket of water, which will reduce the risk of igniting adjacent cells that have not yet reached run-away temperature.
Wait for the battery to cool down completely.
See What to do in case of damaged batteries .
Shipping and storage
Ambient operating temperature between -17 °C and +60 °C / 1 °F and 140 °F.
Storage temperature between -20 °C and +40 °C / -4 °F and 104 °F.
Do not store batteries on the charger. Always separate battery and charger after use.
Store batteries in a place that is as cool and dry as possible. Cool storage will increase battery life. Never store batteries where they are exposed to direct sunlight, on sources of heat or behind glass.
Do not send batteries through the mail. Consult your shipper for instructions on how to ship undamaged batteries.
Never transport batteries in bulk form (loose, unprotected). During transport, batteries should be protected from excessive shock and vibration and isolated from any conductive materials or other batteries that may come in contact with the terminals and cause a short circuit.
Maintenance and disposal
Keep the battery clean and free from oil and grease. Wipe off foreign matter of this nature with a clean, dry cloth.
Never use a battery with clogged ventilation slots. Clean the ventilation slots carefully with a soft brush.
Prevent foreign matter from penetrating into the interior.
Prevent unnecessary accumulations of dust or dirt on the battery. Clean the battery with a soft brush or a clean, dry cloth.
Do not permit moisture to penetrate inside the battery. If water does penetrate inside the battery treat it as a damaged battery and isolate it in a non-flammable container.
See What to do in case of damaged batteries
Improper disposal may cause health hazards from leaking gases or fluids. Dispose of the battery at your Hilti Store , or consult your local garbage disposal or public health and safety resources for disposal instructions. Do not ship or mail damaged batteries!
Do not dispose of batteries as household waste.
Dispose of your battery out of the reach of children. Cover the terminals with a non-conductive material to prevent short circuiting.