Please note, the order volume has been updated. This is due to package and minimum order quantities.
Please note, the order volume has been updated to {0}. This is due to package and minimum order quantities.. This is due to package and minimum order quantities.
Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
Observe the safety instructions and warnings in this documentation and on the product.
Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
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
Draws attention to a potentially dangerous situation that could lead to slight personal injury or damage to the equipment or other property.
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
The following symbols are used on the product:
Risk of crushing injury!
Wireless data transfer
Hilti Li-ion battery type series used. Observe the information given in the section headed Intended use .
Product information
products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
The type designation and serial number are printed on the rating plate.
Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product. Product information
Crimping tool
NCR 060 II-A22
Generation
01
Serial no.
Declaration of conformity
We declare, on our sole responsibility, that the product described here complies with the applicable directives and standards. A copy of the declaration of conformity can be found at the end of this documentation.
The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | 86916 Kaufering, Germany
Safety
General power tool safety warnings
WARNINGRead all safety warnings, instructions, illustrations and specifications provided with this power tool. Failure to follow all instructions listed below may result in electric shock, fire and/or serious injury.
Save all warnings and instructions for future reference. The term "power tool" in the warnings refers to your mains-operated (corded) power tool or battery-operated (cordless) power tool.
Work area safety
Keep work area clean and well lit. Cluttered or dark areas invite accidents.
Do not operate power tools in explosive atmospheres, such as in the presence of flammable liquids, gases or dust. Power tools create sparks which may ignite the dust or fumes.
Keep children and bystanders away while operating a power tool. Distractions can cause you to lose control.
Electrical safety
Power tool plugs must match the outlet. Never modify the plug in any way. Do not use any adapter plugs with earthed (grounded) power tools. Unmodified plugs and matching outlets will reduce risk of electric shock.
Avoid body contact with earthed or grounded surfaces, such as pipes, radiators, ranges and refrigerators. There is an increased risk of electric shock if your body is earthed or grounded.
Do not expose power tools to rain or wet conditions. Water entering a power tool will increase the risk of electric shock.
Do not abuse the cord. Never use the cord for carrying, pulling or unplugging the power tool. Keep cord away from heat, oil, sharp edges or moving parts. Damaged or entangled cords increase the risk of electric shock.
When operating a power tool outdoors, use an extension cord suitable for outdoor use. Use of a cord suitable for outdoor use reduces the risk of electric shock.
If operating a power tool in a damp location is unavoidable, use a residual current device (RCD) protected supply. Use of an RCD reduces the risk of electric shock.
Personal safety
Stay alert, watch what you are doing and use common sense when operating a power tool.Do not use a power tool while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating power tools may result in serious personal injury.
Use personal protective equipment. Always wear eye protection. Protective equipment such as a dust mask, non-skid safety shoes, hard hat or hearing protection used for appropriate conditions will reduce personal injuries.
Prevent unintentional starting. Ensure the switch is in the off-position before connecting to power source and/or battery pack, picking up or carrying the tool. Carrying power tools with your finger on the switch or energising power tools that have the switch on invites accidents.
Remove any adjusting key or wrench before turning the power tool on. A wrench or a key left attached to a rotating part of the power tool may result in personal injury.
Do not overreach. Keep proper footing and balance at all times. This enables better control of the power tool in unexpected situations.
Dress properly. Do not wear loose clothing or jewellery. Keep your hair, clothing and gloves away from moving parts. Loose clothes, jewellery or long hair can be caught in moving parts.
If devices are provided for the connection of dust extraction and collection facilities, ensure these are connected and properly used. Use of dust collection can reduce dust-related hazards.
Do not let familiarity gained from frequent use of tools allow you to become complacent and ignore tool safety principles. A careless action can cause severe injury within a fraction of a second.
Power tool use and care
Do not force the power tool. Use the correct power tool for your application. The correct power tool will do the job better and safer at the rate for which it was designed.
Do not use the power tool if the switch does not turn it on and off. Any power tool that cannot be controlled with the switch is dangerous and must be repaired.
Disconnect the plug from the power source and/or remove the battery pack, if detachable, from the power tool before making any adjustments, changing accessories, or storing power tools. Such preventive safety measures reduce the risk of starting the power tool accidentally.
Store idle power tools out of the reach of children and do not allow persons unfamiliar with the power tool or these instructions to operate the power tool. Power tools are dangerous in the hands of untrained users.
Maintain power tools and accessories. Check for misalignment or binding of moving parts, breakage of parts and any other condition that may affect the power tool’s operation. If damaged, have the power tool repaired before use. Many accidents are caused by poorly maintained power tools.
Keep cutting tools sharp and clean. Properly maintained cutting tools with sharp cutting edges are less likely to bind and are easier to control.
Use the power tool, accessories and tool bits etc. in accordance with these instructions, taking into account the working conditions and the work to be performed. Use of the power tool for operations different from those intended could result in a hazardous situation.
Keep handles and grasping surfaces dry, clean and free from oil and grease. Slippery handles and grasping surfaces do not allow for safe handling and control of the tool in unexpected situations.
Battery tool use and care
Recharge only with the charger specified by the manufacturer. A charger that is suitable for one type of battery pack may create a risk of fire when used with another battery pack.
Use power tools only with specifically designated battery packs. Use of any other battery packs may create a risk of injury and fire.
When battery pack is not in use, keep it away from other metal objects, like paper clips, coins, keys, nails, screws or other small metal objects, that can make a connection from one terminal to another. Shorting the battery terminals together may cause burns or a fire.
Under abusive conditions, liquid may be ejected from the battery; avoid contact. If contact accidentally occurs, flush with water. If liquid contacts eyes, additionally seek medical help. Liquid ejected from the battery may cause irritation or burns.
Do not use a battery pack or tool that is damaged or modified. Damaged or modified batteries may exhibit unpredictable behaviour resulting in fire, explosion or risk of injury.
Do not expose a battery pack or tool to fire or excessive temperature. Exposure to fire or temperature above 130° C (265 °F) may cause explosion.
Follow all charging instructions and do not charge the battery pack or tool outside the temperature range specified in the instructions. Charging improperly or at temperatures outside the specified range may damage the battery and increase the risk of fire.
Service
Have your power tool serviced by a qualified repair person using only identical replacement parts. This will ensure that the safety of the power tool is maintained.
Never service damaged battery packs. Service of battery packs should only be performed by the manufacturer or authorized service providers.
Additional safety instructions for crimping tools
Personal safety
Use the product only if it is in perfect working order.
Never tamper with or modify the tool in any way.
Check that the locking pin is pushed in all the way and securely engaged.
Electrical safety
Before use of the power tool, all live cables or other items carrying electric voltage within the area in which the user is working are to be switched off. If this is not possible, the corresponding safety precautions for working in the proximity of live cables or equipment must be implemented and observed.
Do not crimp live parts, i.e. parts carrying electric voltage. The tool must be considered to be uninsulated and must therefore be used in conjunction with personal protective equipment (protective gloves, protective footwear, protective clothing, etc.) of a type suitable to provide protection for yourself and other persons in the vicinity. The power tool is suitable for use on insulated platforms.
Power tool use and care
After approx. 50 consecutive crimping operations, switch the power tool off and allow it to cool down for about 15 minutes. Overheating can lead to damage to the power tool.
Battery use and care
Observe the special regulations and instructions applicable to the transport, storage and use of Li-ion batteries.
Do not expose batteries to high temperatures, direct sunlight or fire.
Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C.
Do not use or charge batteries that have suffered mechanical impact, have been dropped from a height or show signs of damage. In this case, always contact your HiltiService .
If the battery is too hot to touch it may be defective. In this case, place the product in a non-flammable location, well away from flammable materials, where it can be kept under observation and allowed to cool down. In this case, always contact your HiltiService .
Description
Product overview
Crimping / pressing head
Piston reset slider for use in case of fault or emergency
Servicing and fault indicator (red LED)
Battery release button
Battery
Slot on both sides to fasten the Hilti retaining leash
White LED to illuminate the working area
Control switch
Crimping / pressing ram (stepped)
Pivoting bar to open the tool head
Lever to lock/unlock the tool head
Intended use
The product described is a cordless electro-hydraulic crimping tool.
It is designed for crimping connectors made of copper (Cu) or aluminum (Al).
Before use of the power tool, all live cables or other items carrying electric voltage within the area in which the user is working must be switched off. If this is not possible, the corresponding safety precautions for working in the proximity of live cables or equipment must be implemented and observed.
Use only Hilti lithium‑ion batteries of the B 22 series with this product.
Use only Hilti battery chargers of the C4/36 series for charging these batteries.
Possible misuse
Do not use this hand-held product clamped in a fixed position or as a stationary device.
Do not use the product in heavy rain or under water.
Lithium‑ion battery status display
The charge state of the Li-ion battery and malfunctions of the product are indicated by the indicator of the Li‑ion battery. The charge status of the Li‑ion battery is indicated after one of the two battery release buttons is short-pressed.
Status
Meaning
4 LEDs light.
State of charge: 75 % to 100 %
3 LEDs light.
State of charge: 50 % to 75 %
2 LEDs light.
State of charge: 25 % to 50 %
1 LED lights.
State of charge: 10 % to 25 %
1 LED flashes.
State of charge: < 10 %
Battery state of charge cannot be displayed while the control switch is pressed and for up to 5 seconds after releasing the control switch. If the LEDs of the charge state indicator flash, follow the instructions in the 'Troubleshooting' section.
Items supplied
Crimping / pressing tool, operating instructions.
Other system products approved for use with this product can be found at your local
HILTI STORE or online at:
www.hilti.group
Selection of the connecting material
A table to assist with selecting the type of cable and cable terminal to be used can be found at the end of these operating instructions.
Technical data
NCR 060 II-A22
Rated voltage
21.6 V
Weight in accordance with EPTA procedure 01
2.98 kg
Max. crimping force
53 kN
Crimping time
≈ 5 s
Max. permissible crimping capacity
500 MCM (240 mm²) Cu
350 MCM (240 mm²) Al
Storage temperature
−20 ℃ … 70 ℃
Ambient temperature for operation
−17 ℃ … 60 ℃
Noise information and vibration values in accordance with EN 60745
The sound pressure and vibration values given in these instructions were measured in accordance with a standardized test and can be used to compare one power tool with another. They can also be used for a preliminary assessment of exposure. The data given represents the main applications of the power tool. However, if the power tool is used for different applications, with different accessory tools, or is poorly maintained, the data can vary. This can significantly increase exposure over the total working period. An accurate estimation of exposure should also take into account the times when the tool is switched off, or when it is running but not actually being used for a job. This can significantly reduce exposure over the total working period. Identify additional safety measures to protect the operator from the effects of noise and/or vibration, for example: Maintaining the power tool and accessory tools, keeping the hands warm, organization of work patterns.
Noise values
Sound (power) level (L WA)
80 dB(A)
Uncertainty for the sound power level (K WA)
2.5 dB(A)
Emission sound pressure level (L pA)
70 dB(A)
Uncertainty for the sound pressure level (K pA)
2.5 dB(A)
Vibration values
Total vibration (during operation) (a)
2.5 m/s²
Uncertainty (K)
1.5 m/s²
Battery
Battery operating voltage
21.6 V
Ambient temperature for operation
−17 ℃ … 60 ℃
Storage temperature
−20 ℃ … 40 ℃
Battery charging starting temperature
−10 ℃ … 45 ℃
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
Use an approved charger to charge the battery.
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
Push the battery into the battery holder until it engages with an audible click.
Check that the battery is seated securely.
Removing the battery
Press the release buttons on the battery.
Pull the battery out of its holder in the device.
Assemble Hilti retaining leash (optional)
ATTENTION
Damage to the product and / or the retaining leash. Incorrect handling can result in damage to the product and/or retaining leash.
Do not use a metal chain as a retaining leash. Do not use retaining leashes longer than 6 ft (2 m).
To avoid damage and injury, when working at a height it is advisable to use the
Hilti retaining strap.
The retaining strap allows a securing cord or leash to be attached.
When working with the product, you must comply with national regulations for working at heights.
Remove the battery.
Insert the two tabs on the retaining leash into the slots on each side of the base.
Secure the retaining leash with the screws supplied.
Refit the battery.
Dismantle the Hilti retaining leash (optional)
Remove the battery.
Remove the two retaining strap securing screws.
Pull the two retaining strap tabs out of the slots in the base and remove the retaining strap.
Refit the battery.
Crimping
WARNING
Danger! Risk of fire due to faulty crimping.
Use only cable terminals of the correct type and size for the cable. Failure to observe this point can result in faulty crimping.
Listen for the signal tone and check that the piston has retracted. If no signal tone is heard or if the piston does not retract then the crimping is faulty.
WARNING
Risk of injury! Unintentional starting.
Remove the battery before inserting the parts to be connected, i.e. crimped.
Open the latch and pivoting bar and insert the connector in the die.
Close the pivoting bar and the latch.
Insert the battery.
Press the control switch.
Keep the control switch pressed until the piston has retracted.
Open the latch and pivoting bar and remove the connector.
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
To help ensure safe and reliable operation, use only genuine Hilti spare parts and consumables. Spare parts, consumables and accessories approved by Hilti for use with the product can be found at your local
Hilti Store or online at:
www.hilti.group .
Transport and storage of cordless tools
Transport
CAUTION
Accidental starting during transport !
Always transport your products with the batteries removed!
Remove the battery.
Never transport batteries in bulk form (loose, unprotected).
Check the tool and batteries for damage before use after long periods of transport.
Storage
CAUTION
Accidental damage caused by defective or leaking batteries !
Always store your products with the batteries removed!
Store the tool and batteries in a place that is as cool and dry as possible.
Never store batteries in direct sunlight, on heating units or behind a window pane.
Store the tool and batteries in a place where they cannot be accessed by children or unauthorized persons.
Check the tool and batteries for damage before use after long periods of storage.
Troubleshooting
If the trouble you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, please contact
Hilti Service.
The crimping tool is not in working order.
Malfunction
Possible cause
Action to be taken
The LEDs on the battery indicate nothing.
The battery is not correctly inserted.
Push the battery in until it engages with a double click.
The battery is discharged.
Change the battery and charge the empty battery.
The battery is too hot or too cold.
Allow the battery to cool down or to warm up to room temperature.
1 LED on the battery blinks.
The battery is discharged.
Change the battery and charge the empty battery.
The battery is too hot or too cold.
Allow the battery to cool down or to warm up to room temperature.
4 LEDs on the battery blink.
Product momentarily overloaded.
Allow the product to cool down.
Red LED => lights continuously and a warning tone is emitted.
Technical problem.
Incorrect operation is possible! Contact Hilti Service.
Red LED => blinks at short intervals and a warning tone is emitted.
The state of charge of the battery is too low to allow a complete operating cycle.
Change the battery and charge the empty battery.
Red LED => lights briefly and no warning tone is emitted.
Product overheated.
Allow the product to cool down.
The crimping tool is in working order.
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
The battery does not engage with an audible double click.
The retaining lugs on the battery are dirty.
Clean the retaining lugs and refit the battery.
Red LED => blinks at long intervals and a warning tone is emitted.
Crimping pressure not achieved (tool was used incorrectly).
Make sure that the tool is used correctly and check the crimped / pressed part if unsure.
Red LED => lights continuously and a warning tone is emitted.
Technical problem.
Incorrect operation is possible! Contact Hilti Service.
Disposal
Most of the materials from which
Hilti tools and appliances are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to
Hilti for recycling. Ask
Hilti Service or your Hilti representative for further information.
Battery disposalImproper disposal of batteries can result in health hazards from leaking gases or fluids.
DO NOT send batteries through the mail!
Cover the terminals with a non-conductive material (such as electrical tape) to prevent short circuiting.
Dispose of your battery out of the reach of children.
Dispose of the battery at your Hilti Store , or consult your local governmental garbage disposal or public health and safety resources for disposal instructions.
Do not dispose of power tools, electronic equipment or batteries as household waste!
RoHS (Restriction of Hazardous Substances)
Click on the link to go to the table of hazardous substances: qr.hilti.com/r7794687.
There is a link to the RoHS table, in the form of a QR code, at the end of this document.
Manufacturer’s warranty
Please contact your local Hilti representative if you have questions about the warranty conditions.