Choose language

SR 30-A36

Original operating instructions

Information about the documentation

About this documentation

  • Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
  • Observe the safety instructions and warnings in this documentation and on the product.
  • Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.

Explanation of symbols used

Warnings

Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:
DANGER
DANGER !
  • Draws attention to imminent danger that will lead to serious personal injury or fatality.
WARNING
WARNING !
  • Draws attention to a potential threat of danger that can lead to serious injury or fatality.
CAUTION
CAUTION !
  • Draws attention to a potentially dangerous situation that could lead to slight personal injury or damage to the equipment or other property.

Symbols in the documentation

The following symbols are used in this document:
Image alternative Read the operating instructions before use.
Image alternative Instructions for use and other useful information
Image alternative Dealing with recyclable materials
Image alternative Do not dispose of electric equipment and batteries as household waste

Symbols in the illustrations

The following symbols are used in illustrations:
Image alternative These numbers refer to the corresponding illustrations found at the beginning of these operating instructions
Image alternative The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text
Image alternative Item reference numbers are used in the overview illustrations and refer to the numbers used in the product overview section
Image alternative This symbol is intended to draw special attention to certain points when handling the product.

Product-dependent symbols

Symbols on the product

The following symbols can be used on the product:
Image alternative Direct current (DC)
Image alternative Stroke rate under no load
Image alternative Wireless data transfer
Image alternative Li-ion battery
Image alternative Hilti Li-ion battery type series used. Observe the information given in the section headed Intended use .

Product information

Image alternative products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
The type designation and serial number are printed on the rating plate.
  • Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
    Product information
    Reciprocating saw
    SR 30-A36
    Generation
    01
    Serial no.

Declaration of conformity

We declare, on our sole responsibility, that the product described here complies with the applicable directives and standards. A copy of the declaration of conformity can be found at the end of this documentation.
The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | 86916 Kaufering, Germany

Safety

General power tool safety warnings

Image alternative WARNING Read all safety warnings, instructions, illustrations and specifications provided with this power tool. Failure to follow all instructions listed below may result in electric shock, fire and/or serious injury.
Save all warnings and instructions for future reference.
The term "power tool" in the warnings refers to your mains-operated (corded) power tool or battery-operated (cordless) power tool.
Work area safety
  • Keep work area clean and well lit. Cluttered or dark areas invite accidents.
  • Do not operate power tools in explosive atmospheres, such as in the presence of flammable liquids, gases or dust. Power tools create sparks which may ignite the dust or fumes.
  • Keep children and bystanders away while operating a power tool. Distractions can cause you to lose control.
Electrical safety
  • Power tool plugs must match the outlet. Never modify the plug in any way. Do not use any adapter plugs with earthed (grounded) power tools. Unmodified plugs and matching outlets will reduce risk of electric shock.
  • Avoid body contact with earthed or grounded surfaces, such as pipes, radiators, ranges and refrigerators. There is an increased risk of electric shock if your body is earthed or grounded.
  • Do not expose power tools to rain or wet conditions. Water entering a power tool will increase the risk of electric shock.
  • Do not abuse the cord. Never use the cord for carrying, pulling or unplugging the power tool. Keep cord away from heat, oil, sharp edges or moving parts. Damaged or entangled cords increase the risk of electric shock.
  • When operating a power tool outdoors, use an extension cord suitable for outdoor use. Use of a cord suitable for outdoor use reduces the risk of electric shock.
  • If operating a power tool in a damp location is unavoidable, use a residual current device (RCD) protected supply. Use of an RCD reduces the risk of electric shock.
Personal safety
  • Stay alert, watch what you are doing and use common sense when operating a power tool. Do not use a power tool while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating power tools may result in serious personal injury.
  • Use personal protective equipment. Always wear eye protection. Protective equipment such as a dust mask, non-skid safety shoes, hard hat or hearing protection used for appropriate conditions will reduce personal injuries.
  • Prevent unintentional starting. Ensure the switch is in the off-position before connecting to power source and/or battery pack, picking up or carrying the tool. Carrying power tools with your finger on the switch or energising power tools that have the switch on invites accidents.
  • Remove any adjusting key or wrench before turning the power tool on. A wrench or a key left attached to a rotating part of the power tool may result in personal injury.
  • Do not overreach. Keep proper footing and balance at all times. This enables better control of the power tool in unexpected situations.
  • Dress properly. Do not wear loose clothing or jewellery. Keep your hair, clothing and gloves away from moving parts. Loose clothes, jewellery or long hair can be caught in moving parts.
  • If devices are provided for the connection of dust extraction and collection facilities, ensure these are connected and properly used. Use of dust collection can reduce dust-related hazards.
  • Do not let familiarity gained from frequent use of tools allow you to become complacent and ignore tool safety principles. A careless action can cause severe injury within a fraction of a second.
Power tool use and care
  • Do not force the power tool. Use the correct power tool for your application. The correct power tool will do the job better and safer at the rate for which it was designed.
  • Do not use the power tool if the switch does not turn it on and off. Any power tool that cannot be controlled with the switch is dangerous and must be repaired.
  • Disconnect the plug from the power source and/or remove the battery pack, if detachable, from the power tool before making any adjustments, changing accessories, or storing power tools. Such preventive safety measures reduce the risk of starting the power tool accidentally.
  • Store idle power tools out of the reach of children and do not allow persons unfamiliar with the power tool or these instructions to operate the power tool. Power tools are dangerous in the hands of untrained users.
  • Maintain power tools and accessories. Check for misalignment or binding of moving parts, breakage of parts and any other condition that may affect the power tool’s operation. If damaged, have the power tool repaired before use. Many accidents are caused by poorly maintained power tools.
  • Keep cutting tools sharp and clean. Properly maintained cutting tools with sharp cutting edges are less likely to bind and are easier to control.
  • Use the power tool, accessories and tool bits etc. in accordance with these instructions, taking into account the working conditions and the work to be performed. Use of the power tool for operations different from those intended could result in a hazardous situation.
  • Keep handles and grasping surfaces dry, clean and free from oil and grease. Slippery handles and grasping surfaces do not allow for safe handling and control of the tool in unexpected situations.
Battery tool use and care
  • Recharge only with the charger specified by the manufacturer. A charger that is suitable for one type of battery pack may create a risk of fire when used with another battery pack.
  • Use power tools only with specifically designated battery packs. Use of any other battery packs may create a risk of injury and fire.
  • When battery pack is not in use, keep it away from other metal objects, like paper clips, coins, keys, nails, screws or other small metal objects, that can make a connection from one terminal to another. Shorting the battery terminals together may cause burns or a fire.
  • Under abusive conditions, liquid may be ejected from the battery; avoid contact. If contact accidentally occurs, flush with water. If liquid contacts eyes, additionally seek medical help. Liquid ejected from the battery may cause irritation or burns.
  • Do not use a battery pack or tool that is damaged or modified. Damaged or modified batteries may exhibit unpredictable behaviour resulting in fire, explosion or risk of injury.
  • Do not expose a battery pack or tool to fire or excessive temperature. Exposure to fire or temperature above 130° C (265 °F) may cause explosion.
  • Follow all charging instructions and do not charge the battery pack or tool outside the temperature range specified in the instructions. Charging improperly or at temperatures outside the specified range may damage the battery and increase the risk of fire.
Service
  • Have your power tool serviced by a qualified repair person using only identical replacement parts. This will ensure that the safety of the power tool is maintained.
  • Never service damaged battery packs. Service of battery packs should only be performed by the manufacturer or authorized service providers.

Additional safety instructions for saws with reciprocating saw blade

  • Hold the power tool by the insulated gripping surfaces when performing work in which the accessory tool might come into contact with concealed wiring. If the accessory tool comes into contact with a live wire, metal parts of the power tool can also become live, resulting in an electric shock.
  • Use clamps or some other suitable means to firmly secure the workpiece to a stable supporting surface. Holding the workpiece only by hand or against your body leaves it unstable, which can lead to loss of control.

Additional safety instructions for saws

Personal safety
  • Keep your hands away from the cutting area and the blade. Keep your second hand on the auxiliary handle or the motor housing. When both hands are on the saw they cannot be injured by it.
  • Use the product only when it is in perfect working order.
  • Never tamper with or modify the power tool in any way.
  • Wear protective gloves also when changing the accessory tool. Touching the accessory tool presents a risk of injury (cuts or burns).
  • Before starting work, check the hazard class of the dust that will be produced when working. Use an industrial vacuum cleaner with an officially approved protection class in compliance with the locally applicable dust protection regulations. Dust from materials such as lead-based paint, certain types of wood and concrete/masonry/stone containing quartz, minerals or metal can be harmful to health.
  • Make sure that the workplace is well ventilated and, if necessary, wear a respirator appropriate for the type of dust generated. Contact with or inhalation of the dust can cause allergic reactions and/or respiratory or other diseases among operators or bystanders. Only specialists are permitted to handle material containing asbestos.
  • Do not reach underneath the workpiece.
  • Never hold the workpiece with your hand or across your leg. Secure the workpiece in a sturdy holder.
  • Always hold the power tool firmly with both hands on the handles provided for the purpose and position your arms to absorb kickback forces.
  • Keep the grips clean and dry.
  • Position yourself off to one side of the blade, never bring the blade into line with your body. The saw can jump backward toward you if kickback occurs.
  • If the saw blade binds or when you interrupt work for any reason, switch off the saw and hold it motionless in the material until the saw blade comes to a complete stop. Never attempt to remove the saw from the workpiece or pull the saw back while the blade is in motion, as otherwise the saw could kick back.
  • When restarting a saw in the workpiece, center the saw blade in the kerf and check that saw teeth are not in engagement with the workpiece.
  • Use extra caution when sawing into walls or other blind areas. As it enters the material the blade might encounter a hidden obstruction, resulting in kickback.
Electrical safety
  • Before beginning work, check the working area for concealed electric cables or gas and water pipes. External metal parts of the power tool can become live, presenting a risk of electric shock, if you accidentally damage an electric cable.
  • Hold the power tool by the insulated gripping surfaces when performing work in which the accessory tool might come into contact with concealed wiring. If the accessory tool comes into contact with a live wire, metal parts of the power tool can also become live, resulting in an electric shock.
Power tool use and care
  • Do not use dull or damaged blades. These cause increased friction and present a high risk of the saw blade binding or kicking back.
  • Comply with the manufacturer's instructions for handling and storing saw blades.
  • The product must be pressed against the workpiece until the contact shoe makes firm contact. This ensures optimum and safe progress as you work.
  • Wear suitable protective clothing as protection against hot particles of material.

Additional safety instructions

  • Use the product only when it is in perfect working order.
  • Never tamper with or modify the power tool in any way.
  • Do not use dull or damaged blades. These cause increased friction and present a high risk of the saw blade binding or kicking back.
  • Before beginning work, check the working area for concealed electric cables or gas and water pipes. External metal parts of the power tool can become live, presenting a risk of electric shock, if you accidentally damage an electric cable.
  • Secure the workpiece in a sturdy holder. Never hold the workpiece with your hand or across your leg.
  • Switch the product on only after bringing it to the working position.
  • When working with the power tool, always guide it away from your body.
  • Apply only moderate pressure and cut at an appropriate speed, especially when cutting large-diameter pipes. This will help to prevent the power tool overheating.
  • Before cutting through pipes, make sure that they are empty of medium. Drain the pipes if necessary.
  • When cutting through pipes, hold the power tool above the level of the pipe you are cutting through.
  • The power tool is not protected against ingress of moisture. Liquid running out of a pipe can cause a short circuit in the power tool.
  • Never cut into unknown materials and make sure the path of the saw is free of obstructions above and below the workpiece.
  • The power tool can kick back if the saw blade comes into contact with an obstructing object.
  • Wear protective gloves also when changing the accessory tool. Touching the accessory tool presents a risk of injury (cuts or burns).
  • Always remove the battery when the power tool is not in use, before maintenance, before changing accessory tools and before transport.
  • Engage the transport lock before storing or transporting the power tool.
  • Comply with the manufacturer's instructions for handling and storing saw blades.
  • The user and any other persons in the vicinity must wear suitable eye protection, a hard hat, ear protection, protective gloves and breathing protection while the power tool is in use.
  • Always use a saw blade of appropriate length. The saw blade must project past the workpiece throughout the entire stroke.
  • Take breaks between working and do relaxation and finger exercises to improve the blood circulation in your fingers.
  • Do not look directly into the light source (LEDs) of the power tool and do not aim the beam at other persons’ faces. Risk of dazzling or eye damage.
  • Flying fragments can injure the body and eyes. Wear your personal protective equipment and always wear protective glasses and protective gloves.
  • If work involves break-through, always secure the area on the side opposite where the work is carried out.

Battery use and care

  • Observe the special regulations and instructions applicable to the transport, storage and use of Li-ion batteries.
  • Do not expose batteries to high temperatures, direct sunlight or fire.
  • Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C.
  • Do not use or charge batteries that have suffered mechanical impact, have been dropped from a height or show signs of damage. In this case, always contact your Hilti  Service .
  • If the battery is too hot to touch it may be defective. In this case, place the product in a non-flammable location, well away from flammable materials, where it can be kept under observation and allowed to cool down. In this case, always contact your Hilti  Service .

Description

Product overview

Image alternative
  1. Blade holder
  2. Mount for cutting assist
  3. Folding scaffold hook
  4. Speed preselection
  5. Safety lock
  6. Control switch
  7. Rear grip
  8. Battery state of charge indicator
  9. Battery release button
  10. Battery
  11. Attachment eye for lanyard
  12. Front gripping area
  13. Saw blade release lever
  14. Dust removal adapter (USA: accessory)
  15. Contact shoe
  16. Release button for contact shoe
  17. Saw blade
  18. Cutting assist (accessory)

Intended use

The product described is a cordless reciprocating saw. It is designed for cutting wood, wood-like materials, metals and plastics.

The product is designed for two-handed operation.
  • Use only Hilti Li-ion batteries from the B 36 series with this product.

  • Use only Hilti battery chargers from the C4/36 series for these batteries.

Possible misuse

  • Do not use the power tool to cut bricks, concrete, cellular concrete, natural stone or tiles.
  • Do not use the product to cut pipes containing liquids.
  • Do not saw into unknown materials.

Lithium‑ion battery status display

The Li-ion battery state of charge and malfunctions of the power tool are indicated by the display on the Li‑ion battery. The Li‑ion battery state of charge is displayed after pressing one of the two battery release buttons.
Status
Meaning
4 LEDs light.
State of charge: 75 % to 100 %
3 LEDs light.
State of charge: 50 % to 75 %
2 LEDs light.
State of charge: 25 % to 50 %
1 LED lights.
State of charge: 10 % to 25 %
1 LED blinks.
State of charge: < 10 %
1 LED blinks, the power tool is not ready for use.
The battery has overheated or is completely discharged.
4 LEDs blink, the power tool is not ready for use.
The power tool is overloaded or has overheated.
Battery state of charge cannot be displayed while the control switch is pressed and for up to 5 seconds after releasing the control switch.
If the battery display LEDs blink, please observe the instructions given in the Troubleshooting section.

Items supplied

Reciprocating saw, operating instructions.
Other system products approved for use with this product can be found at your local Hilti Store or at: www.hilti.group .

Technical data


SR 30-A36
Rated voltage
36 V
Weight in accordance with EPTA procedure 01
5.2 kg
Stroke rate (Stage 1)
2,500 /min
Stroke rate (Stage 2)
2,800 /min
Stroke length
32 mm
Blade holder
0.5 in
Ambient temperature for operation
−17 ℃ … 60 ℃
Storage temperature
−20 ℃ … 70 ℃

Noise information and vibration values in accordance with EN 62841

The sound pressure and vibration values given in these instructions were measured in accordance with a standardized test and can be used to compare one power tool with another. They can also be used for a preliminary assessment of exposure.
The data given represent the main applications of the power tool. However, if the power tool is used for different applications, with different accessory tools, or is poorly maintained, the data can vary. This can significantly increase exposure over the total working period.
An accurate estimation of exposure should also take into account the times when the tool is switched off, or when it is running but not actually being used for a job. This can significantly reduce exposure over the total working period.
Identify additional safety measures to protect the operator from the effects of noise and/or vibration, for example: maintaining the power tool and accessory tools, keeping the hands warm, organization of work patterns.
Noise information

SR 30-A36
Sound power level (LWA)
96 dB(A)
Uncertainty for the sound power level (KWA)
5 dB(A)
Sound pressure level (LpA)
85 dB(A)
Uncertainty for the sound pressure level (KpA)
5 dB(A)
Total vibration

SR 30-A36
Vibration emission value for sawing chipboard (ah,B)
22.5 m/s²
Uncertainty sawing chipboard (K)
3.7 m/s²
Vibration emission value for sawing wooden beams (ah,WB)
20.5 m/s²
Uncertainty sawing wooden beams (K)
3.3 m/s²

Battery

Battery operating voltage
36 V
Ambient temperature for operation
−17 ℃ … 60 ℃
Storage temperature
−20 ℃ … 40 ℃
Battery charging starting temperature
−10 ℃ … 45 ℃

Preparations at the workplace

CAUTION
Risk of injury by inadvertent starting!
  • Before inserting the battery, make sure that the product is switched off.
  • Remove the battery before making any adjustments to the power tool or before changing accessories.
Observe the safety instructions and warnings in this documentation and on the product.

Charging the battery

  1. Before charging the battery, read the operating instructions for the charger.
  2. Make sure that the contacts on the battery and the contacts on the charger are clean and dry.
  3. Use an approved charger to charge the battery.

Inserting the battery

CAUTION
Risk of injury by short circuit or falling battery!
  • Before inserting the battery, make sure that the contacts on the battery and the contacts on the product are free of foreign matter.
  • Make sure that the battery always engages correctly.
  1. Charge the battery fully before using it for the first time.
  2. Push the battery into the battery holder until it engages with an audible click.
  3. Check that the battery is seated securely.

Removing the battery

  1. Press the release buttons on the battery.
  2. Pull the battery out of its holder in the device.

Installing the scaffold hook (accessory)

Image alternative
  1. Engage the transport lock.
  2. Install the scaffold hook.

Inserting the saw blade

Use only saw blades with a 1/2" connection end.
Image alternative
  1. Activate the transport lock or separate the battery from the power tool.
  2. Check that the connection end of the accessory tool is clean and lightly greased. Clean it and grease it if necessary.
  3. Push the locking lever up as far as it will go and hold it in this position.
  4. Push the saw blade into the chuck from in front.
  5. Allow the locking lever to return to its original position.
  6. Grip and pull the saw blade to check that it is locked in position.

Installing the dust removal adapter (USA: accessory)

Image alternative
  1. Pull the contact shoe out.
  2. Set the dust removal adapter on the contact shoe mount.
  3. Insert the lightly greased contact shoe fully into the guide.

Operation

CAUTION
Risk of injury by short circuit or falling battery!
  • Before inserting the battery, make sure that the contacts on the battery and the contacts on the product are free of foreign matter.
  • Make sure that the battery always engages correctly.
Observe the safety instructions and warnings in this documentation and on the product.

Guiding the saw

Image alternative
  1. Hold the saw by the grips provided for the purpose.
  2. Guide the saw to the workpiece.
  3. Guide the saw forward and back.
    • If you press the saw against the workpiece there is a risk of the saw blade breaking and causing injuries.

Sawing

WARNING
Risk of injury by defective scaffold hook! A falling tool could injure you or others.
  • Before starting work, check that the scaffold hook is secure and undamaged.
Image alternative
  1. Disengage the transport lock and press the control switch.
    • The graphics section illustrates various ways of guiding the saw effectively.
  2. Release the control switch when you finish the cut.
  3. Engage the transport lock.

Removing the saw blade

Image alternative
CAUTION
Risk of injury! The accessory tool may be hot and/or have sharp edges.
  • Wear protective gloves when changing the accessory tool.
  • Never lay down a hot accessory tool on a flammable surface.
  1. Engage the transport lock or remove the battery from the power tool.
  2. Push the locking lever up as far as it will go and hold it in this position.
  3. Pull the blade forward out of the blade holder.
  4. Allow the locking lever to return to its original position.

Care and maintenance

WARNING
Risk of injury with battery inserted !
  • Always remove the battery before carrying out care and maintenance tasks!
Care and maintenance of the tool
  • Carefully remove stubborn dirt from the tool.
  • Clean the air vents carefully with a dry brush.
  • Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
  • Clean and lubricate the chuck from the outside at regular intervals. Use the Hilti spray 314648 for this purpose.
Care of the Li‑ion batteries
  • Keep the battery free from oil and grease.
  • Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
  • Avoid ingress of moisture.
Maintenance
  • Check all visible parts and controls for signs of damage at regular intervals and make sure that they all function correctly.
  • Do not operate the product if signs of damage are found or if parts malfunction. Have it repaired immediately by Hilti Service.
  • After cleaning and maintenance, fit all guards or protective devices and check that they function correctly.
To help ensure safe and reliable operation, use only genuine Hilti spare parts and consumables. Spare parts, consumables and accessories approved by Hilti for use with the product can be found at your local Hilti Store or online at: www.hilti.group .

Replacement of the contact shoe

The contact shoe can be replaced when necessary.
Image alternative
  1. Remove the battery.
  2. Remove the saw blade.
  3. Press the red release button for the contact shoe on the underside of the reciprocating saw.
  4. Pull the contact shoe out.
  5. Press the red release button for the contact shoe on the underside of the reciprocating saw.
  6. Insert the lightly greased contact shoe fully into the guide.
  7. Check that the contact shoe has engaged.

Transport and storage of cordless tools

Transport
    CAUTION
    Accidental starting during transport !
  • Always transport your products with the batteries removed!
  • Remove the battery.
  • Never transport batteries in bulk form (loose, unprotected).
  • Check the tool and batteries for damage before use after long periods of transport.
Storage
    CAUTION
    Accidental damage caused by defective or leaking batteries !
  • Always store your products with the batteries removed!
  • Store the tool and batteries in a place that is as cool and dry as possible.
  • Never store batteries in direct sunlight, on heating units or behind a window pane.
  • Store the tool and batteries in a place where they cannot be accessed by children or unauthorized persons.
  • Check the tool and batteries for damage before use after long periods of storage.

Troubleshooting

If the trouble you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, please contact Hilti Service.

The reciprocating saw is not in working order

Trouble or fault
Possible cause
Action to be taken
The tool doesn’t start.
The battery is not correctly inserted.
  • Push the battery in until it engages with a click.
The battery is empty.
  • Charge the battery.
The transport lock is engaged.
  • Disengage the transport lock.
The saw blade cannot be removed from the chuck.
The locking lever was not pushed as far as it will go.
  • Push the locking lever as far as it will go and remove the saw blade.
Chuck clogged by residues from sawing operations.
  • Remove the residues from sawing operations and regularly clean the chuck from the outside. Care of the power tool.

The reciprocating saw is in working order

Trouble or fault
Possible cause
Action to be taken
The tool does not develop full power.
The control switch is not fully pressed
  • Press the control switch fully.
The battery is discharged
  • Change the battery and charge the empty battery.
The saw blade cannot be removed from the chuck.
The locking lever was not pushed as far as it will go.
  • Push the locking lever as far as it will go and remove the saw blade.

Disposal

Image alternative Most of the materials from which Hilti tools and appliances are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to Hilti for recycling. Ask Hilti Service or your Hilti representative for further information.
Battery disposalImproper disposal of batteries can result in health hazards from leaking gases or fluids.
  • DO NOT send batteries through the mail!
  • Cover the terminals with a non-conductive material (such as electrical tape) to prevent short circuiting.
  • Dispose of your battery out of the reach of children.
  • Dispose of the battery at your Hilti Store , or consult your local governmental garbage disposal or public health and safety resources for disposal instructions.
Image alternative
  • Do not dispose of power tools, electronic equipment or batteries as household waste!

RoHS (Restriction of Hazardous Substances)

Click on the link to go to the table of hazardous substances: qr.hilti.com/r5962277.
There is a link to the RoHS table, in the form of a QR code, at the end of this document.

Manufacturer’s warranty

  • Please contact your local Hilti representative if you have questions about the warranty conditions.
Image alternative
Image alternative