Please note, the order volume has been updated. This is due to package and minimum order quantities.
Please note, the order volume has been updated to {0}. This is due to package and minimum order quantities.. This is due to package and minimum order quantities.
Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
Observe the safety instructions and warnings in this documentation and on the product.
Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
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
Draws attention to a potentially dangerous situation that could lead to slight personal injury or damage to the equipment or other property.
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
The following symbols are used on the product:
General mandatory sign
Wear eye protection
Wear ear protection
Wear a hard hat
Direct current (DC)
Product information
products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
The type designation and serial number are printed on the rating plate.
Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product. Product information
Fastening tool
BX 3 | BX 3-L
Generation
02
Serial no.
Declaration of conformity
We declare, on our sole responsibility, that the product described here complies with the applicable directives and standards. A copy of the declaration issued by the certification department can be found at the end of this documentation.
The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | 86916 Kaufering, Germany
Safety
General power tool safety warnings
WARNING
Read all safety warnings and all instructions. Failure to follow the warnings and instructions may result in electric shock, fire and/or serious injury.
Save all warnings and instructions for future reference. Work area safety
Keep work area clean and well lit. Cluttered or dark areas invite accidents.
Do not operate power tools in explosive atmospheres, such as in the presence of flammable liquids, gases or dust. Power tools create sparks which may ignite the dust or fumes.
Keep children and bystanders away while operating a power tool. Distractions can cause you to lose control.
Electrical safety
Avoid body contact with earthed or grounded surfaces, such as pipes, radiators, ranges and refrigerators. There is an increased risk of electric shock if your body is earthed or grounded.
Do not expose power tools to rain or wet conditions. Water entering a power tool will increase the risk of electric shock.
Personal safety
Stay alert, watch what you are doing and use common sense when operating a power tool. Do not use a power tool while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating power tools may result in serious personal injury.
Use personal protective equipment. Always wear eye protection. Protective equipment such as dust mask, non-skid safety shoes, hard hat, or hearing protection used for appropriate conditions will reduce personal injuries.
Prevent unintentional starting. Ensure the switch is in the off‐position before connecting to battery pack, picking up or carrying the tool. Carrying power tools with your finger on the switch or energising power tools that have the switch on invites accidents.
Remove any adjusting key or wrench before turning the power tool on. A wrench or a key left attached to a rotating part of the power tool may result in personal injury.
Do not overreach. Keep proper footing and balance at all times. This enables better control of the power tool in unexpected situations.
Dress properly. Do not wear loose clothing or jewellery. Keep your hair, clothing and gloves away from moving parts. Loose clothes, jewellery or long hair can be caught in moving parts.
If devices are provided for the connection of dust extraction and collection facilities, ensure these are connected and properly used. Use of dust collection can reduce dust-related hazards.
Power tool use and care
Do not force the power tool. Use the correct power tool for your application. The correct power tool will do the job better and safer at the rate for which it was designed.
Do not use the power tool if the switch does not turn it on and off. Any power tool that cannot be controlled with the switch is dangerous and must be repaired.
Disconnect the battery pack from the power tool before making any adjustments, changing accessories, or storing power tools. Such preventive safety measures reduce the risk of starting the power tool accidentally.
Store idle power tools out of the reach of children and do not allow persons unfamiliar with the power tool or these instructions to operate the power tool. Power tools are dangerous in the hands of untrained users.
Maintain power tools. Check for misalignment or binding of moving parts, breakage of parts and any other condition that may affect the power tool’s operation. If damaged, have the power tool repaired before use. Many accidents are caused by poorly maintained power tools.
Keep cutting tools sharp and clean. Properly maintained cutting tools with sharp cutting edges are less likely to bind and are easier to control.
Use the power tool, accessories and tool bits etc. in accordance with these instructions, taking into account the working conditions and the work to be performed. Use of the power tool for operations different from those intended could result in a hazardous situation.
Battery tool use and care
Recharge only with the charger specified by the manufacturer. A charger that is suitable for one type of battery pack may create a risk of fire when used with another battery pack.
Use power tools only with specifically designated battery packs. Use of any other battery packs may create a risk of injury and fire.
When battery pack is not in use, keep it away from other metal objects, like paper clips, coins, keys, nails, screws or other small metal objects, that can make a connection from one terminal to another. Shorting the battery terminals together may cause burns or a fire.
Under abusive conditions, liquid may be ejected from the battery; avoid contact. If contact accidentally occurs, flush with water. If liquid contacts eyes, additionally seek medical help. Liquid ejected from the battery may cause irritation or burns.
Service
Have your power tool serviced by a qualified repair person using only identical replacement parts. This will ensure that the safety of the power tool is maintained.
Tacker safety warnings
Always assume that the tool contains fasteners. Careless handling of the fastening tool can result in unexpected firing of nails causing personal injury.
Do not point the tool towards yourself or anyone nearby. A nail will be ejected by the tool if it is triggered unexpectedly, possibly leading to injury.
Do not actuate the tool unless the tool is placed firmly against the workpiece. If the tool is not in contact with the workpiece, the fastener may be deflected away from your target.
Disconnect the tool from the power source when the fastener jams in the tool. While removing a jammed fastener, the fastening tool may be accidentally activated if it is plugged in.
Use caution while removing a jammed fastener. The mechanism may be under tension and the nail may be forcefully ejected while attempting to free a jam.
When fastening electrical cables, make sure the cables are not energized. Hold the fastening tool only by insulated gripping surfaces. Use only fasteners designed for electrical cable installations. Check that the fastener has not damaged the insulation of the electrical cable. A nail that damages the insulation of electric cables can lead to electric shock and fire hazards.
Safety instructions
Basic information concerning safetyWARNING!Read all safety precautions and other instructions. Failure to observe the safety precautions and other instructions may result in electric shock, fire and/or serious injury.
Keep all safety precautions and instructions for future reference.
Requirements to be met by users
Only authorized, appropriately trained persons may operate or service this tool.
Personal protective equipment
You and any other persons in the vicinity must wear suitable eye protection and a hard hat while the tool is in use.
Wear ear protectors.
Exposure to noise can cause hearing loss.
Personal safety
Observe the information printed in the operating instructions concerning operation, care and maintenance.
Stay alert, watch what you are doing and use common sense when operating a direct fastening tool. Don’t use the tool when you are tired or under the influence of drugs, alcohol or medication. Take a break if you experience pain or feel unwell. A moment of inattention while operating tools may result in serious personal injury.
Avoid working in awkward body positions. Make sure you work from a safe stance and stay in balance at all times.
Wear non-skid shoes.
Never pull the fastener guide or fastener back with your hand.
Under certain circumstances, the tool could be made ready to fire by pulling the fastener guide or the fastener back by hand. When the tool is ready to fire, fasteners or the piston could be driven inadvertently into parts of the body.
Keep the arms slightly bent while operating the tool (do not straighten the arms).
Keep other people away from the working area, especially children.
Use and care of direct fastening toolsWARNING!Danger of fasteners penetrating right through. Before driving fasteners, check to make sure that no one is present behind or below the object into which the fastener is to be driven.
Before beginning the work, carry out a test by driving 2 fasteners into the material you are working on.
Use the right tool for the work you are carrying out. Do not use the tool for purposes for which it was not intended. Use it only as directed and when in faultless condition.
Never leave a loaded tool unattended.
Transport and store the tool in a secured toolbox.
Always unload the tool (remove fasteners) before cleaning, maintenance, changing the fastener guide, before work breaks and before storing the tool.
When not in use, the tool should be unloaded and stored in a locked, dry place where it is inaccessible to children.
Check the tool and the accessories for any damage. Check that moving parts function faultlessly, without sticking, and that no parts are damaged.
All parts must be fitted correctly and fulfill all conditions necessary for correct operation of the tool. Damaged parts must be properly repaired or replaced by Hilti Service unless otherwise stated in the operating instructions.
Before driving fasteners, check that there is no electrical wiring behind the surface on which you are working.
Do not attempt to drive fasteners into unsuitable materials.
Unsuitable materials include welded steel and cast steel, cast iron, glass, marble, plastic, bronze, brass, copper, insulating material, hollow brick, ceramic brick, thin sheet metal (< 4 mm) and cellular concrete. Driving a fastener into these materials may cause the fastener to break, shatter or to be driven right through.
Pull the trigger only when the tool is fully pressed against the working surface at right angles.
When driving fasteners, always hold the fastening tool at right angles to the working surface in order to prevent the fastener being deflected by the surface.
Keep the grips dry, clean and free from oil and grease.
Never drop the tool.
Do not use the magazine as a grip.
Do not use the tool in places where there is a risk of fire or explosion unless the tool is specially approved for this type of use.
Never drive fasteners into existing holes unless this is recommended by Hilti (e.g. DX-Kwik).
Workstation
Keep the workplace tidy. Objects which could cause injury should be removed from the working area.
Untidiness in the working area can lead to accidents.
Make sure that the working area is well lit and well ventilated.
Mechanical safety rules
Do not tamper with or modify the tool or parts of it, especially the piston.
Use only fasteners of a type approved for use with the tool.
Thermal safety rules
Do not exceed the recommended maximum fastener driving rate.
If the tool has overheated, allow it to cool down.
Do not dismantle the tool while it is hot. Allow the tool to cool down.
Battery use and care
Observe the special regulations and instructions applicable to the transport, storage and use of Li-ion batteries.
Do not expose batteries to high temperatures, direct sunlight or fire.
Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C.
Do not use or charge batteries that have suffered mechanical impact, have been dropped from a height or show signs of damage. In this case, always contact your HiltiService .
If the battery is too hot to touch it may be defective. In this case, place the product in a non-flammable location, well away from flammable materials, where it can be kept under observation and allowed to cool down. In this case, always contact your HiltiService .
Description
Overview of the product
Nosepiece
Fastener guide X-FG B3-ME 02
Fastener guide X-FG B3-IF 02
Fastener guide locking mechanism
Air vents
Safety trigger
Grip
Release buttons
Belt hook/scaffold hook
State of charge display
Li‑ion battery
Nail pusher, locked position
Nail pusher release mechanism
Support leg
Magazine
Status indicator
On/off button
Nail pusher, unlocked position
Intended use
The product is a hand-held, battery-operated fastening tool for indoor use. It is designed to drive specially-manufactured fasteners (nails) into concrete, steel, masonry, sand-lime block and other materials suitable for use of the direct fastening technique. The product is also designed to fasten electrical cables with clips if the appropriate fasteners are used. Use only approved fasteners in conjunction with the fastener guide designed for use with these specific fasteners (see “Technical data” section).
The fastening tool, battery and fasteners form a single technical unit. This means that trouble-free fastening can be ensured with this fastening tool only when it is used in conjunction with the
Hilti fasteners specially designed and manufactured for it and with the batteries and chargers recommended by
Hilti . The fastening and application recommendations made by
Hilti apply only when this condition is observed.
The fastening tool is for hand-held use only.
Misuse of the fastening tool must be ruled out. Misuse of the tool is understood to include driving fasteners into very soft materials (e.g. wood) or into excessively hard materials (e.g. high-strength steel or very hard natural stone).
Use only Hilti Li‑ion batteries of the B 22 series with this product.
Use only Hilti battery chargers of the C 4/36 series to charge these batteries.
Safety devices
When using the nail magazine, the nail detector prevents triggering without a nail loaded, which could damage the fastening tool.
The contact pressure safety device is intended to prevent the free flighting of nails (i.e. actuation and driving a nail when the nosepiece is not in contact with the workpiece). When using a nail magazine, the fastening tool can be pressed against the surface and triggered only when a nail is loaded in the tool.
Features
The fastening tool is equipped with an ergonomic, non-slip and vibration-absorbing grip, a belt and scaffold hook and a support leg. The tool is protected from overloading by electronic overload protection and from overheating by temperature monitoring.
Bluetooth
The product has a Bluetooth interface. Wireless communication via Bluetooth is possible as soon as the battery has been fitted and the fastening tool switched on at the on/off button.
Data transfer continues for three hours after the tool has switched to standby mode or after the tool has been switched off at the on/off button.
To deactivate Bluetooth manually, press and hold down the on/off button for at least 5 seconds until the LED shows blue twice.
When the battery is removed, no further data are transferred.
Bluetooth is not available in all markets.
Status indicator
The status indicator provides information about the status of the fastening tool.
Status
Meaning
Off
The fastening tool is switched off.
The LED lights green.
The fastening tool is switched on and ready for use.
The LED blinks green every 3 seconds.
The fastening tool is in stand-by mode. Press the nose of the tool against the working surface to switch it on.
The LED lights blue.
The fastening tool is switched on, nail strips require to be loaded.
LED blinks blue.
The fastening tool is switched on, the magazine is completely empty.
The LED blinks green.
The fastening tool is too hot or the battery has insufficient power. Please refer to “Troubleshooting”.
The LED blinks red.
Malfunction – please refer to “Troubleshooting”.
The LED lights red.
Malfunction – please refer to “Troubleshooting”.
Indication of battery charge status
When one of the battery release buttons is pressed the display indicates the battery’s state of charge.
Reliable indication of the charge status is not possible while a fastener is being driven or immediately after a fastener is driven.
Status
Meaning
All four LEDs light green.
Charge status is 75 % to 100 %.
Three LEDs light green.
Charge status is 50 % to 75 %.
Two LEDs light green.
Charge status is 25 % to 50 %.
One LED lights green.
Charge status is 10 % to 25 %.
One LED flashes green.
Charge status is below 10 %. The battery has insufficient power.
Items supplied
BX 3 or BX 3-L fastening tool, operating instructions.
You can find other system products approved for your product at your local
Hilti Center or online at:
www.hilti.com
Technical data, fastening tool
BX 3
BX 3-L
Weight
B 22/2.6 Li‑Ion (02)
8.8 lb (4.0 kg)
8.8 lb (4.0 kg)
B 22/3.0 Li‑Ion (01)
9.0 lb (4.1 kg)
9.0 lb (4.1 kg)
B 22/5.2 Li-Ion (01)
9.5 lb (4.3 kg)
9.5 lb (4.3 kg)
Nail length (collated nails)
0.6 in … 1.2 in (14 mm … 30 mm)
0.6 in … 1.4 in (14 mm … 36 mm)
Accessibility
2.0 in (52 mm)
1.8 in (46 mm)
Nail diameter
0.1 in (3 mm)
0.108 in … 0.12 in (2.75 mm … 3.0 mm)
Magazine capacity
30 nails
30 nails
Compression stroke
0.5 in (12 mm)
0.5 in (12 mm)
Contact pressure
11 lbf … 16 lbf (50 N … 70 N)
11 lbf … 16 lbf (50 N … 70 N)
Application temperature (ambient temperature)
5 ℉ … 122 ℉ (−15 ℃ … 50 ℃)
5 ℉ … 122 ℉ (−15 ℃ … 50 ℃)
Recommended maximum fastening rate
650/h
650/h
Rated voltage
21.6 V
21.6 V
Battery
Battery operating voltage
21.6 V
Ambient temperature for operation
1 ℉ … 140 ℉ (−17 ℃ … 60 ℃)
Storage temperature
−4 ℉ … 104 ℉ (−20 ℃ … 40 ℃)
Battery charging starting temperature
14 ℉ … 113 ℉ (−10 ℃ … 45 ℃)
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
In order to achieve maximum battery lifetime, replace the discharged battery with a fully charged battery as soon as you notice a clear drop in battery performance.
Check that the contacts on the battery and on the tool are free from foreign objects.
Fit the battery and make sure that it is heard to engage.
Once the battery has been fitted, the charge status LEDs light for a short time.
CAUTION
A falling battery presents a hazard. If the battery is not secured correctly it may drop out and fall while the work is in progress.
Always check that the battery is securely seated.
Check that the battery is securely seated in the fastening tool.
Slide the fastener guide locking catch as far as it will go in the direction of the arrow and hold it in this position.
Slide the fastener guide into the nosepiece until it is heard to engage.
Release the fastener guide locking catch.
The fastener guide jumps to the middle position.
Grip and pull the fastener guide to check that it is securely seated.
Working safely with the belt and scaffold hook
Before beginning work, make sure that the belt hook / scaffold hook is securely attached to the tool.
Use the belt hook / scaffold hook only when necessary. Lay the tool down in a safe place when it is not in use for a long period.
Loading for magazine operation
WARNING
Risk of crushing! Allowing the nail pusher to snap back under spring pressure may result in finger injuries and cause damage to the fastening tool.
When pulling the nail pusher down, take care to ensure that it engages securely. Do not allow the nail pusher to jump back under spring pressure.
Pull the nail pusher down until it engages.
Slide the nail strips into the magazine (a maximum of 3 strips of 10 nails).
Hold the nail pusher securely and press the nail pusher release button.
Guide the nail pusher back until it contacts a nail.
Types of work
Using the support leg
On an even working surface, the support leg makes it easier to hold the fastening tool perpendicular as attention then only has to be paid to lateral alignment. On uneven surfaces it may necessary to retract the support leg in order to ensure that the fastener guide is perpendicular to the working surface.
Retracting the support leg
Push against the support leg to release it from its resting position.
Pivot the support leg back through about 230°.
Push against the support leg from below until it engages in the retracted position.
Extending the support leg
CAUTION
Risk of pinching the fingers! When folding the support leg back there is a risk of trapping and pinching the fingers between the support leg and the casing of the tool.
Hold the fastening tool by the grip when extending/retracting the support leg.
Push against the support leg to release it from its resting position.
Pivot the support leg forward through about 230°.
Push against the support leg from below until it engages in the extended position.
Switching the fastening tool on/off
Switching the fastening tool on
WARNING
Risk of injury! Pressing the nosepiece of the fastening tool against a part of the body may lead to serious injury due to inadvertent firing and release of a fastener.
Never press the nosepiece of the tool against your hand or any other part of the body.
Press the on/off button.
The spring mechanism can be heard to build up tension and the status indicator lights green.
When battery performance drops, tensioning of the spring mechanism will take longer than with a fully charged battery.
Battery performance drops at low temperatures.
If you continue to operate the fastening tool after noticing a drop in battery performance, the fastening tool will switch itself off automatically before damage to the battery cells occurs.
Switching the fastening tool off
Press the on/off button.
The spring mechanism can be heard to release the tension and the status indicator goes out.
Driving a nail
WARNING
Risk of injury by flying parts! When driving a fastener, there is a risk of injury to the body and eyes caused by splintered fragments of the workpiece and by flying parts of the nail strip.
Wear personal protective equipment and always wear protective glasses and protective gloves. Other persons in the vicinity must also wear eye protection and a hard hat.
WARNING
Risk of injury! Pressing the nosepiece of the fastening tool against a part of the body may lead to serious injury due to inadvertent firing and release of a fastener.
Never press the nosepiece of the tool against your hand or any other part of the body.
Position the nose of the fastening tool at right angles to the working surface and then press it against the surface, pushing the fastener guide in as far as it will go.
Drive the nail by pressing the safety trigger.
Lift the fastening tool completely away from the working surface after driving a fastener.
The fastening tool switches itself off automatically if the fastener guide is pressed against the working surface for longer than 6 seconds without a nail being driven. The fastening tool can be switched on again by pressing the on/off button.
If the fastening tool is not used for 6 minutes, spring tension is relaxed and the fastening tool switches to stand-by mode automatically. The springs are automatically retensioned and the fastening tool becomes ready for use again as soon as it is pressed against the working surface.
If the fastening tool is left in stand-by mode for longer than three hours it switches itself off automatically. The fastening tool can be switched back on again by pressing the on/off button.
Switching off Bluetooth
Press the on/off button for at least 5 seconds until the LED shows blue twice.
No further data transfer is possible.
Bluetooth is not available in all markets.
Bluetooth can be deactivated if you are in a sensitive environment (e.g. a hospital) where use of Bluetooth is prohibited.
Removing a nail when in magazine mode
Pull the nail pusher down until it engages.
Slide the nail downwards out of the magazine.
Hold the nail pusher securely and press the nail pusher release button.
Guide the nail pusher back to its original position.
Jammed nails
Individual nails may get stuck in the fastener guide. You can remove jammed nails from the fastener guide with the aid of the X-NP drift punch set. Accessories are available from your
Hilti Center or can be ordered online at
www.hilti.com .
WARNING
There is a risk of injury and damage to the fastening tool. Use of unsuitable items instead of the recommended genuine
Hilti accessories may result in injury or damage to the fastening tool.
To release a jammed nail, use only the recommended drift punch set.
CAUTION
Risk of injury by flying parts! Triggering the tool (attempting to drive a fastener) when foreign objects are present in the area around the fastener guide, or when a fastener is jammed in the fastener guide, may lead to injury caused by flying objects or fragments.
Never attempt to remedy tool malfunctions by continuing to trigger the tool.
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
Do not operate the cordless tool if signs of damage are found or if parts malfunction. Have the tool repaired by Hilti Service immediately.
After cleaning and maintenance, fit all guards or protective devices and check that they function correctly.
To help ensure safe and reliable operation, use only genuine Hilti spare parts and consumables. Spare parts, consumables and accessories approved by Hilti for use with the product can be found at your local
Hilti Store or online at:
www.hilti.group | USA:
www.hilti.com
There is a delay before the spring mechanism is tensioned, the status indicator flashes blue and a signal tone is emitted simultaneously; the status indicator then lights blue for 6 minutes.
Most of the materials from which
Hilti tools and appliances are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to
Hilti for recycling. Ask
Hilti Service or your Hilti representative for further information.
Battery disposalImproper disposal of batteries can result in health hazards from leaking gases or fluids.
DO NOT send batteries through the mail!
Cover the terminals with a non-conductive material (such as electrical tape) to prevent short circuiting.
Dispose of your battery out of the reach of children.
Dispose of the battery at your Hilti Store , or consult your local governmental garbage disposal or public health and safety resources for disposal instructions.
Do not dispose of power tools, electronic equipment or batteries as household waste!
Manufacturer’s warranty
Please contact your local Hilti representative if you have questions about the warranty conditions.
FCC statement (applicable in US) / IC statement (applicable in Canada)
The product complies with part 15 of the FCC Rules and RSS‑210 of the IC.
Operation is subject to the following two conditions:
This device shall cause no harmful interference.
This device must accept any interference received, including interference that may cause undesired operation.
Changes or modifications not expressly approved by
Hilti may restrict the user’s authorization to operate the equipment.