SF 10W‑A22
Original operating instructions
Information about the documentation
About this documentation
- Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
- Observe the safety instructions and warnings in this documentation and on the product.
- Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
Explanation of symbols used
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the documentation
The following symbols are used in this document:![]() |
Read the operating instructions before use. |
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
Symbols in the illustrations
The following symbols are used in illustrations:![]() |
These numbers refer to the corresponding illustrations found at the beginning of these operating instructions |
![]() |
The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text |
![]() |
Item reference numbers are used in the overview illustrations and refer to the numbers used in the product overview section |
![]() |
This symbol is intended to draw special attention to certain points when handling the product. |
Product-dependent symbols
Symbols on the product
The following symbols are used on the product:![]() |
Rated speed under no load |
![]() |
Revolutions per minute |
![]() |
Active Torque Control (ATC) |
![]() |
Direct current (DC) |
![]() |
Li-ion battery |
![]() |
Hilti Li-ion battery type series used. Observe the information given in the section headed Intended use . |
![]() |
The power tool supports near-field communication (NFC) technology, which is compatible with iOS and Android platforms. |
![]() |
Never use the battery as a striking tool. |
![]() |
Do not drop the battery. Never use a battery that has suffered an impact or is damaged in any other way. |
Product information
Hilti products are designed for professional use and may be operated, serviced and maintained only by trained, authorized personnel. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
Product informationDrill/driver SF 10W‑A22 Generation 02 Serial no.
Declaration of conformity
We declare, on our sole responsibility, that the product described here complies with the applicable directives and standards. A copy of the declaration of conformity can be found at the end of this documentation.The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | 86916 Kaufering, Germany
Safety
General power tool safety warnings
![Image alternative](https://files-techDocs.hilti.com/2130485/H2_SYM-Hinweis_M_M_DEU_Gefahr.jpg)
Read all safety warnings and all instructions. Failure to follow the warnings and instructions may result in electric shock, fire and/or serious injury.
Save all warnings and instructions for future reference.
The term “power tool” in the warnings refers to your mains-operated (corded) power tool or battery-operated (cordless) power tool.
Work area safety
- Keep work area clean and well lit. Cluttered or dark areas invite accidents.
- Do not operate power tools in explosive atmospheres, such as in the presence of flammable liquids, gases or dust. Power tools create sparks which may ignite the dust or fumes.
- Keep children and bystanders away while operating a power tool. Distractions can cause you to lose control.
- Power tool plugs must match the outlet. Never modify the plug in any way. Do not use any adapter plugs with earthed (grounded) power tools. Unmodified plugs and matching outlets will reduce risk of electric shock.
- Avoid body contact with earthed or grounded surfaces, such as pipes, radiators, ranges and refrigerators. There is an increased risk of electric shock if your body is earthed or grounded.
- Do not expose power tools to rain or wet conditions. Water entering a power tool will increase the risk of electric shock.
- Do not abuse the cord. Never use the cord for carrying, pulling or unplugging the power tool. Keep cord away from heat, oil, sharp edges or moving parts. Damaged or entangled cords increase the risk of electric shock.
- When operating a power tool outdoors, use an extension cord suitable for outdoor use. Use of a cord suitable for outdoor use reduces the risk of electric shock.
- If operating a power tool in a damp location is unavoidable, use a residual current device (RCD) protected supply. Use of an RCD reduces the risk of electric shock.
- Stay alert, watch what you are doing and use common sense when operating a power tool. Do not use a power tool while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating power tools may result in serious personal injury.
- Use personal protective equipment. Always wear eye protection. Protective equipment such as dust mask, non-skid safety shoes, hard hat, or hearing protection used for appropriate conditions will reduce personal injuries.
- Prevent unintentional starting. Ensure the switch is in the off‐position before connecting to power source and/or battery pack, picking up or carrying the tool. Carrying power tools with your finger on the switch or energising power tools that have the switch on invites accidents.
- Remove any adjusting key or wrench before turning the power tool on. A wrench or a key left attached to a rotating part of the power tool may result in personal injury.
- Do not overreach. Keep proper footing and balance at all times. This enables better control of the power tool in unexpected situations.
- Dress properly. Do not wear loose clothing or jewellery. Keep your hair, clothing and gloves away from moving parts. Loose clothes, jewellery or long hair can be caught in moving parts.
- If devices are provided for the connection of dust extraction and collection facilities, ensure these are connected and properly used. Use of dust collection can reduce dust-related hazards.
- Do not force the power tool. Use the correct power tool for your application. The correct power tool will do the job better and safer at the rate for which it was designed.
- Do not use the power tool if the switch does not turn it on and off. Any power tool that cannot be controlled with the switch is dangerous and must be repaired.
- Disconnect the plug from the power source and/or the battery pack from the power tool before making any adjustments, changing accessories, or storing power tools. Such preventive safety measures reduce the risk of starting the power tool accidentally.
- Store idle power tools out of the reach of children and do not allow persons unfamiliar with the power tool or these instructions to operate the power tool. Power tools are dangerous in the hands of untrained users.
- Maintain power tools. Check for misalignment or binding of moving parts, breakage of parts and any other condition that may affect the power tool’s operation. If damaged, have the power tool repaired before use. Many accidents are caused by poorly maintained power tools.
- Keep cutting tools sharp and clean. Properly maintained cutting tools with sharp cutting edges are less likely to bind and are easier to control.
- Use the power tool, accessories and tool bits etc. in accordance with these instructions, taking into account the working conditions and the work to be performed. Use of the power tool for operations different from those intended could result in a hazardous situation.
- Recharge only with the charger specified by the manufacturer. A charger that is suitable for one type of battery pack may create a risk of fire when used with another battery pack.
- Use power tools only with specifically designated battery packs. Use of any other battery packs may create a risk of injury and fire.
- When battery pack is not in use, keep it away from other metal objects, like paper clips, coins, keys, nails, screws or other small metal objects, that can make a connection from one terminal to another. Shorting the battery terminals together may cause burns or a fire.
- Under abusive conditions, liquid may be ejected from the battery; avoid contact. If contact accidentally occurs, flush with water. If liquid contacts eyes, additionally seek medical help. Liquid ejected from the battery may cause irritation or burns.
- Have your power tool serviced by a qualified repair person using only identical replacement parts. This will ensure that the safety of the power tool is maintained.
Drill safety warnings
- Use auxiliary handle(s), if supplied with the tool. Loss of control can cause personal injury.
- Hold power tool by insulated gripping surfaces, when performing an operation where the cutting accessory may contact hidden wiring. Cutting accessory contacting a "live" wire may make exposed metal parts of the power tool "live" and could give the operator an electric shock.
Drill/driver safety warnings
- Hold power tool by insulated gripping surfaces, when performing an operation where the fastener may contact hidden wiring. Fasteners contacting a "live" wire may make exposed metal parts of the power tool "live" and could give the operator an electric shock.
Additional safety instructions
Personal safety- Tampering with or modification of the power tool is not permitted.
- Always hold the tool securely with both hands on the gripping section. Always grip the side handle at its outermost end. Keep the grips dry, clean and free from oil and grease. When drilling and screwdriving, the grip of the power tool may be deflected laterally (the power tool tends to pivot about its own axis).
- Avoid touching rotating parts. Switch the power tool on only after bringing it into position at the workpiece. Touching rotating parts, especially rotating accessory tools, may lead to injury.
- Activate the safety lock (forward/reverse selector switch in the middle position) when changing accessory tools or batteries and before storage or transportation of the power tool.
- Wear protective gloves. The drill/driver may get hot during use. There is a risk of injury (cutting or burning) if the accessory tool is touched while changing it.
- The user and any other persons in the vicinity must wear suitable eye protection, a hard hat, ear protection, protective gloves and breathing protection while the power tool is in use.
- Improve the blood circulation in your fingers by relaxing your hands and exercising your fingers during breaks between working.
- Dust from materials, such as paint containing lead, some wood species, concrete / masonry / stone containing silica, and minerals as well as metal, may be harmful. Contact with or inhalation of the dust may cause allergic reactions and/or respiratory or other diseases to the operator or bystanders. Certain kinds of dust are classified as carcinogenic such as oak and beech dust, especially in conjunction with additives for wood conditioning (chromate, wood preservative). Material containing asbestos may be handled only by specialists. Use a dust removal system whenever possible. To achieve a high level of dust collection, use a suitable vacuum cleaner. When indicated, wear a respirator appropriate for the type of dust generated. Ensure that the workplace is well ventilated. Follow national requirements for the materials you want to work with.
- Before beginning the work, check the hazard classification of the dust that will be produced. Use an industrial vacuum cleaner with an officially approved protection classification in compliance with locally applicable dust protection regulations.
- Working on the material may cause it to splinter. Wear eye protection. Flying fragments present a risk of injury to the body and eyes.
- The power tool is not intended for use by debilitated persons who have received no special training. Keep the power tool out of reach of children.
- Observe the national health and safety requirements.
- Before beginning work, check the working area (e.g. using a metal detector) to ensure that no concealed electric cables or gas and water pipes are present. External metal parts of the power tool may become live, for example, when an electric cable is damaged accidentally. This presents a serious risk of electric shock.
- Secure the workpiece. Use clamps or a vice to hold the workpiece in position. The workpiece is thus held more securely than by hand and both hands remain free to operate the power tool.
- Check that the accessory tools used are compatible with the chuck system and that they are secured in the chuck correctly.
- Use large, heavy accessory tools only with the power tool set to first gear. There is otherwise a risk of causing damage to the power when switching it off or, under unfavorable circumstances, the chuck may work loose.
- Do not use the battery as a power source for other unspecified appliances.
- Observe the special guidelines applicable to the transport, storage and use of Li-ion batteries.
- Do not expose batteries to high temperatures, the direct heat of the sun, and keep them away from fire. There is a risk of explosion.
- Do not disassemble, squash or incinerate batteries and do not subject them to temperatures over 80°C. This presents a risk of fire, explosion or injury through contact with caustic substances.
- Do not continue to use or attempt to charge damaged batteries (e.g. batteries with cracks, broken parts, bent or pushed-in / pulled-out contacts).
- If the battery is too hot to touch it may be defective. In this case, place the power tool in a non-flammable location, well away from flammable materials, where it can be kept under observation and allowed to cool down. Contact Hilti Service after the battery has cooled down.
Description
Overview of the product
![Image alternative](https://files-techDocs.hilti.com/2130485/H2_BILD-Objekt_System_SF_10W-A22-G2_DEU_SF10W_Uebersicht_P1_00.jpg)
- Side handle
- Keyless chuck
- Torque and drilling mode selector ring
- Gear selector switch
- Forward/reverse selector switch with safety lock
- Control switch (with electronic speed control)
- Grip
- Light to illuminate the work area
- Belt hook (optional)
- Li‑ion battery
- Battery release button
- State of charge and fault display (Li-ion battery)
Intended use
The product described is a hand-held cordless drill/driver. It is designed for driving and removing screws and for drilling in steel, wood and plastic.
Use only Hilti lithium‑ion batteries of the B 22 series with this product.
Use only Hilti -approved battery chargers to charge these batteries. More information is available from your Hilti Store or from www.hilti.group
ATC
The product is equipped with the ATC (Active Torque Control) quick-acting electronic cut-out.If the accessory tool sticks or stalls, the product will suddenly pivot about its own axis in the opposite direction. ATC detects this sudden pivoting movement of the product and switches the product off immediately.
Li‑ion battery display
The charge status of the Li-ion battery and malfunctions of the power tool are indicated by the display on the Li‑ion battery. The charge status of the Li‑ion battery is displayed after pressing one of the two battery release buttons.Status |
Meaning |
---|---|
4 LEDs light. |
Charge status: 75 % to 100 % |
3 LEDs light. |
Charge status: 50 % to 75 % |
2 LEDs light. |
Charge status: 25 % to 50 % |
1 LED lights. |
Charge status: 10 % to 25 % |
1 LED blinks, the power tool is ready for use. |
Charge status: < 10 % |
1 LED blinks, the power tool is not ready for use. |
The battery has overheated or is completely discharged. |
4 LEDs blink, the power tool is not ready for use. |
The power tool is overloaded or has overheated. |
Items supplied
Drill / driver, side handle, operating instructions.Other system products approved for use with this product can be found at your local Hilti Store or at: www.hilti.group
Technical data
Drill/driver
Rated voltage |
21.6 V |
|
Weight in accordance with EPTA Procedure 01 including B22⁄8.0 battery |
3.3 kg |
|
Speed |
1st gear |
0 /min … 310 /min |
2nd gear |
0 /min … 530 /min |
|
3rd gear |
0 /min … 1,210 /min |
|
4th gear |
0 /min … 2,100 /min |
|
Torque range (15 settings) |
2 Nm … 12 Nm |
|
Ø drill bit (softwood) |
1.5 mm … 50 mm |
|
Ø drill bit (hardwood) |
1.5 mm … 20 mm |
|
Ø drill bit (metal) |
1.5 mm … 13 mm |
Battery
Battery operating voltage |
21.6 V |
Ambient temperature |
−10 ℃ … 60 ℃ |
Storage temperature |
−20 ℃ … 40 ℃ |
Battery charging starting temperature |
−10 ℃ … 45 ℃ |
Noise information and vibration values determined in accordance with EN 60745
The sound pressure and vibration values given in these instructions have been measured in accordance with a standardized test and may be used to compare one electric tool with another. They may be used for a preliminary assessment of exposure.The data given represents the main applications of the electric tool. However, if the electric tool is used for different applications, with different accessory tools, or is poorly maintained, the data may vary. This may significantly increase exposure over the total working period.
An accurate estimation of exposure should also take into account the times when the power tool is switched off, or when it is running but not actually being used for a job. This may significantly reduce exposure over the total working period.
Prescribe additional safety measures to protect the operator from the effects of noise and/or vibration, for example: maintaining the power tool and accessory tools, keeping the hands warm, organization of work patterns.
Noise emission values
SF 10W-A22 |
|
---|---|
Emission sound pressure level (LpA) |
75 dB(A) |
Uncertainty for the sound pressure level (KpA) |
3 dB(A) |
Sound (power) level (LWA) |
86 dB(A) |
Uncertainty for the sound power level (KWA) |
3 dB(A) |
SF 10W-A22 |
|
---|---|
Vibration emission value for screwdriving (ah) |
< 2.5 m/s² |
Uncertainty for screwdriving (K) |
1.5 m/s² |
Drilling in metal (ah,D) |
< 2.5 m/s² |
Uncertainty for drilling in metal (K) |
1.5 m/s² |
Preparations at the workplace
Observe the safety instructions and warnings in this documentation and on the product.Inserting the battery
- Charge the battery fully before using it for the first time.
- Push the battery into the battery holder until it engages with an audible click.
- Check that the battery is seated securely.
Removing the battery
- Press the battery release buttons.
- Remove the battery from the tool.
Charging the battery
- Before charging the battery, read the operating instructions for the charger.
- Make sure that the contacts on the battery and the contacts on the charger are clean and dry.
- Use an approved charger to charge the battery.
Fitting the belt hook (optional)
![Image alternative](https://files-techDocs.hilti.com/2130485/H2_BILD-Objekt_System_SF_10W-A22-G2_DEU_SF10W_GuertelhakenMontieren_00.jpg)
- Fit the belt hook.
- Attach your power tool to the belt hook.
- Check that belt hook and power tool are secure.
Fitting the side handle
![Image alternative](https://files-techDocs.hilti.com/2130485/H2_BILD-Objekt_System_SF_10W-A22-G2_DEU_SF10W_SeitenhandgriffMontieren_00.jpg)
- Fit the side handle.
Adjusting the side handle
![Image alternative](https://files-techDocs.hilti.com/2130485/H2_BILD-Objekt_System_SF_10W-A22-G2_DEU_SF10W_SeitenhandgriffEinstellen_00.jpg)
- Adjust the side handle to the desired position.
Setting forward or reverse rotation
![Image alternative](https://files-techDocs.hilti.com/2130485/H2_BILD-Objekt_System_SF_10W-A22-G2_DEU_SF10W_R-L-Umschalter_00.jpg)
- Set the forward/reverse switch to the desired direction of rotation.
Types of work
Observe the safety instructions and warnings in this documentation and on the product.Fitting the accessory tool
- Set the forward/reverse switch to the middle position or remove the battery from the power tool.
- Check that the connection end of the accessory tool is clean. Clean the connection end if necessary.
- Open the keyless chuck.
- Insert the accessory tool in the keyless chuck and then turn the chuck firmly by hand until tight and several clicks are heard.
- Check that the accessory tool is held securely.
Selecting the gear
![Image alternative](https://files-techDocs.hilti.com/2130485/H2_BILD-Objekt_System_SF_10W-A22-G2_DEU_SF10W_Gangwahlschalter_00.jpg)
- Select the desired gear by adjusting the two gear selector switches.
Switching on
- Press the control switch.
Drilling
- Set the torque and operating mode selector ring to the
symbol.
- Set the forward/reverse switch to the “forward” position.
Screwdriving
- Set the torque and operating mode selector ring to the required torque.
- Set the forward/reverse switch to the desired direction of rotation.
Switching off
- Release the control switch.
Removing the accessory tool
- Set the forward/reverse switch to the middle position or remove the battery from the power tool.
- Open the keyless chuck.
- Pull the accessory tool out of the keyless chuck.
Care, maintenance, transport and storage
Care and maintenance
Care and maintenance of the tool- Carefully remove stubborn dirt.
- Clean the air vents carefully with a dry brush.
- Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
- Keep the battery free from oil and grease.
- Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as these may attack the plastic parts.
- Avoid ingress of moisture.
- Check all visible parts and controls for signs of damage at regular intervals and make sure that they all function correctly.
- Do not operate the product if signs of damage are found or if parts malfunction. Have it repaired immediately by Hilti Service.
- After cleaning and maintenance, fit all guards or protective devices and check that they function correctly.
Transport and storage of cordless tools
Transport- Remove the battery.
- Never transport batteries in bulk form (loose, unprotected).
- Check the tool and batteries for damage before use after long periods of transport.
- Store the tool and batteries in a place that is as cool and dry as possible.
- Never store batteries in direct sunlight, on heating units or behind a window pane.
- Store the tool and batteries in a place where they cannot be accessed by children or unauthorized persons.
- Check the tool and batteries for damage before use after long periods of storage.
Troubleshooting
If the trouble you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, please contact Hilti Service.Trouble or fault |
Possible cause |
Action to be taken |
---|---|---|
The power tool doesn’t run. |
The battery is not fully inserted. |
|
Low battery. |
|
|
The power tool doesn’t work and all four LEDs blink. |
The power tool has been overloaded briefly. |
|
The overheating cut-out has been activated. |
|
|
The power tool doesn’t work and one LED blinks. |
Low battery. |
|
The battery is too hot or too cold. |
|
|
The on/off button cannot be pressed, i.e. the button is locked. |
The forward/reverse selector switch is in the middle position. |
|
The battery runs down more quickly than usual. |
Very low ambient temperature. |
|
The battery doesn’t engage with an audible double click. |
The retaining lugs on the battery are dirty. |
|
The power tool or battery gets very hot. |
The tool is overloaded (application limits exceeded). |
|
Disposal
![Image alternative](https://files-techDocs.hilti.com/2130485/H2_SYM-Hinweis_M_M_DEU_Recycling_f.jpg)
Battery disposalImproper disposal of batteries can result in health hazards from leaking gases or fluids.
- DO NOT send batteries through the mail!
- Cover the terminals with a non-conductive material (such as electrical tape) to prevent short circuiting.
- Dispose of your battery out of the reach of children.
- Dispose of the battery at your Hilti Store , or consult your local governmental garbage disposal or public health and safety resources for disposal instructions.
Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.
![Image alternative](https://files-techDocs.hilti.com/2130485/H2_BILD-Objekt_System_SF_10W-A22-G2_DEU_Konform.jpg)