Get Hilti Discount CodesSave with our exclusive offers and promotionsView now

Powder-actuated nailer products

Shop versatile and ergonomic fastening tools

New

DX 6 MX Powder-actuated tool with magazine

DX 6 MX Powder-actuated tool with magazine

Fully automatic powder-actuated fastening tool with magazine for fastening collated nails
Shop

New

DX 6 Powder-actuated nailer kit

DX 6 Powder-actuated nailer kit

Fully automatic powder-actuated nailer – wall and formwork kit
Shop
DX 351 M&E Powder-actuated tool

DX 351 M&E Powder-actuated tool

Fully automatic, high-productivity, compact powder-actuated tool for mechanical and electrical fastenings
Shop
DX 351 MX Powder-actuated tool

DX 351 MX Powder-actuated tool

Fully automatic, high-productivity, compact powder actuated tool for fastening collated nails
Shop
DX 9-ENP powder-actuated decking tool

DX 9-ENP powder-actuated decking tool

Fully automatic, high-productivity, stand-up powder-actuated nailer for fastening metal decks
Shop
    MAN USING A HILTI DX 6

    What is a powder actuated tool?

    A powder actuated tool (PAT), also known as a powder actuated nailer, stands out as an exceptionally versatile direct fastening solution, embraced by tradesmen across all trades. As they are often lightweight, in comparison to other fastening tools, this makes them an ideal choice for various applications, especially in confined or overhead workspaces. These tools transfer the energy from the cartridge to the piston to deploy fasteners (e.g. nails, threaded studs) at speed into materials such as concrete, masonry and metal.

    PATs revolutionize the world of direct fastening, making it accessible for most, if not all, trades in the industry.

    MAN USING A HILTI DX TOOL

    What are powder actuated nailer tools used for?

    Powder actuated tools, owing to their versatility and productivity, present a superior fastening solution compared to traditional methods (e.g. drill-and-plug, manual screwing) when working with various materials. This method is highly trusted to handle substantial loads and ensures robust connections. Our product line includes both semi-automatic and fully automatic PATs, designed to excel in applications involving metal, wood, concrete and other materials. These also include tools equipped with magazines for repetitive fastening at speed, as well as single-nail option for precision.

    FAQS

    Application picture of DX 6 MX with 6.8/11 M10 cartridges, fastening membrane and steel washer

    How does a powder actuated nail gun tool work?

    A powder actuated tool or nailer works by producing high pressure gas, normally from a controlled explosive reaction using the ‘powder’ from the cartridge. This powers a piston which fires or deploys a fastener into a chosen material.

    DX 76 used on a metal roof application

    Are powder actuated tools safe to use?

    In essence, they are perfectly safe to use as long as you maintain and service your tools while also using them correctly. When using a powder actuated tool (PAT) for regular operation, they should work as intended. In addition, most modern nailers also incorporate safety features, such as pressure sensitive firing from a muzzle safety interlock to ensure the tool won’t go off when not being used.

    PATs also require training for operators using the tools due to the risks involved with it.

    DX 6 with P8 Piston assy, application on a jobsite

    Do you need training to use a powder actuated tool?

    Yes you do. In many regions formal training and/ or certification is required to operate a powder actuated tool. Especially as they operate using an explosive charge. As with any power tool, we would always recommend relevant safety training to protect you and those around you.

    Mood image of the Nuron   cordless nailer family BX 3-22 L and BX 3-22 ME

    What’s the difference between a powder actuated tool and a nail gun?

    What’s the difference between a powder‑actuated tool and a nail gun?

    While both tools are similar in how they are used in applications, there is a difference in how they operate:

    • Powder actuated tools and nailers

      use controlled explosive charges to deploy fasteners into a surface material.

    • A nail gun or battery nailer

      on the other handuses cordless battery power or compressed air to deploy fasteners into a surface material.