Robotic Total Stations

Learn more, compare your options and talk to our specialists
A robotic total station, sometimes known as a total station or automatic total station, helps site surveyors, engineers and other construction specialists with an array of early project tasks.

Why use a robotic total station?

One of the most crucial parts of any construction job is planning and plotting what’s on paper into the ground on site. As most projects face mounting costs and pressure, there is no margin for error when it comes to getting the groundwork and initial foundations right.

A robotic total station, sometimes known as a total station or automatic total station, helps site surveyors, engineers and other construction specialists with an array of early project tasks. These include boundary surveys, construction stakeout, setting out foundations, layout, laying out reference points from BIM plans, locating underground assets, structural monitoring and more.

One of the most compelling reasons to use a modern total station, such as those from Hilti, allow for single person operation – compared to other models or previous processes which required two-person operation. This saves resource for firms who may not have the capacity to have two people out on a job at any one time.

In addition, a robotic total station leaves no room for error when it comes to measurements and tracking. Making sure your projects start with accuracy and confidence.

When you buy from a premium construction company, you get so much more than just a top-of-the-range product.

Why choose Hilti total stations?

When you buy from a premium construction company, you get so much more than just a top-of-the-range product. You get peace of mind with a two-year warranty on the main layout tools, such as the PLT 300, PLT 400 and layout tablets. It’s also worth noting that our PLT 400 is the first construction layout tool with automatic levelling and site self-calibration, helping ensure you work with accuracy every time.

Our total stations are built to withstand the elements with IP 55 ratings for dust and water spray, while still operating between temperatures from minus 20 to 50 degrees. That means you can still get to work in sub-optimal conditions or environments and not lose time on site. In addition, our PROFIS Layout Office design software also makes preparing BIM data for the field easier than ever.

If you’re looking at options to get your hands on a robotic total station, you can choose to either purchase outright or lease these direct from Hilti with our Fleet Management approach.

Can I lease a Robotic Total Station?

Yes you can. If you’re looking at options to get your hands on a robotic total station, you can choose to either purchase outright or lease these direct from Hilti with our Fleet Management approach. This includes free unit calibration and repairs for the duration of the lease with fixed monthly costs.

In addition, our Fleet Management lease also includes theft coverage, where we cover up to 80% of costs of stolen tools and a free loan tool for whenever you send your PLT to us for repair - minimising downtime on site and making sure you always have a tool.

Total stations for construction surveys, measuring and more

PLT 300 Digital layout tool

PLT 300 Digital layout tool

Automated construction layout tool to speed-up jobsite stake-out using digital methods and BIM
ShopRequest more info
PLT 400-4 Construction layout tool

PLT 400-4 Construction layout tool

Versatile and easy-to-use construction layout tool for one-person operation, with 4" angle measurement accuracy and extended range for faster stake out of positions on the jobsite
ShopRequest more info
PLT 400-2 Construction layout tool

PLT 400-2 Construction layout tool

Versatile and easy-to-use construction layout tool for one-person operation, with 2" angle measurement accuracy and extended range for faster stake out of positions on the jobsite
ShopRequest more info

What’s the difference between total stations and a robotic total station?

While both terms are used to describe products in this area that do the same job, there is a big difference. Total stations will do everything that a robotic total station can do, but it needs two people to complete tasks – one at the base unit and another at any prism or reflector rod instruments where points are being marked or measured. A robotic total station on the other hand only needs one person to complete tasks, as once the base unit is set up it can be controlled remotely by a tablet or wireless control unit.

Total Station

Robotic Total Station

Minimum number of people required to operate

2

1

Can be used remotely – away from base unit?

No

Yes

Automatic prism tracking capabilities?

No. Requires manual intervention.No. Requires manual intervention.

Yes – can be initialised via remote control panel to target prism or fixing points

Everyday labour costs to operate

At least two people per project

Can just be one employee, unless more people involvedCan just be one employee, unless more people involved

Accuracy

High

High

Initial costs

Low-mid range

High outlay, though can save money on cheaper staff operating costs over time

Best use case scenarios

Small-mid range projects

Capable of handling all projects, including big infrastructure developments

FAQs

Application of the PLT 400 layout on interior jobsite

What is a robotic total station

A robotic total station is a device that is widely used in the construction industry to survey an area prior to, or during, construction. While old fashioned methods included the use of string and multiple people to measure distances on site, robotic total stations of today can be operated by one person using wireless connectivity to save time.

While this is a professional tool used by construction specialists, a robotic total station can be used to accurately measure or set-out key points on a job site. It can help to verify plans on the ground and measure points on a site to help gA robotic total station is a device that is widely used in the construction industry to survey an area prior to, or during, construction. While old fashioned methods included the use of string and multiple people to measure distances on site, robotic total stations of today can be operated by one person using wireless connectivity to save time. While this is a professional tool used by construction specialists, a robotic total station can be used to accurately measure or set-out key points on a job site. It can help to verify plans on the ground and measure points on a site to help ground teams work in the correct locations. round teams work in the correct locations.

Male topo field engineer doing a PLT 300 and PLC 400 training with male client on a jobsite

How to use a robotic total station

How you use a total station would potentially depend on the use or mode you’re using it for. The initial part of the setup for many jobs would be to mount and level the unit on a tripod or fixed point. Once set up, you would need to set or program the unit to its current location using co-ordinates or another fixed location(s) relative to where it is. Some devices, such as Hilti’s PLT 400-4, offer self-calibration to make the setup process easier.

Once you’ve set up your unit, and assuming you’re using an additional remote-control unit or tablet, connect your additional hardware to the total station via Wi-Fi or Bluetooth. This part of the setup could also include connecting prisms or reflection rods to the tablet and/or total station base unit - to help with measuring or layout tasks.

Then, assuming you either have plans to use as a reference or points to measure, you can set your robotic total station to the relevant mode such as measuring, set-out or plotting, while tracking your movements.

Once completed you can save changes on the device, or to the cloud, and then review on PC or laptop.

Asian Account Manager consulting with customer on jobsite holding tablet and showing a PLT 300 Digital Layout laser tool

How does a robotic total station work with a single operator?

The manual method of measuring and plotting a project would often require a surveyor to operate the base unit and position the reflector rods. Older methods would also include one or 2 surveyors using a ball of string to measure points while noting them down on drawings.

Modern total stations also work with reflector rods to help the base unit target and measure a distance between 2 points. However, with current robotic total stations users can also use a wireless tablet to see measurements, points and layout of a project in real time, without having to be physically present at the base unit – as it tracks the user and reflection rods autonomously. This enables single-person operation on a task, which saves resource and money that can be used elsewhere.

Client working on jobsite with his PLT 300 and PLC 400 tablet

What’s the difference between total stations and a robotic total station?

While both terms are used to describe products in this area that do the same job, there is a big difference. Total stations will do everything that a robotic total station can do, but it needs two people to complete tasks – one at the base unit and another at any prism or reflector rod instruments where points are being marked or measured. A robotic total station on the other hand only needs one person to complete tasks, as once the base unit is set up it can be controlled remotely by a tablet or wireless control unit. Please refer to the table above for more details.

Application picture of the ceiling and wall drilling robot JAIBOT with a PLT 300 layout tool on a construction site.

What are the advantages of using a robotic total station?

When it comes to measuring, set-out, layout and other tasks, there are a range of benefits when using a robotic total station:

  • Single person operation for tasks

  • Increased productivity – with only one person needed, frees up time for other employees

  • Reduced costs on resource

  • High accuracy vs manual and traditional methods

A total station PLT 400 in a construction site hall with wooden roof. In the background some jobsite workers and a Hilti representative

Are robotic total stations accurate?

Yes they are. While accurate in their own right, compared to traditional methods robotic total stations can offer pinpoint accuracy. Regular device calibration according to manufacturers spec is also recommended to maintain accurate readings each time.

Application picture of the PLT 400-22

Is a robotic total station worth the investment?

While the initial outlay to purchase or lease a robotic total station may be high, there are productivity gains which are worth considering. Especially if in the long run it saves money through the following ways:

  • Faster project completion – by using one person, rather than two, which frees resource for other project tasks

  • Lower people cost per task – by reducing the number of employees needed when using an RTS

  • Improved data quality – potentially compared to older methods of measurement, which reduces re-work and errors

  • Long-term return on investment – when used on several and large projects