VC 40H-X
VC 40H-XE
Original operating instructions
Information about the documentation
About this documentation
- Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
- Observe the safety instructions and warnings in this documentation and on the product.
- Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
Explanation of symbols
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the documentation
The following symbols are used in our documentation:![]() |
Read the operating instructions before use |
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
Symbols in the illustrations
The following symbols are used our in illustrations:![]() |
These numbers refer to the corresponding illustrations found at the beginning of these operating instructions |
![]() |
The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text |
![]() |
Item reference numbers are used in the overview illustrations and refer to the numbers used in the product overview section |
![]() |
This symbol is intended to draw special attention to certain points when handling the product. |
![]() |
Wireless data transfer |
Additional symbols
The following symbols are used on the product:![]() |
Transport by crane is not permissible. |
Product-dependent symbols
Symbols on the product
The following symbols are used on the product:![]() |
Warning: hot surface |
Special stickers on the product
H-class vacuum cleanersPeel the sticker with the appropriate national language wording from the sheet of stickers and affix it over the corresponding part of the warning sticker:![Image alternative](https://files-techDocs.hilti.com/2243106/H2_BILD-Objekt_System_VC_20-U-G3_DEU_Warnaufkleber_SaugerH.jpg)
Product information
![Image alternative](https://files-techDocs.hilti.com/2243106/H2_SYM-Logo_M_M_DEU_Hilti-Logo.jpg)
The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
Product informationWet / dry vacuum cleaner VC 40H-X
VC 40H-XEGeneration 01 Serial no.
Declaration of conformity
We declare, on our sole responsibility, that the product described here complies with the applicable directives and standards. A copy of the declaration of conformity can be found at the end of this documentation.The technical documentation is filed and stored here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | D-86916 Kaufering, Germany
Safety
General safety instructions
In addition to the safety instructions given in the various sections of these operating instructions, the following points must be strictly observed at all times.- Read all the instructions. Failure to follow all the instructions listed below may result in electric shock, fire and/or serious injury.
- If the appliance is used in conjunction with an electric tool, read and follow the operating instructions for the electric tool and all the warnings.
- Modification of the appliance is not permitted.
- Use the right appliance for the job. Do not use the appliance for purposes for which it was not intended. Use it only as directed and when in faultless condition.
- Before beginning work with the appliance, find out how to operate it correctly and about any hazards associated with the materials it will be picking up and how these materials can be disposed of.
- Take the influences of the surrounding area into account. Do not use the appliance where there is a risk of fire or explosion.
- Store appliances in a secure place when not in use. When not in use, appliances must be stored in a dry, high place or locked away out of reach of children.
- Only persons who are familiar with it, who have been trained on how to use it safely and who understand the resulting hazards are permitted to use the device. The device is not intended for use by children.
- Children must receive instruction and be supervised to ensure that they do not play with the appliance.
Personal safety
- Stay alert, watch what you are doing and use common sense when working with the product. Do not use the vacuum cleaner while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating the appliance may result in serious personal injury.
- The user and any other persons in the vicinity must wear suitable eye protection, a hard hat, ear protection, protective gloves, safety footwear and breathing protection while the appliance is in use or while maintenance work on it is being carried out.
- Engage the wheel brakes so that the tool stands securely. If the wheel brakes are not locked, the tool can begin to roll unchecked.
- If devices are provided for the connection of dust extraction and collection facilities, ensure these are connected and properly used. Use of a vacuum cleaner can reduce dust-related hazards.
Use and care of the appliance
- Never leave the appliance unattended.
- Do not deactivate the filter cleaning system when picking up hazardous dusts, especially when the appliance is used in conjunction with electric tools that generate dust.
- Protect the appliance from frost.
- Clean the water level limiting device regularly with a brush, in accordance with the instructions, and check it for signs of damage.
- When fitting the top section of the vacuum cleaner, take care to avoid pinching your fingers or damaging the supply cord. This presents a risk of injury or damage.
- Check the appliance and its accessories for any damage. Guards, safety devices and any slightly damaged parts must be checked carefully to ensure that they function faultlessly and as intended. Check that moving parts function faultlessly, without sticking, and that no parts are damaged. In order to ensure faultless operation of the appliance, all parts must be fitted correctly and must meet the necessary requirements.
- Have the appliance serviced by a qualified repair person using only genuine Hilti spare parts. The safety of the appliance can thus be maintained.
- Always unplug the supply cord from the power outlet when the appliance is not in use (during breaks), before cleaning and maintenance and before changing the filter or accessories. This preventive safety measure reduces the risk of starting the appliance accidentally.
- Never pull the vacuum cleaner by the supply cord to a new working position. Do not run the wheels of the vacuum cleaner over the supply cord.
- Do not transport the appliance by crane.
- Close the hose inlet socket with the cap before transporting the appliance and when it is not in use.
Electrical safety
- The plug on the supply cord of the appliance must match the outlet. Do not change the plug in any way. Do not use adapter plugs with earthed (grounded) appliances. Unmodified plugs and matching outlets reduce risk of electric shock.
- Insert the plug in a suitable earthed/grounded power outlet which has been correctly and safely installed and is in compliance with local regulations. If you are in doubt about the effectiveness of the power outlet’s earth/ground connection, have it checked by a qualified specialist.
- Avoid body contact with earthed or grounded surfaces such as pipes, radiators, cookers, stoves and refrigerators. There is an increased risk of electric shock if your body is grounded.
- Do not expose the appliance to rain or wet conditions. Water entering an electric appliance will increase the risk of electric shock.
- Check to ensure that the supply cord does not lie in a puddle of water.
- Check the appliance’s supply cord at regular intervals and have it replaced by Hilti Service if damage is found. Check extension cords at regular intervals and replace them if found to be damaged.
- Do not touch the supply cord or extension cord if they are damaged while working. Disconnect the supply cord plug from the power outlet. Damaged supply cords or extension cords present a risk of electric shock.
- The electric supply cord may be replaced only with a cord of the type specified in the operating instructions.
- Do not abuse the cord. Never use the cord for carrying, pulling or unplugging the appliance. Keep the cord away from heat, oil, sharp edges or moving parts. Damaged or entangled cords increase the risk of electric shock.
- When operating an electric appliance outdoors, use only extension cords of a type suitable for outdoor use. Use of an extension cord suitable for outdoor use reduces the risk of electric shock.
- In the event of an interruption in the electric supply, switch the appliance off and unplug it from the power outlet.
- Use the power outlet on the appliance only for the purposes described in the operating instructions.
- Never operate the appliance when it is dirty or wet. Dust (especially dust from conductive materials) or dampness adhering to the surface of the appliance may, under unfavorable conditions, lead to electric shock. Dirty or dusty appliances should thus be checked by Hilti Service at regular intervals, especially if used frequently for working on conductive materials.
Workplace
- Ensure that the workplace is well lit.
- Ensure that the workplace is well ventilated. Exposure to dust at a poorly ventilated workplace may result in damage to the health.
- Keep the workplace tidy. Objects which could cause injury should be removed from the working area. Untidiness at the workplace can lead to accidents.
- Do not operate the appliance in explosive atmospheres, such as in the presence of flammable liquids, gases or dust. Electric appliances cause sparks which may ignite the dust or fumes.
- Use extra care when working on stairs.
- Make sure that the air exchange rate L in the room is adequate if the spent air is vented into the room. Comply with the regulations applicable in the country in which the appliance is used.
The material picked up
- Do not use the device to vacuum up flammable and/or explosive dusts (magnesium or aluminum dust etc.) or dusts that constitute a health hazard. Do not use the appliance to vacuum up materials hotter than 60 °C (140 °F) (e.g. glowing cigarettes, hot ash).
- Do not use the appliance to pick up flammable, explosive or aggressive liquids (coolants and lubricants, gasoline, solvents, acids (pH < 5), alkalies (pH > 12.5), etc.).
- Switch the appliance off immediately if foam or liquids escape from it.
- Wear protective gloves when using the appliance to pick up hot materials at temperatures up to 60 °C (140 °F).
- When working with mineral drilling slurry, wear protective clothing and avoid skin contact with the slurry (pH > 9: caustic).
- Avoid contact with alkaline or acidic liquids. If contact accidentally occurs, rinse with water. In the event of the liquid coming into contact with the eyes, rinse the eyes with plenty of water and consult a doctor.
- The appliance is suitable for the vacuum pick-up of dry, non-flammable dusts, wood chips and hazardous dusts of EN 60335-2-69 dust class H. Do not operate the appliance without filter when picking up class H hazardous dusts.
- Do not use the appliance to wet-vacuum hazardous substances.
- When carrying out maintenance work, always wear a P2 or higher-classification dust mask and a disposable oversuit.
- Collected dust must be transported in dust-tight containers. Transfer of dust from one container to another is not permissible. Waste containing asbestos must be disposed of in accordance with the regulations and rules for waste disposal.
- Once removed, the main filter element cannot be re-used. Only persons with expert knowledge are permitted to replace permanently installed filters and the work must be carried out in a suitable environment, e.g. at a decontamination station. Dispose of the used filter in accordance with the applicable regulations.
Description
Product overview
![Image alternative](https://files-techDocs.hilti.com/2243106/H2_BILD-Objekt_System_VC_20-U-G3_DEU_VCUH_Uebersicht.jpg)
- Power outlet on the appliance (only VC 40H-XE)
- Automatic filter cleaning
- Filter cleaning ON/OFF button
- "Automatic filter cleaning system" status indicator
- Control switch
- Intake fitting
- Waste material container
- Grip recess
- Catch
- Suction head
- Grip
- Supply cord hook
- Catch for filter cover with safety screw
Intended use
The products described here are industrial vacuum cleaners designed for universal, commercial use. They may be used for wet or dry applications.
Use of the product to clean down persons or animals is not permissible. Underwater use is not permissible.The product is suitable for vacuuming dry, non-flammable, hazardous dusts of dust class H in accordance with EN 60335-2-69. In the Federal Republic of Germany, the provisions of Technical Rule for Hazardous Substances TRGS 519 apply for asbestos applications. Always comply with the regulations of the country in which the device is used.
-
Special safety instructions:
Comply with the applicable national accident prevention regulations when working with H-class vacuum cleaners.
After being used in an asbestos application in the "black" partitioned-off zone, a H-class vacuum cleaner cannot subsequently be used in the "white", or uncontaminated, zone.
Exceptions are permissible only after the H-class vacuum cleaner has been decontaminated completely (i.e. also cooling space, installation spaces for electrical equipment, the equipment itself, etc.) by a person with expert knowledge in accordance with TRGS 519 Nr. 2.7. Decontamination must be recorded in writing and signed off by the person with expert knowledge.H-class vacuum cleaners must be serviced as necessary, but at least once a year. and if necessary repaired, and tested by a person with expert knowledge (qualification in accordance with TRGS 519 Nr. 5.3, Abs. 2. The test result must be produced on request.
Waste containing asbestos must be disposed of in accordance with the regulations and rules for waste disposal.
-
This product is suitable for the following applications in commercial use:
Collecting large quantities of dust from Hilti diamond grinders, diamond cutters, rotary hammers and core drilling machines using dry-cutting core bits.
Vacuum pick-up of mineral drilling slurry with Hilti diamond core bits and Hilti diamond saws and liquid material up to a temperature < 60 °C (140 °F).
Vacuum pick-up of oil and liquid media up to a temperature < 60 °C (140 °F).
Wet and/or dry cleaning of wall and floor surfaces
Possible misuse
- Do not operate the industrial vacuum cleaner when it is laid on its side.
- Do not use the industrial vacuum cleaner to pick up substances that present a risk of explosion, glowing, burning or flammable substances or aggressive dusts (e.g. magnesium or aluminum dust, etc.) (exception: wood chips or shavings).
- Do not use the industrial vacuum cleaner to pick up flammable liquids (e.g. gasoline, solvents, coolants and lubricants, etc.).
Items supplied
Wet/dry vacuum cleaner including filter element, suction hose complete with rotatable connector (at the vacuum cleaner end) and connector for accessories, PE VC 20/40 plastic dust bag, operating instructions.Warning tone
Class M and class H vacuum cleaners feature an acoustic warning. The warning tone is emitted for safety reasons when the air speed in the hose drops below 20 m/s.In order to ensure that the warning tone is emitted correctly, the hose diameter setting must be set to the diameter of the suction hose in use.
Automatic filter cleaning
The vacuum cleaner is equipped with an automatic filter cleaning system that removes most of the dust adhering to the filter element.The filter cleaning system can be switched off by pressing the “Automatic filter cleaning ON/OFF” button and switched back on by pressing the button again.
Status |
Meaning |
---|---|
LED lights. |
The filter cleaning system is active. |
LED doesn’t light. |
The filter cleaning system is not active. |
The filter element is cleaned automatically by a blast of air (a pulsating noise is heard).
Instructions for use
Accessories and how they are usedAccessories |
Item number |
Type of use |
---|---|---|
VC 40H-XE dust bag |
2250854 |
Mineral-materials use, wet and dry (for VC 40H-X and VC 40H-XE) |
HEPA filter |
2240481 |
Special filter for applications with dust class H |
Suction hose, 27 x 3.5 m AS |
203865 |
Wet and dry |
Suction hose, 36 mm |
203866 |
Mainly wet, not for dust |
Suction hose, 36 x 5 m AS |
203867 |
Wet and dry |
- It is essential to use a safety filter bag and a corresponding filter when vacuuming dust that contains asbestos.
Technical data
Product properties
VC 40H-X |
VC 40H-XE |
|
---|---|---|
Dimensions (L x W x H) |
505 mm x 380 mm x 610 mm |
505 mm x 380 mm x 610 mm |
Weight in accordance with EPTA procedure 01 |
14.6 kg |
14.6 kg |
Container capacity |
36 ℓ |
36 ℓ |
Effective dust capacity |
40 kg |
40 kg |
Water capacity |
25 ℓ |
25 ℓ |
Operating temperature |
−10 ℃ … 40 ℃ |
−10 ℃ … 40 ℃ |
Automatic filter dedusting (interval) |
15 s |
15 s |
Protection class |
I |
I |
Protection class |
IP X4 |
IP X4 |
AC frequency |
50 Hz … 60 Hz |
50 Hz … 60 Hz |
Rated voltage
Overview, 110 V to 240 VRated voltage |
110 V (GB) |
220 V … 240 V |
220 V … 240 V (CH) |
220 V … 240 V (NZ) |
---|---|---|---|---|
Rated power input |
1,100 W |
1,200 W |
||
Power rating of power outlet on the appliance (optional) |
·/· |
2,400 W |
1,100 W |
1,200 W |
Mains connection (type) |
H07BQ-F 3G 1.5 mm² |
H07RN-F 3G 1.5 mm² |
Maximum volumetric flow rate and maximum vacuum
VC 40H-X |
VC 40H-XE |
||
---|---|---|---|
Maximum volumetric flow rate (Turbine data) |
1100 W |
68 ℓ/s |
68 ℓ/s |
1200 W |
74 ℓ/s |
74 ℓ/s |
|
Maximum volumetric flow rate (air) |
1100 W |
134 m³/h |
134 m³/h |
1200 W |
146 m³/h |
146 m³/h |
|
Maximum partial vacuum |
1100 W |
229 hPa |
229 hPa |
1200 W |
249 hPa |
249 hPa |
Noise and vibration information (measured in accordance with EN 60335)
The following information applies to all VC 20 and VC 40 industrial vacuum cleaners.Emission sound pressure level (LpA) |
73 dB(A) |
Uncertainty for the sound pressure level (KpA) |
2.5 dB(A) |
Vibration emission value |
< 2.5 m/s² |
Use of extension cords
- Use only extension cords of a type approved for the application and with conductors of adequate gauge.
- Do not use extension cords with a conductor cross section of less than 1.5 mm2.
- When working outdoors, use only extension cords that are approved and correspondingly marked for this application.
- Check the extension cord for damage at regular intervals.
- Replace damaged extension cords.
Before use
Inserting the PE disposal bag
![Image alternative](https://files-techDocs.hilti.com/2243106/H2_BILD-Objekt_System_VC_20-U-G3_DEU_VC150_020.jpg)
- Disconnect the supply cord plug from the power outlet.
- Open the two catches.
- Lift the vacuum cleaner top section away from the waste material container.
- Secure a new PE disposal bag in the waste material container.
- Fit the vacuum cleaner top section onto the waste material container and close the two catches.
Inserting/changing the dust bag (for dust class H applications)
![Image alternative](https://files-techDocs.hilti.com/2243106/H2_BILD-Objekt_System_VC_20-U-G3_DEU_VC150_020_UH.jpg)
- Disconnect the supply cord plug from the power outlet.
- Open the two catches.
- Lift the vacuum cleaner top section away from the waste material container.
- Close the dust bag with a cable tie positioned below the felt vent opening.
- Remove the dust bag.
- Clean the waste material container with a cloth.
- Fit a new dust bag in the waste material container.
- Fit the vacuum cleaner top section onto the waste material container and close the two catches.
Inserting the safety filter bag (for asbestos applications)
- Open the two catches.
- Lift the vacuum cleaner top section away from the waste material container.
- Insert the safety filter bag.
- Draw the safety filter bag over the container.
- Insert the adapter of the safety filter bag into the holder.
- Fit the vacuum cleaner top section onto the waste material container and close the two catches.
- Check to ensure that the vacuum cleaner top section is fitted correctly and secured.
Removing/changing the safety filter bag (for asbestos applications)
- Release the vacuum cleaner top section.
- Pull the safety filter bag up at the flange.
- Seal the intake of the safety filter bag.
- Draw the safety filter bag up and close off the vent hole with the adhesive tab.
- Use the cable tie affixed to the safety filter bag to close it securely.
- Dispose of the dust-tight bag in accordance with the applicable regulations.
- Dispose of the dust-tight bag in accordance with the applicable regulations.
- Clean the waste material container with a cloth.
Operation
Operation without use of the electric tool power outlet
- Check that the switch on the appliance is in the “OFF” position off before plugging the supply cord into a power outlet.
- Plug the vacuum cleaner’s supply cord into the power outlet.
- Turn the control switch to the “ON” position.
Operation with use of the power outlet on the appliance
- Unplug the vacuum cleaner’s supply cord from the power outlet.
- Check that the maximum power drawn by the electric tool is below the maximum permissible output of the power outlet on the vacuum cleaner (please refer to the “Technical data” section of the operating instructions and information printed at the power outlet on the appliance).
- Check to ensure that the electric tool is switched off before plugging its supply cord into the power outlet.
- Plug the electric tool’s supply cord into the power outlet on the vacuum cleaner.
- Plug the vacuum cleaner’s supply cord into the power outlet.
- Turn the control switch to the “Auto” position.
- Switch on the power tool.
Picking up dry dust
- Check that the filter element is dry and that the correct type of dust bag is fitted.
Picking up liquids
- Check the container level monitoring system.
- If possible, use a separate filter element for wet applications.
- After picking up liquids, open the two catches.
- Lift the vacuum cleaner top section away from the waste material container and place it on a level surface so that the filter element can dry.
- Empty the waste material container and use a water hose to rinse it out. Use a brush to clean the electrodes and clean the filter element, after allowing it to dry, by wiping it off with your hand.
- Allow the waste material container to dry.
After use of the vacuum cleaner
- Switch off the electric tool.
- Turn the vacuum cleaner control switch to the “OFF” position.
- Unplug the vacuum cleaner’s supply cord from the power outlet.
- Coil up the supply cord and hang it on the hook.
- Empty the container and clean the appliance by wiping it with a damp cloth.
- Coil up the suction hose.
- Store the vacuum cleaner in a secure, dry place where it is inaccessible to unauthorized users.
Emptying the waste material container when no dust bag is fitted (picking up liquids)
- Disconnect the supply cord plug from the power outlet.
- Lift the vacuum cleaner top section away from the waste material container and place it on a level surface.
- Grip the waste material container by the recess provided and empty it by tipping out the contents.
- Clean the edge of the waste material container with a cloth.
- Fit the vacuum cleaner top section onto the waste material container and close the two catches.
Care and maintenance
Care and maintenance of the appliance
- Keep the appliance, especially its grip surfaces, clean and free from oil and grease. Do not use cleaning agents containing silicone.
- Never operate the vacuum cleaner when the air vents are blocked. Clean the air vents carefully using a dry brush. Do not permit foreign objects to enter the interior of the appliance.
- Clean the outer surfaces of the appliance with a slightly damp cloth at regular intervals. Do not use a spray system, pressure jet washer or running water for cleaning as this may negatively affect the electrical safety of the appliance.
- Use filtered forced ventilation.
- Wear personal protective equipment.
- Clean the maintenance area in a way that prevents hazardous substances escaping into the surrounding environment.
- Vacuum off the outer surfaces of the appliance and wipe it clean or seal it in a suitable container, e.g. large plastic bag, before removing it from an area contaminated with hazardous substances. This will help to avoid distribution of the hazardous dust deposited on it.
- When maintenance or repairs are carried out, all contaminated parts which cannot be satisfactorily cleaned must be packed in impermeable bags and disposed of in compliance with the applicable disposal regulations.
- The appliance must be subjected to a technical inspection by Hilti Service or a trained person at least once a year to check, for example, for damage to the filter, air leakage, and to ensure correct operation of controlling devices.
- In addition, the filter efficiency of H-class vacuum cleaners has to be tested at least once a year or possibly more frequently if so required by country-specific regulations. The procedure for verifying the filter efficiency of the vacuum cleaner is set out in 22.AA.201.2. If failed, the test has to be repeated with a new main filter installed.
Automatic filter cleaning
The condition of the filter element deteriorates with use.- Replace the filter element at least every six months.
- However, if used intensively, the filter element should be replaced more often.
Changing the filter element
- Disconnect the supply cord plug from the power outlet.
- Slacken the securing screw of the filter cover.
- Open the filter cover.
- Carefully remove the filter element, gripping it at the areas provided in the holder.
- Immediately place the filter in a dust-tight bag.
- Dispose of the filter in the sealed bag in accordance with the applicable regulations.
- Dispose of the filter in the sealed bag in accordance with the applicable regulations.
- Clean the filtered-gas side and the sealing surface in the vacuum cleaner.
- Fit the new filter element.
- Close the filter cover by flipping the cover catch forward.
- Fit the fastening screw.
Checking the container level monitoring system
![Image alternative](https://files-techDocs.hilti.com/2243106/H2_BILD-Objekt_System_VC_20-U-G3_DEU_VC150_060.jpg)
- Engage the wheel brakes so that the vacuum cleaner stands securely.
- Disconnect the supply cord plug from the power outlet.
- Open the two catches.
- Lift the vacuum cleaner top section away from the waste material container and place it on a level surface.
- Check the cut-out contacts and clean them with a brush if necessary (if dirty).
- Check the seal at the vacuum cleaner top section and clean it with a cloth if necessary.
- Fit the vacuum cleaner top section onto the waste material container and close the two catches.
Checks after cleaning and maintenance
- After cleaning or carrying out maintenance, check that the vacuum cleaner is assembled correctly and that it functions faultlessly.
- Test each of the functions.
Transport and storage
Transport
Do not attempt to carry the device when it is full of waste material.Do not attempt to crane-lift the device.
- Remove the power conditioner and all loose accessory tools from the cradle.
- Empty the device before carrying it to another location.
- Do not tilt the device or transport it lying on its side after using it to pick up liquids.
- Use the tapered adapter to connect both ends of the hose together conveniently for transport.
- Place the suction hose in the transport bag provided for the purpose and seal the transport bag.
- Seal the suction intake.
- Remove the suction tube with floor nozzle from the holder. Carry the appliance by the carrying handle, not the pushbar.
Storage
- Store the vacuum cleaner in a secure, dry place where it is inaccessible to unauthorized users.
Troubleshooting
If the trouble you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, please contact Hilti Service.Troubleshooting table
Malfunction |
Possible cause |
Action to be taken |
---|---|---|
Class M and class H vacuum cleaners: Acoustic warning (of reduced suction) |
The dust bag is full. |
|
The filter element is clogged with dirt or dust. |
|
|
The suction hose or dust hood on the electric tool is blocked. |
|
|
The hose diameter setting is incorrect. |
|
|
Dust is blown out of the appliance. |
The filter element is not fitted correctly. |
|
The filter element is damaged. |
|
|
The appliance switches itself off or on inadvertently or static electricity discharges through the user. |
Electrostatic charge is not conducted away – the appliance is connected to an unearthed/ungrounded power outlet. |
|
The appliance doesn’t start or switches itself off after a short time. |
The water level cut-out is activated. |
|
The motor doesn’t restart. |
The mains circuit breaker has been tripped. |
|
The waste material container is full. |
|
|
The motor overheating protection cut-out has been activated. |
|
|
The motor is repeatedly switched off by its thermal cut-out. |
|
|
The motor doesn’t run when set to “AUTO”. |
The appliance is faulty or is not correctly plugged in. |
|
The automatic filter element cleaning system doesn’t work. |
No suction hose is connected. |
|
Disposal
![Image alternative](https://files-techDocs.hilti.com/2243106/H2_SYM-Hinweis_M_M_DEU_Recycling_f.jpg)
In accordance with the European Directive on waste electrical and electronic equipment and its implementation in conformance with national law, electric tools or appliances that have reached the end of their life must be collected separately and returned to an environmentally compatible recycling facility.
Drilling slurryDisposal of drilling slurry directly into rivers, lakes or the sewerage system without suitable pretreatment presents environmental problems.
- Ask the local public authorities for information about current regulations.
- Collect the drilling slurry (for example, using a wet-type vacuum cleaner).
- Allow the drilling slurry to settle and dispose of the solid material at a construction waste disposal site (addition of a flocculent may accelerate the settling process).
- The remaining water (alkaline, pH value greater than 7) must be neutralized by the addition of an acidic neutralizing agent or diluted with a large volume of water before it is allowed to flow into the sewerage system.
- Dispose of the drilling dust collected by the vacuum cleaner in accordance with the applicable national regulations.
Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.
![Image alternative](https://files-techDocs.hilti.com/2243106/H2_BILD-Objekt_System_VC_20-U-G3_DEU_Konform_UH.jpg)