DSH 600
DSH 600-X
Original operating instructions
Information about the documentation
About this documentation
- Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
- Observe the safety instructions and warnings in this documentation and on the product.
- Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
Explanation of symbols used
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the documentation
The following symbols are used in this document:![]() |
Read the operating instructions before use. |
![]() |
Instructions for use and other useful information |
![]() |
Dealing with recyclable materials |
![]() |
Do not dispose of electric equipment and batteries as household waste |
Symbols in the illustrations
The following symbols are used in illustrations:![]() |
These numbers refer to the corresponding illustrations found at the beginning of these operating instructions |
![]() |
The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text |
![]() |
Item reference numbers are used in the overview illustrations and refer to the numbers used in the product overview section |
![]() |
This symbol is intended to draw special attention to certain points when handling the product. |
Product-dependent symbols
Symbols on the product
The following symbols are used on the product:![]() |
Direction-of-rotation arrow on the guard |
![]() |
Engine stop position |
![]() |
Engine run position |
![]() |
Primer bulb |
![]() |
Idling jet adjusting screw |
![]() |
Full-throttle jet adjusting screw |
![]() |
Idling adjusting screw |
![]() |
Fuel mixture |
![]() |
Fuel-tank cap opening direction |
![]() |
Choke (not -X) |
![]() |
Wear ear protection, eye protection, respiratory protection and a hard hat |
![]() |
Wear protective gloves |
![]() |
Wear protective footwear |
![]() |
Wireless data transfer |
Adhesive labels on the machine
Warning signs![]() |
Warning: Risk of fire due to flying sparks |
![]() |
Warning: Risk of kickback |
![]() |
Warning: Do not inhale toxic vapors or exhaust fumes |
![]() |
Maximum spindle speed |
![]() |
Warning: Hot surface |
![]() |
Do not use toothed cutting discs |
![]() |
Do not use damaged cutting discs |
![]() |
No smoking, no naked flame |
Product information

The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
Product informationCut-off saw DSH 600 | DSH 600-X Generation 01 Serial no.
Declaration of conformity
We declare, on our sole responsibility, that the product described here complies with the applicable directives and standards. A copy of the declaration of conformity can be found at the end of this documentation.The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | 86916 Kaufering, Germany
Safety
Personal safety
- Use the right tool for the job. Do not use the tool for purposes for which it was not intended. Use it only as directed and when in technically faultless condition.
- Never tamper with or modify the tool in any way.
- Only persons who are familiar with it, who have been trained on how to use it safely and who understand the resulting hazards are permitted to use the tool. The tool is not intended for use by children.
- Stay alert, watch what you are doing and use common sense when operating the tool. Do not use the tool while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating the tool can result in serious personal injury.
- The user and persons in the vicinity must wear suitable protective goggles, a hard hat, ear defenders, protective gloves, protective footwear and light respiratory protection while the tool is in use.
- Always hold the tool firmly with both hands on the grips provided. Keep the grips dry, clean and free from oil and grease.
- Never use the tool without the guard (hood). Adjust the guard to the correct position. The guard must be securely attached and positioned for maximum safety, so that the smallest possible part of the cutting disc is exposed to the operator. Make sure that sparks created during use do not present a hazard. The guard helps to protect the operator from broken disc fragments, inadvertent contact with the cutting disc and uncontrolled flying sparks.
- Do not touch rotating parts – risk of injury!
- Maintain a firm footing and balance at all times. This will allow you to control the tool better, even in unexpected situations. Avoid unusual postures.
- Wear suitable work clothes. Do not wear jewelry or loose clothing. Keep your hair, clothing and gloves away from moving parts. Loose clothes, jewelry or long hair can be snagged by moving parts.
- Releasing the throttle safety grip when the tool is running at full speed causes the tool to tip forward slightly due to the braking torque. Be prepared for this and grip the tool securely with both hands on the grips provided.
- If the tool or the cutting disc has been dropped or has fallen, check the tool and the cutting disc for damage. Change the cutting disc if necessary.
- Switch the tool off before adjusting the guard or changing the cutting disc.
- Wear protective gloves also when changing the cutting disc. Touching the cutting disc presents a risk of injury (cuts or burns).
- Wear eye protection. Flying fragments present a risk of injury to the body and eyes.
- Use of the wet cutting method is preferable in order to reduce the amount of dust produced when cutting mineral materials and asphalt.
- Avoid skin contact with the slurry created when using the wet cutting method.
- Dust from materials such as paint containing lead, some types of wood, minerals and metal can be harmful to health. Contact with or inhalation of the dust can cause allergic reactions and/or respiratory or other diseases to the operator or bystanders. To reduce the amount of dust produced when cutting, we recommend use of the wet cutting method. Make sure that the workplace is well ventilated. It is advisable to wear a filter class P2 dust mask. Comply with national regulations applicable to the materials you will be working with.
- Cutting material containing asbestos is not permissible.
- Take breaks between working and do relaxation and finger exercises to improve the blood circulation in your fingers. Exposure to vibration during long periods of work can lead to disorders of the blood vessels and nervous system in the fingers, hands and wrists.
- Consult the responsible structural engineer, architect or person in charge of the building project before starting work. Slits cut into load-bearing walls or other structures can influence the statics of the structure, especially when reinforcing bars or load-bearing components are cut.
- If work involves break-through, always secure the area on the side opposite where the work is carried out. Pieces of debris could drop out and/or fall down and injure other persons.
- Never leave the tool running while unattended. Switch the engine off and wait until the cutting disc has come to a complete standstill before placing the tool on the ground or before transporting it.
- Make sure that the pump cover is installed if you operate the tool without an external water pump.
- Switch the tool off after use.
- Maintain the tool carefully. Check whether parts are broken or damaged to the extent that the tool is not in full working order. Have damaged parts repaired before using the tool.
- To avoid risk of injury, use only genuine Hilti accessories and accessory tools.
- Have the tool repaired only by qualified specialists using only genuine Hilti spare parts. The safety of the tool can thus be maintained.
- Comply with national health and safety requirements.
Electrical safety
- Before beginning work, check the working area for concealed electric cables or gas and water pipes. External metal parts of the machine may give you an electric shock if you damage an electric cable accidentally.
Safety at the workplace
- Ensure that the workplace is well lit.
- Don’t work in closed rooms. Carbon monoxide, unburned hydrocarbons and benzene in the exhaust gas may cause asphyxiation.
- Keep the workplace tidy. Objects which could cause injury should be removed from the working area. Untidiness at the workplace can lead to accidents.
- Hot exhaust gases containing sparks or sparks generated by the cutting operation may cause fire or explosion. Take care to ensure that the sparks generated do not ignite flammable (gasoline, dry grass, etc.) or explosive (gas, etc.) substances.
- Before fitting the water pump, check to ensure that the maximum permitted water supply pressure of 6 bar is not exceeded.
Liquids (gasoline and oil) and vapors
- Allow the product to cool before refueling.
- Never smoke while refueling.
- Don’t refuel the product at the workplace area. When refueling, take care to avoid fuel spillage. Use a suitable funnel.
- Avoid inhaling gasoline vapors and exhaust fumes. Take care to ensure adequate ventilation.
- Don’t use the gasoline or other flammable liquids for cleaning.
Cutting work using cutting discs
- Use only cutting discs with a rated maximum permissible speed that’s at least as high as the highest spindle speed.
- Check that the outside diameter and the thickness of the cutting disc comply with the capacity rating of the product.
- Never use cutting discs that are damaged, run untrue or vibrate.
- Do not use damaged diamond cutting discs (cracks in the steel disc, broken or polished segments, damaged arbor hole, bent or distorted steel disc, heavy discoloration due to overheating, steel disc worn away beneath the segments, diamond segments with no lateral overhang, etc.).
- Do not use toothed accessory cutting tools (e.g. toothed saw blades).
- When fitting the cutting disc, always take care to ensure that the disc’s specified direction of rotation corresponds to the direction of rotation of the spindle.
- The cutting disc and flange or any other accessory must fit the arbor of the product exactly. Cutting discs or accessories with arbor holes that do not match the mounting hardware of the product will run out of balance, vibrate excessively and may cause loss of control.
- Always use an undamaged clamping flange of the correct diameter which fits the cutting disc used. The correctly fitting clamping flange supports the cutting disc and thus reduces the possibility of disc breakage.
- Guide the product smoothly and do not apply lateral pressure to the cutting disc. Always bring the cutting disc into contact with the workpiece at right angles. Don’t attempt to alter the line of cut by applying lateral pressure or by bending the cutting disc while cutting is in progress.
- Wear protective gloves when changing the cutting disc as the disc will get hot during use.
- Abrasive cutting discs which are used for wet cutting must be used up the same day as long periods of exposure to moisture have a negative effect on the strength of the disc.
- Observe the expiry date for resin-bonded cutting discs and don’t use the discs after this date.
Transport and storage
- Switch the product off before transporting it.
- Remove the cutting disc from the product after use. The cutting disc may suffer damage during transport with the disc fitted.
- Handle the cutting disc carefully and store it in accordance with the manufacturer’s instructions.
- Always store and transport the product in an upright position, not lying on its side.
- Do not transport the product by crane.
- Store the product in a secure place when not in use. Products which are not in use must be stored in a dry, high place or locked away out of reach of children.
- When laying the product down, make sure that it stands securely.
- After use, allow the product to cool down before packing it away or placing a cover over it.
- Store gasoline and oil in a well-ventilated room in fuel containers that comply with regulations.
Description
Product overview
Gasoline-powered cut-off saw

- Guard
- Water supply
- Water connection
- Front grip
- Throttle trigger
- Rear grip
- Recoil starter pull handle
- Fuel tank cap
- Primer bulb
- Fuel level indicator
- Choke lever (DSH 600)
- Footplate
- Exhaust discharge with spark filter
- Cutting disc
- Clamping screw
- Clamping flange
- Rating plate
- Throttle safety grip (DSH 600)
- Safety grip with integrated brake actuation (DSH 600-X)
- Start/stop switch with integrated half-throttle lock
- Water cock
- Spark plug connector
- Cleaning screw for water nozzle
- Grip for guard adjustment
- Curved water distributor with integrated water nozzles
- Hole for locking pin for changing cutting discs
- Saw arm
- Pump cover
- Air filter cover
Intended use
The product described is a gasoline-powered cut-off saw for the wet or dry cutting of asphalt, mineral construction materials or metals using diamond cutting discs or abrasive cutting discs.
The saw is not suitable for use in environments where there is risk of fire or explosion.Possible misuse
- “Shoveling” with the gasoline-powered saw is not permissible.
Instructions for use
- Use of the wet cutting method is preferable in order to reduce the amount of dust produced when cutting. By using the self-priming water pump (accessory) you can work without need for a water supply hose. The water can be drawn, for example, directly from a container.
- Do not cut right through the workpiece in one pass. Move the saw back and forward several times until it gradually reaches the desired cutting depth.
- To avoid damaging the diamond cutting disc when dry cutting, lift the disc out of the cut for approx. 10 seconds every 30 to 60 seconds while the saw is still running.
- Resharpen a polished diamond disc (i.e. when no diamonds project from the segment matrix) by cutting with the disc in a very abrasive material such as sandstone.
Cutting disc specifications
Diamond discs in accordance with EN 13236 are to be used with the product. Synthetic resin-bonded, fiber-reinforced cutting discs in accordance with EN 12413 (straight, not dish-shaped, type 41) may also be used with the product for working on metals.The disc mounting instructions and instructions for use issued by the cutting disc manufacturer must be observed.
Items supplied
Gasoline-powered cut-off saw, DSH 600/DSH 600-X tool set, DSH 600/DSH 600-X consumables set, operating instructions.You can find other system products approved for your product at your local Hilti Center or online at: www.hilti.com
Saw blade brake
DSH 600-XThe product is equipped with an integrated saw blade brake to increase operator safety.
The saw blade is braked to a standstill in a maximum of 10 seconds after the throttle safety grip is released.
Consumables and wearing parts
- Air filter
- Cord (5 pcs)
- Starter
- Fuel filter
- Spark plug
- Tool set
- Cylinder set
- Mounting screw assy.
- Flange for abrasive cutting disc (with integral centering ring 20 mm/1")
- Flange for diamond cutting disc (with integrated centering ring 20 mm/1")
Technical data
Gasoline-powered cut-off saw
DSH 600 |
DSH 600-X |
|
---|---|---|
Cubic capacity |
63.3 cm³ |
63.3 cm³ |
Weight with diamond disc flange, without cutting disc, tank empty |
9.75 kg |
9.85 kg |
Rated power at 8,500/min in accordance with ISO 7293 |
3.2 kW |
3.2 kW |
Maximum spindle speed |
5,500 /min |
5,500 /min |
Max. rotational speed of the cutting disc |
5,500 /min |
5,500 /min |
Maximum cutting depth |
120 mm |
120 mm |
Carburetor |
Walbro; model: WT-1207 |
Walbro; model: WT-1203 |
Additional technical data
Engine type |
Single-cylinder, air-cooled two-stroke engine |
Maximum engine speed |
9350 ± 200 /min |
Idle speed |
2900 ± 200 /min |
Ignition (type) |
Electronic |
Electrode gap |
0.5 mm |
Spark plug |
NGK, type: CMR7A-5 |
Tightening torque for fitting the spark plug |
12 Nm |
Fuel mixture |
API-TC oil 2% (1:50) |
Tank capacity |
0.87 ℓ |
Cutting disc arbor size / diameter of centering bush |
20 mm |
Cutting disc arbor size / diameter of centering bush |
25.4 mm |
![]() |
60 mm |
![]() |
78 mm |
Maximum disc outside diameter |
300 mm |
Maximum disc outside diameter |
12 in |
Maximum nominal disc thickness (only for steel core discs) |
4.5 mm |
Maximum nominal disc thickness (composite discs) |
4.0 mm |
Tightening torque for fitting the cutting disc |
25 Nm |
Noise information and vibration values determined in accordance with ISO 19432
The sound pressure and vibration values given in these instructions have been measured in accordance with a standardized test and may be used to compare one gasoline-powered saw with another. They may be used for a preliminary assessment of exposure.The data given represents the main applications of the machine. However, if the machine is used for different applications, with different accessory tools or is poorly maintained, the data may vary. This may significantly increase exposure over the total working period.
An accurate estimation of exposure should also take into account the times when the machine is switched off, or when it is running but not actually being used for a job. This may significantly reduce exposure over the total working period.
Identify additional safety measures to protect the operator from the effects of noise and/or vibration, for example: Maintaining the machine and accessory tools, keeping the hands warm and organizing work patterns.
Noise emission values
DSH 600 |
DSH 600-X |
|
---|---|---|
Sound pressure level (Lpa,eq) |
102 dB(A) |
102 dB(A) |
Uncertainty |
3.0 dB(A) |
3.0 dB(A) |
Measured sound power level (Lwa) |
113 dB(A) |
113 dB(A) |
Uncertainty |
2.2 dB(A) |
2.2 dB(A) |
Guaranteed sound power level (Lwa) |
115 dB(A) |
115 dB(A) |
DSH 600 |
DSH 600-X |
|
---|---|---|
Vibration value at grip, front (ahv,eq) |
≤ 2.5 m/s² |
≤ 2.5 m/s² |
Uncertainty |
1.3 m/s² |
1.3 m/s² |
Vibration value at grip, rear (ahv,eq) |
≤ 2.5 m/s² |
≤ 2.5 m/s² |
Uncertainty |
1.3 m/s² |
1.3 m/s² |
Before use
Fuel
The two-stroke engine runs on a mixture of gasoline and oil. The quality of the fuel mixture decisively influences operation and life expectancy of the engine.Using two-stroke oil
- Use good-quality, two-stroke oil for air-cooled engines that meets at least the API-TC specification.
Gasoline
- Use regular or super gasoline with an octane rating of at least 89 ROZ.
Mixing fuel
- Pour the required quantity of two-stroke oil into the fuel canister.
- Then fill the gasoline into the fuel canister.
- Close the fuel canister.
- Mix the fuel by shaking the fuel container.
Filling the fuel tank
- Mix the fuel (two-stroke oil / gasoline mixture) by shaking the fuel container.
- Place the product in a steady upright position.
- Open the fuel tank by turning the cap counterclockwise and then removing the cap.
- Fill the tank slowly using a funnel.
- Close the fuel tank by fitting the cap and then turning it clockwise.
- Close the fuel canister.
Assembly and adjustment
Fitting a cutting disc

- Insert the locking pin in the hole in the drive belt cover and turn the cutting disc until the locking pin engages.
- Release the securing screw by turning the screw counterclockwise with the wrench and then remove the screw and washer.
- Remove the locking pin.
- Remove the clamping flange and the cutting disc.
- Check that the diameter of the arbor hole in the cutting disc to be fitted matches the centering collar of the cutting disc mounting flange.
- Clean the clamping and centering surfaces on the tool and on the cutting disc.
- Select one of the following alternatives.
- Use only the large flange to secure the abrasive cutting disc.
- Use the small flange with diamond cutting discs in order to utilize the full cutting depth.
- Use only the large flange to secure the abrasive cutting disc.
- Place the cutting disc with centering collar on the drive arbor and check that the direction of rotation is correct.
- The direction-of-rotation arrow on the cutting disc must match the direction of rotation indicated on the tool.
- The direction-of-rotation arrow on the cutting disc must match the direction of rotation indicated on the tool.
- Place the clamping flange and washer on the drive arbor and tighten the securing screw by turning it clockwise.
- Insert the locking pin in the locking hole in the drive belt cover and turn the cutting disc until the locking pin engages.
- Securely tighten the clamping screw (tightening torque: 25 Nm).
- Remove the locking pin.
Adjusting the guard
- Hold the guard by the grip provided and rotate it to the desired position.
Fitting the water pump (accessory)

- Release the three pump cover retaining screws, remove the parts and store the pump cover in a safe place.
- Hold the water pump in position and turn the cutting disc slightly to bring the splines of water pump and clutch bell into alignment so that the splines engage.
- The position is keyed so it is not possible to position the pump incorrectly.
- The position is keyed so it is not possible to position the pump incorrectly.
- Fit the three retaining screws and tighten them securely (tightening torque: 8 Nm).
- Connect the pump hose to the hose connector on the saw.
- Remove the protective cap from the end of the water connection hose.
- Connect the water pump to the water supply or immerse the end of the suction hose in a container filled with water.
Removing the water pump (accessory)
- Disconnect the water supply from the water pump.
- Fit the protective cap to the end of the water connection hose.
- Disconnect the connector between the pump and the tool.
- Release the three fastening screws on the pump and then remove the pump.
- Fit the pump cover on the tool, insert the three retaining screws and tighten the screws securely (tightening torque: 4 Nm).
Fitting the wheel set (accessory)

- Slacken the two bottom securing screws on the metal guard.
- Secure the base plate with the two screws.
- Secure the wheels and washers with the screws on both sides of the base plate.
Operation
Starting the engine
- If the following equipment exists, also take this action:
DSH 600
- Press and hold down the throttle safety grip.
- Press and hold down the throttle trigger.
- Move the start/stop switch to the “start” position.
- Release the throttle safety grip and throttle trigger.
- The half-throttle position is activated.
- The half-throttle position is activated.
- Squeeze the primer bulb 2 to 3 times until the primer bulb is completely filled with fuel.
- If the following conditions are met, also take this action:
Conditions : The engine is cold.
- Pull the choke lever up.
- The choke is activated.
- The choke is activated.
- Pull the choke lever up.
- Check that the cutting disc is free to rotate.
- Place your left foot on the footplate.
- Pull the recoil starter pull handle slowly with your right hand until resistance is perceptible.
- Vigorously pull the recoil starter pull handle.
- When you hear the engine start to fire (after 2 to 5 pulls of the starter), move the choke lever back down to its original position.
- Vigorously pull the recoil starter pull handle repeatedly until the engine fires.
- Briefly press the throttle trigger as soon as the engine fires.
- This disengages the half-throttle position and the engine will idle when the throttle trigger is released.
- This disengages the half-throttle position and the engine will idle when the throttle trigger is released.
- Press and hold down the throttle safety grip.
- If the following equipment exists, also take this action:
DSH 600-X
- Press and hold down the throttle safety grip.
- Press and hold down the throttle trigger.
- Move the start/stop switch to the “start” position.
- Release the throttle safety grip and throttle trigger.
- The half-throttle position is activated.
- The half-throttle position is activated.
- Squeeze the primer bulb 2 to 3 times to fill the primer pump bulb with fuel only when starting with the engine cold.
- Check that the cutting disc is free to rotate.
- Place your left foot on the footplate.
- Pull the recoil starter pull handle slowly with your right hand until resistance is perceptible.
- Vigorously pull the recoil starter pull handle.
- Repeat this procedure until the engine fires.
- Briefly press the throttle trigger as soon as the engine fires.
- This disengages the half-throttle position and the engine will idle when the throttle trigger is released.
- This disengages the half-throttle position and the engine will idle when the throttle trigger is released.
- Press and hold down the throttle safety grip.
Checks after starting the engine
- Check that the cutting disc remains stationary when the engine is idling and, after briefly running at full speed, that the disc again comes to a complete standstill.
- Readjust (reduce) the idling speed if the cutting disc doesn’t stop rotating when the engine is idling. If this is not possible, please bring the product to Hilti Service.
- Readjust (reduce) the idling speed if the cutting disc doesn’t stop rotating when the engine is idling. If this is not possible, please bring the product to Hilti Service.
- Check that the start/stop switch is functioning correctly. Move the start/stop switch to the “stop” position.
- If the following equipment exists, also take this action:
DSH 600
- If the engine doesn’t stop, push the choke lever upwards. If the engine still doesn’t stop, pull the spark plug connector off the spark plug and bring the product to Hilti Service.
- If the engine doesn’t stop, push the choke lever upwards. If the engine still doesn’t stop, pull the spark plug connector off the spark plug and bring the product to Hilti Service.
- If the following equipment exists, also take this action:
DSH 600-X
- If the engine doesn’t stop, compress the primer bulb. If the engine still doesn’t stop, pull the spark plug connector off the spark plug and bring the product to Hilti Service.
- If the engine doesn’t stop, compress the primer bulb. If the engine still doesn’t stop, pull the spark plug connector off the spark plug and bring the product to Hilti Service.
Switching the engine off
- Release the throttle trigger.
- Move the start/stop switch to the “stop” position.
- The engine stops.
- The engine stops.
Cutting techniques

In order to work optimally with this tool, the following safety instructions must be observed:
- Always hold the tool with both hands on the grips provided. Keep the grips dry, clean and free from oil and grease.
- Before beginning the work, or if the disc has inadvertently come into contact with an obstacle (e.g. a concealed object), check the cutting disc and guard immediately for possible damage.
- Check that no persons are present in the working area and, in particular, in the direction in which the cut is to be made. Keep other persons approx. 15 m away from your workplace.
- Guide the tool smoothly and do not apply lateral pressure to the cutting disc.
- Avoid hazardous operating positions.
- Always bring the cutting disc into contact with the workpiece at right angles. Do not attempt to alter the line of cut by applying lateral pressure or by bending the cutting disc while cutting is in progress.
- Secure the workpiece. Use clamps or a vice to hold the workpiece in position. The workpiece is thus held more securely than by hand and both hands remain free to operate the tool.
- Clamp round workpieces so that they cannot rotate.
- Do not cut several workpieces at the same time. Cut them one after the other.
- Secure the workpiece and the part to be cut off in order to prevent uncontrolled movement.
- Always apply full throttle when cutting.

-
Reasons for the cutting disc sticking / stalling:
- The cut is too deep.
- The kerf becomes narrower (e.g. when cutting pipes or slabs).
- The cutting disc is tilted.
- An unsuitable cutting disc is used (the cutting disc becomes clogged).
- The cutting disc is inserted too quickly in an existing kerf.

- Pulling may occur when making horizontal cuts (e.g. in a floor). The saw may suddenly pull forwards, possibly pulling it out of the operator’s hands.
- Climbing may occur when making vertical cuts (e.g. in a wall). The saw may suddenly pull upwards, possibly pulling it out of the operator’s hands.
- Kickback may occur if the prohibited area of the disc is brought into contact with the workpiece.
- Cutting through thick workpieces should be accomplished, as far as possible, by making several cuts. Avoid making excessively deep cuts.
- Support slabs or large workpieces so that the kerf remains open during and after the cutting operation.
- Always bring the cutting disc into contact with the workpiece from above.
- Allow the cutting disc to contact the workpiece only at a point below its rotational axis.
- Be particularly cautious when inserting the cutting disc in an existing kerf.
- Take care to avoid tilting the cutting disc to the side.
Care and maintenance
Maintenance table
1 - Before starting work | 2 - Every six months | 3 - As necessary1 |
2 |
3 |
|
---|---|---|---|
Check that the tool is complete, in perfect condition and free of leaks. Have it repaired if necessary. |
X |
||
Check for dirt and foreign matter. Clean if necessary. |
X |
||
Check that the controls function correctly. Have repairs carried out if necessary. |
X |
||
Check that the cutting disc is in perfect condition. Replace if necessary. |
X |
||
Check that all externally accessible nuts and screws are securely tightened. |
X |
X |
X |
Check that the fuel filter is clean. Replace it if necessary. |
X |
X |
|
Replace the air filter if the product does not start or engine performance fades noticeably. |
X |
||
Clean or replace the spark plug if the product does not start or is difficult to start. |
X |
||
Adjust the idling speed if the cutting disc does not slow to a standstill when the engine is idling. |
X |
||
Have the product repaired by Hilti Service if the drive belt slips when a load is applied to the cutting disc. |
X |
Cleaning or replacing the air filter

- Release the securing screw on the air filter cover and remove the cover.
- Carefully remove the dust adhering to the air filter and the filter chamber (use a vacuum cleaner).
- Release the four screws retaining the filter holder and remove the air filter.
- Fit the new filter and secure it with the filter holder.
- Fit the air filter cover and tighten the retaining screws.
Replacing a broken starter cord

- Release the four securing screws and remove the starter assembly.
- Release the two screws securing the cover and remove the cover.
- Remove the remains of the broken starter cord from the spool and the pull handle.
- Securely knot one end of the replacement starter cord and from above, pass the other end of the cord through the hole in the spool.
- From below, pass the end of the cord through the hole in the starter housing and from below through the pull handle, and securely knot the end of the cord.
- Pull a length of the starter cord out of the housing as shown in the illustration and pass it through the slot in the spool.
- Hold the cord securely close to the slot in the spool and turn the spool clockwise as far as it will go.
- Back the spool off at least ½ to max. 1½ turns, until the slot in the spool is in alignment with the opening in the starter housing.
- Hold the spool securely and pull the cord out of the housing toward the pull handle.
- Hold the cord taut, release the spool and allow the starter cord to be pulled in.
- Pull the starter cord out as far as it will go and check that the spool can be turned by hand at least a further ½ turn clockwise. If this is not possible, spring tension must be reduced by turning the spool one full turn counterclockwise.
- Install the cover and secure it with the two securing screws.
- Place the starter assembly in position and carefully press it down. Pull the starter cord slightly until the coupling engages and the starter assembly is fully seated.
- Secure the starter assembly with the four securing screws.
Replacing the fuel filter

- Remove the cap from the fuel tank.
- Pull the fuel filter out of the fuel tank.
- Check the condition of the fuel filter.
- Replace the fuel filter if it is very dirty or clogged.
- Replace the fuel filter if it is very dirty or clogged.
- Slide back the clip on the hose and remove the dirty fuel filter.
- Fit a new fuel filter and secure it with the clip on the hose.
- Push the fuel filter back into the fuel tank.
- Close the fuel tank.
Cleaning the spark plug, setting the spark plug gap or replacing the spark plug

- Use a gentle twisting motion to pull the cable connector off the spark plug.
- Use the spark plug wrench to unscrew and remove the spark plug from the cylinder.
- If necessary, clean the spark plug electrode with a soft wire brush.
- Check the spark plug gap with the aid of a feeler gauge and, if necessary, reset it to the correct gap (0.5 mm).
- Fit the ignition cable connector to the spark plug and hold the threaded section of the spark plug against the cylinder.
- Move the start/stop switch to the “start” position.
- Pull the starter handle.
- An ignition spark must now be clearly visible.
- An ignition spark must now be clearly visible.
- Use the spark plug wrench to screw the spark plug into the cylinder (tightening torque: 12 Nm).
- Fit the ignition cable connector to the spark plug.
Adjusting the carburetor
The carburetor of this product has been factory set for optimum performance and sealed to prevent tampering (jets H and L). The idling speed of the machine (jet T) may be adjusted by the user. All other adjustments must be carried out by Hilti Service.- Clean the air filter.
- Allow the product to run until it reaches its normal operating temperature.
- Use a suitable flat screwdriver (tip width 4 mm/ ⁵/₃₂ ") and do not force the adjusting screw beyond its intended adjustment range.
- Adjust the idling speed jet (T) so that the engine runs smoothly when idling but the cutting disc does not begin to rotate.

Cleaning the water nozzles

- Remove the cleaning screw on the curved water distributor.
- Use a wire to clean the water nozzles.
- Fit the cleaning screw.
Care of the product
- Keep the product, especially its grip surfaces, clean and free from oil and grease.
- Do not use cleaning agents containing silicone.
- Clean the outer surfaces of the machine at regular intervals with a slightly damp cloth or a dry brush. Do not use a spray, steam pressure cleaning equipment or running water for cleaning.
- Do not allow foreign objects to enter the interior of the product.
Maintenance
- Check all external parts of the product and the accessories for damage at regular intervals and check that all controls operate faultlessly.
- Do not use the product if parts are damaged or if operating controls do not function faultlessly. Have the product repaired by Hilti Service.
Checks after care and maintenance work
- After carrying out care and maintenance, check that all protective and safety devices are fitted and that they function faultlessly.
Transport and storage
Transporting the product in a vehicle
- Remove the cutting disc.
- Secure the product to prevent it falling over, thereby causing damage or fuel spillage.
Storing the fuel mixture
- Mix only enough fuel for a few days’ use.
- Clean the fuel container occasionally.
Troubleshooting
If the trouble you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, contact Hilti Service.Trouble or fault |
Possible cause |
Action to be taken |
---|---|---|
Cutting disc slows down or stops completely while cutting |
Excessive cutting pressure applied (cutting disc sticks and stalls in the kerf). |
|
The cutting disc is not correctly fitted and tightened. |
|
|
Wrong direction of rotation. |
||
The forward section of the saw arm is loose. |
|
|
High vibration, disc wanders off the cutting line. |
The cutting disc is not correctly fitted and tightened. |
|
Cutting disc is damaged (or unsuitable specification, cracked, segments missing, bent, overheated, deformed, etc.). |
|
|
The centering bushing is fitted incorrectly. |
|
|
The diamond cutting disc swings up and may jam. |
Diamond cutting disc does not fit correctly |
|
Flange for diamond cutting disc does not fit correctly |
|
|
The saw doesn’t start or is difficult to start. |
The fuel tank is empty (no fuel in the carburetor). |
|
Air filter clogged with dirt or dust. |
|
|
DSH 600 The engine is flooded (spark plug wet). |
|
|
DSH 600-X The engine is flooded (spark plug wet). |
|
|
Wrong fuel mixture. |
|
|
Air in the fuel line (no fuel reaching the carburetor). |
|
|
The fuel filter is dirty or blocked (no fuel or too little fuel reaching the carburetor). |
|
|
No ignition spark visible or spark is too weak (seen when spark plug is removed). |
|
|
Engine compression is too low. |
|
|
The ambient temperature is too low. |
|
|
The spark arrestor or exhaust exit is clogged. |
|
|
Low engine power / poor cutting performance |
Air filter clogged with dirt or dust. |
|
No ignition spark visible or spark is too weak (seen when spark plug is removed). |
|
|
Wrong fuel mixture. |
|
|
The disc specification is unsuitable for the material to be cut. |
|
|
Drive belt or cutting disc slips. |
|
|
Engine compression is too low. |
|
|
The product is used at an altitude greater than 1500 meters above sea level. |
|
|
Incorrect carburetor setting (fuel / air mixture). |
|
|
Cutting disc rotates while the engine is idling. |
Idling speed is too high. |
|
The half-throttle position is engaged. |
|
|
Faulty centrifugal clutch. |
|
|
Cutting disc doesn’t rotate. |
Inadequate drive belt tension or the drive belt is broken. |
|
Starter assembly doesn’t work. |
The clutch claws are not engaging. |
|
DSH 600-X Saw blade rotates for longer than 15 seconds after the throttle safety grip is released. |
Brake strap is worn. |
|
Action of Bowden cable for brake is stiff. |
|
Disposal

Drilling slurryDisposal of drilling slurry directly into rivers, lakes or the sewerage system without suitable pretreatment presents environmental problems.
- Ask the local public authorities for information about current regulations.
- Collect the drilling slurry (for example, using a wet-type vacuum cleaner).
- Allow the drilling slurry to settle and dispose of the solid material at a construction waste disposal site (addition of a flocculent may accelerate the settling process).
- The remaining water (alkaline, pH value greater than 7) must be neutralized by the addition of an acidic neutralizing agent or diluted with a large volume of water before it is allowed to flow into the sewerage system.
Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.