Skip to main content

PROFIS Engineering & Checkbot

Hilti Engineering Centre
Reading time: < 10 minutes
Article

Revolutionising Structural Engineering: The power of PROFIS Engineering integration with Checkbot. The new structural engineering end-to-end workflow standard.

Baseplate
Software & Services
Structural Connections

Revolutionising Structural Engineering: The power of PROFIS Engineering integration with Checkbot.

Hilti Group and IDEA StatiCa, global leaders in steel-to-concrete and steel-to-steel structural connections respectively, have partnered to introduce a new plugin to enhance the standard design, calculation, and construction workflow for all types of projects. The integration of Hilti Group's PROFIS Engineering Suite with IDEA StatiCa's Checkbot improves accuracy, safety, and efficiency in the construction industry. PROFIS Engineering Suite, which has a presence in over 70 countries, allows the design and calculation of various structural connections under a range of conditions. It provides the latest anchor approvals, a variety of design methods, and a comprehensive calculation report.

Checkbot simplifies communication from various structural design and BIM software by allowing the import of thousands of connections with their loads and geometries, where you can check all important information in each of these connections before exporting them to PROFIS Engineering Suite or other software developed by IDEA Statica. This ensures that all information is correctly and quickly mapped across the end-to-end design and calculation workflow.

This integration brings several benefits, including time saving and simplification, easier organization, better collaboration, and increased accuracy and quality. By setting a new standard for the structural engineering and construction end-to-end workflow, this empowers engineers to take their projects to new levels in terms of quality, efficiency, and precision while providing peace of mind. By adopting this unified approach, structural engineers are well-prepared for the challenges the industry currently faces as well as those that will come.

Follow the guidance below based on your software:

  • Category 1: Automated integration for Tekla Structures, Revit, Advance Steel, Robot, SCIA Engineer, SDS2, STAAD.PRO, AxisVM, RFEM 5 and RSTAB 8

  • Category 2: Automated external integration fro RFEM 6 and RSTAB 9.

  • Category 3: Manual Integration for SAP 2000 and ETABS

  • Category 4: File based for RISA-3D and RAM Structural Systems.

Category 1: Automated Integration

Software supported by this installation procedure: Advance Steel, AxisVM, Revit, Robot, RFEM 5, RSTAB 8, SCIA Engineer, SDS2, STAAD.PRO, Tekla Structures.

The IDEA StatiCa BIM link installer automatically launches after the installation of any IDEA StatiCa software and can also be accessed manually from IDEA StatiCa's main interface. It locates all structural design and BIM software packages on your machine. Once integrated, IDEA StatiCa Checkbot is available through the FEA/BIM partner application, enabling the seamless export of baseplate data to PROFIS Engineering.

Before you start: Ensure you have an active PROFIS Engineering Premium License and confirm that your required FEA/BIM software is installed and up to date. Only the two latest versions are supported. Then follow these steps:

  1. Download and Account Setup: Create an account with IDEA StatiCa (here) and download their latest suite version (here).

  2. Installation: Install the suite as an administrator. The required plugin to connect with PROFIS Engineering is included in the download package.

  3. BIM Link Activation: During installation, you will be prompted to “Activate your BIM

  4. links.” Ensure this step is completed successfully.

  5. Finalizing Installation: Click “Install.” Once the installation is complete and displays green, you will find a new tab in your FEA/BIM software for exporting to Checkbot.

  6. Exporting Data: Once the file is imported to Checkbot, under the “Hilti PROFIS” tab, click the red logo of PROFIS Engineering to transfer your data and start designing your connection.

How To - Engineering Centre

PROFIS Engineering

Category 2: Automated external integration

Software supported by this installation procedure: RFEM 6 and RSTAB 9.

The IDEA StatiCa BIM link installer automatically launches after the installation of any IDEA software and can also be accessed manually from IDEA StatiCa's main interface. It will locate all structural design and BIM software packages on your machine. The BIM link to Checkbot is NOT available in the partner application user interface. It is a separate executable file that you can find on your desktop and needs to be run every time a user wants to proceed with an export.

Before you start: Ensure you have an active PROFIS Engineering Premium License and confirm that your required FEA/BIM software is installed and up to date. Only the two latest versions are supported. Then follow these steps:

  1. Download and Account Setup: Create an account with IDEA StatiCa (here) and download their latest suite version (here).

  2. Installation: Install the suite as an administrator. The required plugin to connect with PROFIS Engineering is included in the download package.

  3. BIM Link Activation: During installation, you will be prompted to “Activate your BIM links.” Ensure this step is completed successfully.

  4. Finalizing Installation: Click “Install.” Once the installation is complete and displays green, you will find a new shortcut icon on your desktop for exporting to Checkbot. Ensure you open the software and navigate to the menu “Options and Program”, then activate the WebService to enable data transfer.

  5. Exporting Data: Once the file is imported to Checkbot, under the “Hilti PROFIS” tab, click the red logo of PROFIS Engineering to transfer your data and start designing your connection.

PROFIS Engineering

Category 3: Manual integration

Software supported under this installation procedure: SAP 2000 and ETABS.

IDEA Checkbot is integrated manually according to the step-by-step tutorial. Instructions are accessible through a URL in the BIMlink installer, via IDEA web pages or following the steps given below.

Before you start: Ensure you have an active PROFIS Engineering Premium License and confirm that your desired FEA/BIM software* is installed and up-to-date. Only the two latest versions are supported. Then follow these steps:

  • Download and Account Setup: Create and account with IDEA StatiCa (here) and download their latest suite version (here).

  • Installation: Install the suite as an administrator. The plugin required to connect with PROFIS Engineering is included in the download package.

  • BIM Link Activation: During installation, you will be prompted to “Activate your BIM links.” Ensure this step is completed successfully.

  • Finalizing Installation: Click “Please install our add-in for your SAP2000 (here), ETABS (here)", and follow activation guideline share by our partners from IDEA StatiCa.

  • Exporting Data: Once the file is imported to Checkbot, under the “Hilti PROFIS” tab, click on the red logo of PROFIS Engineering to transfer your data to it.

PROFIS Engineering

Category 4: File based

File-based integration using SAF or IOM files. Examples: Sofistik, RISA, etc.

File-based import to IDEA Checkbot. There is no direct communication between IDEA Checkbot and partner application.

Before you start: Ensure you have an active PROFIS Engineering Premium License and confirm that your desired FEA/BIM software* is installed and up-to-date. Only the two latest versions are supported. Then follow these steps:

  1. Download and Account Setup: Create and account with IDEA StatiCa (here) and download their latest suite version (here).

  2. Installation: Install the suite as an administrator. The plugin required to connect with PROFIS Engineering is included in the download package.

  3. Finalizing Installation: Follow workflow using following links: RISA-3D (here) and RAM Structural Systems (here)

  4. Exporting Data: Once the file is imported to Checkbot, under the “Hilti PROFIS” tab, click on the red logo of PROFIS Engineering to transfer your data to it.

PROFIS Engineering

List of All Supported FEA and CAD Software by Checkbot

Software

Vendor

Type

Tekla Structures

Trimble

CAD

Autodesk Revit

Autodesk

FEA/CAD

Autodesk Advanced Steel

Autodesk

CAD

Autodesk Robot

Autodesk

FEA

ETABS

Csi

FEA

SAP2000

Csi

FEA

SCIA Engineer

Nemetschek

FEA

SDS2

Allplan

CAD

STAAD.Pro

Bentley

FEA

AxisVM

Inter-CAD kft

FEA

RFEM 5

Dlubal

FEA

RFEM 6

Dlubal

FEA

RSTAB 8

Dlubal

FEA

RSTAB 9

Dlubal

FEA

RAM Structural System

Bentley

FEA

RISA

RISA Tech

FEA

Sofistik (SAF)

Sofistik

FEA

Tekla Structural Designer

Trimble

FEA

FEM-Design

StruSoft

FEA

SPACE GASS

SPACE GASS

FEA

Diamonds / BIM Expert

BuildSoft

FEA/CAD

STRAP

Atir Engineering

FEA

Straus 7

EnginSoft

FEA

FEA: Finite Element Analysis or Structural Software

CAD: BIM Software

Note: Data from software not included in the list can be uploaded directly to Checkbot via a *.saf file