Choosing One Power Tool Battery System

06/02/2026
Hilti Team
Reading time: < 5 minutes
Hilti Innovations

Discover how a single power tool battery system for both regular and heavy-duty tools can benefit the bottom line for your business.

Hilti’s Nuron battery platform is at the cutting edge of construction equipment and offers practical benefits for contractors of all shapes and sizes. Simplification, improved productivity and a safer workplace are just some of the reasons why Nuron is a superior option for forward thinking construction businesses.

It will also become an even bigger advantage in the future as more tools and services join the platform. That makes Nuron a simple way to future proof your operations and get ahead of the competition.

Simplified tool management with a united battery platform

Coordinating and maintaining your fleet of tools is a challenge for all contractors. One of the biggest frustrations can be making sure you have the right cords, chargers, and batteries for everything to keep your site running and your workers operating at maximum productivity.

With Hilti’s Nuron battery platform, you don’t have to worry about this. The batteries are designed to work with more than 70 different Hilti tools and are completely interchangeable, so you only ever need one type of battery and one type of charger.

Other tool management benefits include:

  • More work per charge – The Nuron range can deliver up to twice the power of equivalent 18V and 20V platforms, with performance equivalent to a corded or gas-powered system.

  • Built-in diagnostics – The batteries alert you when they are running low, allowing you to manage your tool fleet effectively and avoid lithium-ion batteries becoming depleted in colder weather.

  • Fully sealed design – Electronics are protected from water, dust, contaminants, and cold conditions, making them more durable.

No matter what application you need or how challenging the job, the same Nuron 22V battery can be used. This means your workers regain the time they once spent searching for the right cord or battery and can focus more on getting the job done.

Improved safety built in

Tools on the Nuron battery system also offer an improved health and safety profile. Most obviously, using the platform can eliminate cords and wires that would otherwise lie across walkways and create a trip hazard.

Nuron tools are also designed with the following features:

  • Active Vibration Reduction (AVR) to minimise hand-arm vibration and reduce the risk of injury.

  • Active Torque Control (ATC) and SensTech technology to reduce tool kickback.

  • Dust Removal Systems (DRS) to reduce exposure to construction dust, including virtually dust-free concrete cutting, drilling, and breaking objects when working at height.

  • Tethering options to reduce the danger of falling objects when working at height.

Improved safety means less time spent managing risk and a lower likelihood of workers needing time off to deal with incidents on site. This leads directly to increased efficiency and productivity on your project.

Looking beyond 2026 and future proofing your business

Finally, using the Nuron platform is a reliable way to future proof your business. It is already useable on both small and heavy duty tools in the Hilti range and will only offer more utility in the next 12 months.

The range of Nuron-compatible tools on offer is always expanding and 2026 will be no different. Businesses which are already on the platform will be able to make use of the new additions seamlessly.

The benefits of using Hilti’s Nuron platform will scale with the new tool releases. More of your tool park will be on the same system, so the time savings and safety benefits will only become more significant.

Want to learn more about Nuron and upgrade your tool park in 2026?

Contact the team today to discuss our options and how your business can benefit.

Request a demo