Skip to main content

Should Psi M,N be different for shear and tension

Posted by PKover 2 years ago
Should Psi M,N be different for shear and tension




In the attached calculation output for HUS-4 Anchors the value of psi M.N is different for tension and shear. As the formula is the same for both, I would expect the values to be the same. Please can you explain why they are different?







mechanical anchors,design load shear

1 Reply
Posted by Engineering Centre Teamover 2 years ago
Hilti Verified

In the concrete breakout failure modes, only the anchors in tension and the tension loads are considered.
In the pryout failure mode, all values (including psi_MN) are recalculated for the shear loads and the anchors are calculated in shear.
In this case psi_MN =1.