Skip to main content

Removal and reinstall HSL-3 anchors

Posted by Mark McVeyalmost 4 years ago
Removal and reinstall HSL-3 anchors

Is it allowable to remove the anchors and then reinstate them?

Removal,Replacement

2 Replies
Posted by Ask HILTI Teamalmost 4 years ago

Thank you for your question we do not supply tools to remove HSL anchors and it is also not possible to reuse them. In case where a baseplate is to be removed and refixed in the same position then I'd suggest looking at an internally threaded socket which is permanently fixed into the concrete but allows for a set screw/ bolt etc to be inserted and removed as required.


1 comment on this reply
Posted by Gregory Katoalmost 2 years ago
Can the Hilti HSL4-I Internally Threaded anchors be used for this purpose? I have a condition where I need to temporarily remove an embed plate to allow access to the interior of a structure for maintenance but would like to be able to reuse the embed plate once the service is completed.

Posted by Ask HILTI Teamalmost 2 years ago

Hi, Thanks for your question the HSL4-I could be an option if you are in N. America as I believe it is available there and can be designed within there local standards. I don't believe this product is available in Europe and I'm also not aware of any European approvals. Depending upon your requirements the HIS -N or HIS-RN internally threaded sockets which can be utilised with various chemicals could be an option or HSC-I internally threaded anchor though the sizes are somewhat limited. I would suggest you contact your local HILTI office to discuss your specific application requirements.