Skip to main content

Question about Hilti connection to RC column with edge distance

Posted by Piotr Pienkowskiover 2 years ago
Question about Hilti connection to RC column with edge distance

Hello,

I came up the following issues while designing connection to RC column. I have connection to take vertical force (downward) of 100kN. If I provide the bottom edge distance say 5000mm the connection failed but if the same distance is changed into infinite then the connection works well (see attached sketch). Could you please clarify what cause the issue and advise which design approach is correct?

edge distance,defined vs. infinite edge distance

3 Replies
Posted by Ask HILTI Teamover 2 years ago
Hilti Verified

Hi, Thanks for the follow up, that's pretty much the beam infinity example to a but flipped to a column to a foundation scenario with the same criteria still applicable.


Posted by Ask HILTI Teamover 2 years ago

Thanks for your question, this really depends upon your structure and whether you decide if the edge distance is restrained or not. I've attached a simplified sketch that gives a general overview.


Posted by Piotr Pienkowskiover 2 years ago

Hi,

Thanks for coming back. Please find the attached sketch with the elevation of the RC column+foundation base and beam connected to the RC column. I hope it will clear up the situation.