Skip to main content

Hilti HIT-FP 700-R in Profis Engineering

Posted by Adam Wisamabout 3 years ago
Hilti HIT-FP 700-R in Profis Engineering

Hello, is Hilti HIT-FP 700-R available in Profis Engineering*? If not, what product resembles it the closest in Profis*?

https://www.hilti.se/c/CLS_FASTENER_7135/CLS_CHEMICAL_ANCHORS_7135/r13812960

*Edit: Anchoring-to-concrete module of Profis

Profis Engineering,hit-fp

2 Replies
Posted by Ask HILTI Teamabout 3 years ago

Thanks for your question yes the FP700-R is in the Profis Engineering software in the concrete to concrete module for example slab - slab and you will see it as an available option.


1 comment on this reply
Posted by Adam Wisamabout 3 years ago
Sorry, I forgot to specify that I meant the anchoring-to-concrete module of Profis.

Posted by Ask HILTI Teamabout 3 years ago

Thanks for the additional query currently the FP700 is post installed rebar, in the anchor model the software will provide results based upon your input for your fire design however you will need to ensure that you have reinforcement to control cracking which controls the crack width to 0.3mm