Skip to main content

Hilti Anchors fixed to Concrete Blockwork Wall Supporting Steel Beam

Posted by Jamieoover 3 years ago
Hilti Anchors fixed to Concrete Blockwork Wall Supporting Steel Beam

I have a steel beam that needs to be fixed to a 100mm thick Blockwork wall. The unfactored end reaction is 14kN. The steel endplate will be 10mm thick. Can you recommend the type and number of anchors required please

Anchors,Blockwork Wall

1 Reply
Posted by Ask HILTI Teamover 3 years ago

Thank you for your enquiry, if you have Profis Engineering you could look at that to run a design within the masonry module using the HY270 resin mortar however it would depend entirely upon the block properties as to the design resistance . I would say that 'by eye' your load is ambitious for a typical block unit and if a low density block material then unrealistic. I'd suggest contacting your local HILTI technical department for further discussion.