Skip to main content

Cannot find rebar from list of available anchors

Posted by  Salvatoreabout 4 years ago
Cannot find rebar from list of available anchors

Hi there, it seems that with profis it's not possible anymore to design post fixed rebar

rebar design,post-installed reinforcement

2 Replies
Posted by Ask HILTI Teamabout 4 years ago

Thanks for your enquiry regarding Profis Engineering. The option to design rebar as an 'anchor' is still available . Please go into the filter option to (Top right hand corner next to your model) select Adhesive and for the Thread type select No Thread (you should then see some options . I've also attached a screen shot for reference.


1 comment on this reply
Posted by F1anaganalmost 4 years ago
Hi Hilti, Has the program changed since this question was answered as when I use the option provided, I end up with only two possible bars both of which are screw anchors? Thanks.

Posted by Ask HILTI Teamalmost 4 years ago

Thanks for the enquiry, Profis Engineering hasn't changed you can still select the HY200-R V3 and the HIT-RE500V4with rebar as per the previous screenshot. Please check you haven't selected any filters or other criteria by accident that has eliminated them as being a suitable option.


2 comments on this reply
Posted by Ask HILTI Teamalmost 4 years ago
Hi, possibly depending upon your region setting and whether the products are available locally and your selected design code allows. Certainly, they aren't locked out for Northern Europe and Eurocode 2 Part 4 which is the local design code.

Posted by F1anaganalmost 4 years ago
I have double checked that no other filters are applied and am still getting the same results, are they perhaps location locked?