Skip to main content

What do we mean by SOFA in PROFIS Engineering?

Hilti Engineering Centre
Reading time: < 5 minutes
Article

In PROFIS Engineering, SOFA (Solution for Fasteners) is an advanced design approach that expands beyond traditional code limits, allowing engineers to safely design complex anchor systems that cannot be solved using EN 1992-4 alone. Find out more in this article.

Baseplate
Software & Services
Structural Connections
Engineers at a desk in an office looking at designs
Engineers in Office

So what do we mean by SOFA?

What possibilities does a design engineer have if the anchor layout is beyond the scope of EN 1992-4, or if the design provisions in EN 1992-4 (utilisation > 100%) do not lead to a solution?

The basis for anchor design in Europe is the design approach given in EN 1992-4. However, there are many cases where solutions cannot be found by strictly following this standard. Therefore, in addition to the design provisions of EN 1992-4, Hilti offers a design approach per the so-called “SOFA method”. SOFA stands for “Solution for Fasteners” which is a design method which goes beyond existing codes. The provisions in SOFA are based on state-of-the-art industry research and undergo extensive review by technical key experts before implementation into PROFIS Engineering.

Comparison with EN 1992-4

Both for static and dynamic (seismic and fatigue) loading, EN 1992-4 covers a limited range of anchor layouts as shown in Figure 1. The individual anchor spacing in one direction must be the same, and the maximum possible anchor layout is restricted to a 3x3 rectangular configuration when not bound by an edge. Other shapes (e.g., circular or free location of anchors within the steel plate) are outside of the scope of EN 1992-4. The allowed anchor layout depends on the following parameters:

  • Hole clearance between steel plate and fastening:

    Depending on the location of the fastening relative to the clearance hole in the steel plate, not all anchors are assumed to evenly resist the shear load. The maximum possible clearance hole is defined in Table 1.

  • Load direction:

    According to EN 1992-4, the fastening can be loaded in tension, shear or a combination between tension and shear.

  • Location of the fastening relative to the edge of a concrete member:

    EN 1992-4 distinguishes between fastenings located close to the edge and far away from the edge. If the edge distance, ci, of the fastening in all directions (i = 1 and 2) is the larger of 10hef and 60dnom, the fastenings is considered far away from the edge. If not, then the influence of the edge distance on the concrete related failure modes needs to be considered.

    Excerpt from EN document regarding fastener information

    a) Fastenings without hole clearance for all edge distances and for all load directions, and fastenings with hole clearance according to Table 1 situated far from edges for all load directions and fastenings with hole clearance according to Table 1 situated near to an edge loaded in tension only

  • Excerpt from EN document regarding fastener information and edge distances

    b) Fastenings with hole clearance according to Table 1 situated near to an edge for all load directions

    Figure 1– Anchor configurations covered in EN 1992-4 (picture taken from EN 1992-4)

Engineers viewing PROFIS on a large screen

SOFA Design method

The SOFA design method offers three main features:

  1. Design provisions for tension, shear, and combined tension and shear for anchor layouts beyond the scope of EN 1992-4, allowing design coverage up to 99 anchors in a group.

  2. Improved shear design provisions to better utilize the fastening for the failure mode “concrete edge failure”.

  3. Design provisions for loading scenarios and anchor configurations not covered in EN 1992-4 (e.g., stand-off close to the edge of a concrete member)

Both for 1) and 2) Profis Engineering (PE) requires filling the gap between fastener and steel plate to guarantee that all fasteners are loaded equally.

PROFIS Engineering