New

Nuron SD 5000-22 Cordless drywall screwdriver
Nuron

ST 2000-22 Cordless metal screwdriver

Why Buy Nuron
Power around 90 tools with a single battery
More work-per-charge
Built-in battery diagnostics
New and improved safety features
Last charged location*

Looking for impact drivers?
For selected professionals, more torque and power may be what’s required for your day-to-day fastening jobs. Or it might be a working material that needs more oomph. We have a great selection of impact drivers with brushless motor on our dedicated page which also run on our Nuron battery platform for total toolpark convenience.

Why Nuron for cordless screwdriver options?
Some of the tools on this page run on our Nuron battery platform, so you can perform corded and petrol-powered applications on a single cordless platform. From breaking and cutting to drilling and fastening, Hilti cordless tools, including our cordless screwdrivers, are designed for maximum performance and improved user comfort. Tools on the Nuron battery platform offer electric screwdrivers without compromise thanks to longer-lasting Li-Ion batteries, time-saving accessories, and a range of services to keep you productive, today and tomorrow.

Cordless screwdriver tools for the jobs you’re on
Choose from tools that cater for drywall or metal that make getting the job done easier. In addition, with accessories such as collated ends to help you screw quicker and stand-up handles, you can benefit from tools that help you move and work faster on the job with precision.
*Fleet subscription and charger module required

Electric screwdriver vs impact driver differences
While the cordless screwdrivers mentioned here can tackle selected jobs and materials, professionals would typically use an impact driver when higher torque settings and power is needed. As these jobs are more challenging, the tools are usually heavier – which can increase fatigue when working with them for prolonged periods. Cordless screwdrivers are often used for tasks where you want to limit any potential damage to the surface material. These are recommended for less challenging tasks.

Electric screwdriver products for your trade
While the tools on this page cover various applications, they are also perfect across a range of trades. This includes drywall professionals and plasterers, roofing specialists, panel installers, general contractors and more. Always remember to use the right tools, accessories and fastenings for your material, as you may cause damage with an incorrect approach.
FAQs

What is the difference between an electric screwdriver and a drill driver?
While both can look and feel similar, the main difference is around the applications you can use them for.
An electric screwdriver, be it for drywall, metal or assembling furniture, is mainly designed for repetitive screwing tasks and isn’t recommended for drilling holes.
A drill driver, while its main purpose is centered around drilling holes can also be used for driving screws into hard materials.

Can an electric screwdriver drill holes?
While some dedicated electric screwdrivers may have the capability to drill holes, it is always recommended that you drill holes with a native drill driver or drill.
In addition, an electric screwdriver may not have the same torque or power compared to a regular drill driver for the material or job at hand.

What is the best electric screwdriver for furniture assembly?
While many items of flatpack furniture or at-home assembly items can be assembled by hand, an electric screwdriver can be handy.
So if you are looking at using an electric screwdriver to assemble furniture, we would recommend a lightweight tool that has enough torque to fasten screws as required.
However, while some users may opt to use a drill driver for screws, there is a risk of damage and/ or overtightening if you don’t use the correct settings on your drill.