Nuron

Nuron NCT 25 S-22 ACSR and guy wire cordless cable cutter
Nuron

NCT 45 S-22 ACSR and guy wire cordless cable cutter
Nuron

NCT 53 C-22 Copper/Aluminum cordless cable cutter
Nuron

NCT 85 C-22 Copper/Aluminum cordless cable cutter

Why Buy Nuron
Power around 90 tools with a single battery
More work-per-charge
Built-in battery diagnostics
New and improved safety features
Last charged location*

Why Nuron for hydraulic cable cutter products?
With Nuron, you can perform corded and petrol-powered applications on a single cordless platform. From breaking and cutting to drilling and fastening, Hilti tools, including our cordless hydraulic cutters, are designed for maximum performance and improved user comfort. Tools on the Nuron battery platform offer cutters without compromise thanks to longer-lasting batteries, time-saving accessories and a range of services to keep you productive, today and tomorrow.
And as a Hilti customer, you can also take advantage of tool inspection services, certification and our repair service to keep your products working effectively – which also adds further confidence to your customers and your reputation. This helps to minimise downtime and ensures productivity across all your projects on even the most challenging of tasks or jobsites.

Hydraulic cable cutting tools for a modern jobsite
Any trade professionals using hydraulic cable cutter products know that a good one is crucial to save time and effort on the jobsite. In addition, you’ll be fully aware that having a reliable hydraulic cutter ensures you can deliver a fully robust standard of work that is compliant and guarantees that the work is done well.
With certification and tool inspection options across our cordless cable cutter products, we are proud to offer cutting quality that you, and your customers, can rely on for the job at hand. While our additional services offer further advantages to owning a Hilti product, additional safety features on selected products such as electronic trigger lock, audio and visual prompts, offer an elevated level of protection to you and your workforce when using our hydraulic cutters.
Our hydraulic cable cutter products, sometimes known as battery cable cutter tools, also offer 350° head rotation to ensure better useability in tight or awkward spaces. In addition, our cutters also make one-handed operation easier when needed.
*Fleet subscription and charger module required
FAQs

What is a hydraulic cable cutter?
A hydraulic cable cutter, as the name suggests, uses hydraulic pressure to cut regular, thick and industrial-grade cables. The force these cutters generate can cut through copper and steel (including reinforced steel) with minimal effort.
Hydraulic cable cutters are used on tasks across several industries. You can usually find them being used for electrical and mains installations, major infrastructure projects, or frequently on jobs in the telecoms industry.

How does a hydraulic cable cutter work?
A hydraulic cable cutter uses hydraulic pressure to cut through the thickest and strongest cable. It works using an internal hydraulic pump which pressurises hydraulic oil, similar to that used in a car jack or power steering components, which in turn applies force to the cutting head/ blade to operate.
While most modern hydraulic cutters use battery power to operate, some require manual operation with a pump to increase pressure before use.

What maintenance do hydraulic cable cutters need?
While hydraulic cutters can have complex inner components, maintenance is relatively straightforward to ensure they work efficiently. Our recommended maintenance routine incudes:
Cleaning blades after use with a microfiber cloth, brush or compressed air
Visual inspection after use or periodically to check for excessive wear
If possible, checking hydraulic fluid levels through sight glass, LED indicators or opening up the unit by trained professionals
If you need to replace oil, do so using the correct oil to maintain recommended viscosity and purge air from the device
Scheduled servicing based on manufacturer guidelines