Get Hilti Discount CodesSave with our exclusive offers and promotionsView now
Top 5 Hilti tools for Christmas 2025

It’s almost Christmas and that means only one thing: Santa Claus will be bringing new tools down the chimneys of contractors and construction workers up and down the land! But what tools should be at the top of your wishlist this year?

Hilti’s top 5 tools of 2025 are a great place to start! These are our most popular and innovative new products that contractors keep coming back for time and again. Read on to learn more about the best tools you can ask for this Christmas…

TE 4-22 Rotary Hammer

Our TE 4-22 cordless rotary hammer offers our best performance-to-weight ratio for overhead drilling. It weighs just 2.45kg and operates at 1,050 RPM, delivering 5,100 impacts per minute. It’s compact but capable, offering 20% more power thanks to a brushless motor and the Nuron battery.

Other features include:

  • Enhanced comfort with a redesigned grip, LED light and better balance

  • Active Torque Control (ATC) to stop uncontrolled spinning if the bit sticks

  • Active Vibration Reduction (AVR) to make the tool less tiring to use, increasing productivity

  • Virtually dust-free drilling for additional safety.

It’s the perfect tool for drilling and hammer drilling into both concrete and masonry. It’s also ideal for overhead drilling where you need to install MEP, hang pipes and conduits, or set anchors into concrete – or perhaps even put Christmas lights up?

Learn more about the TE 4-22 cordless rotary hammer
SD 5000-22 drywall screwdriver

If Santa wanted to gift someone a useful tool, it doesn’t get much better than a market-leading cordless drywall screwdriver. The SD 5000 powered by our Nuron battery system, offering more torque and screws per charge when hanging drywall, sheathing or other boarding.

It’s compatible with your current Hilti magazine and accessories, and also offers the following benefits:

  • 10% more torque for faster screwdriving

  • In-line grip and improved LED light so you can work all day without discomfort

  • More rigid and durable belt hook

  • Cordless with long-lasting Nuron battery.

If you need to hang plasterboard, wood boards, metal studs, sheathing boards or anything else, the SD 5000 is the perfect electric screwdriver for you this Christmas.

Learn more about the Nuron SD 5000-22 cordless drywall screwdriver
SID 4-22 impact driver

If what you need is an impact driver rather than a rotational screwdriver, the SID 4-22 cordless impact driver is the tool for you this Christmas. It’s cordless and runs on the Nuron battery system for maximum manoueverability and ease, as well as offering the following features:

  • Just 134mm from front to back, making it ideal for working in tighter spaces

  • Four built-in LED lights so you always have a clear view of the work

  • Textured and contoured ergonomic grip which stays comforatable even at difficult angles

  • Re-engineered gearing, motor cooling and sealed electronics for enhanced durability

  • 1/4" hex click-in chuck for easier set up.

This impact driver is the perfect tool for smaller fastening jobs, drilling in wood with spade bits, driving self-drilling screws into metal, and driving wood screws through wood. If you’ve got some awkward jobs which are too small for a full-sized driver, the SID 4-22 is an outstanding option.

Learn more about the SID 4-22 cordless impact driver
SM 60-22 Mitre Saw

While you might not need a mitre saw for cutting a christmas tree down to size, it has plenty of other applications that you’ll be able to make use of. The SM 60-22 cordless mitre saw is the right choice for smooth compound cuts and accurate straight cuts all year round:

  • Six speeds (2000-4300 RPM) allow you to optimise cutting quality, performance and battery life

  • Forward-sliding rail and front-facing bevel adjustments

  • Integrated LED shadow queue for faster, more accurate working

  • Effective dust removal and fast blade break for improved safety.

If you need to cut wood, aluminium or PVC in 2026, why not ask Santa for a Hilti SM 60-22 cordless mitre saw for Christmas and get a head start for the new year!

Learn more about the SM 60-22 cordless mitre saw
AG 4S-22 Angle Grinder

Finally, the AG 4S-22 cordless angle grinder is a compact Christmas present that provides power and precision in a small, slimline package. It takes discs up to 125mm in diameter and can cut up to a depth of 34mm.

Features include:

  • The combination of brushless motor and Nuron battery provides 10% improvements to working time and cutting speed

  • Precise speed controls from 3400-7600 allow use for removing rough material and precise surface finishing with the same tool

  • Greater comfort thanks to a slimline, contoured handle

  • Lock-on switch offers improved control in most working positions

  • Active Torque Control (ATC) provides improved protection from kickback.

If you want to cut, grind, polish or deburr metal, concrete, masonry, stone or tiles in the new year, the AG 4S-22 cordless angle grinder is the ideal addition to your Christmas wish list!

Learn more about the AG 4S-22 cordless angle grinder
And if those aren’t what you want for Christmas...

There's plenty to more to see in Hilti's range of power tools. Contact us today for more information.

View our tool portfolio here