A concise overview of shear distribution principles of SOFA design

In the previous articles, we shed light on the details regarding SOFA’s design advantages for design engineers when filling the clearance gap. In summary:
- SOFA provides EN 1992-4 compliant design solutions with for anchor layouts beyond 3x3 rectangular layouts
- SOFA enables greater concrete edge breakout resistance by transferring shear loads to the back anchors.
In this article, we briefly illustrate how SOFA distributes shear loads with different anchor layouts to verify the concrete edge resistance:
- Rectangular layouts up to 3x3
- Rectangular layouts beyond 3x3
- Other layouts (irregular, circular, triangular)
Rectangular Anchor Layouts up to 3x3
The design approach of EN 1992-4 assumes shear loads are transferred to the front row when evaluating the resistance to concrete edge breakout, leading to conservative results. SOFA follows fib Bulletin 58’s design provisions that allow shear distribution to the back row.
PROFIS follows the shear distribution model represented in Figure 1 and checks every case individually. When designing fastenings in a thin base material, edge failure may occur at the back row, making it essential to check the edge breakout for each row. PROFIS Engineering then generates the design report with the most critical row.
Figure 1 – SOFA shear load distribution for anchor layouts up to 3x3
Rectangular Anchor Layouts beyond 3x3
Shear redistribution is not allowed whenever there are more than 3 rows of anchors in the baseplate. This is because it is not possible to assume a sufficient rigidity of the baseplate and the shear load will be allocated entirely at the front row following the EC 2-4 (Figure 2). For this reason, SOFA delivers a worse edge failure resistance with 4x2 than 3x2 when considering the same edge distance and base material parameters. Receiving higher utilization ratios with higher number of rows might give the impression that something is wrong with the design, however it is due to different evaluations for shear load distribution.
Figure 2 – Shear load allocation in case of 4x2 anchor layout
Other Layouts (Irregular, Circular, Triangular)
It is easy to determine the shear load distribution plane with rectangular layouts as we apply the loads to the front or back rows since this does not require much nuance. However, when designing with arbitrary configurations (irregular, circular, triangular etc.), determining the shear load transfer at the edge increases in complexity. In these configurations, anchors contributing to the edge breakout resistance are evaluated through the “bandwidth approach”.
This approach helps whenever two or more fasteners lie almost along the same row (e.g., small deviations in relation to the spacing between the anchors); thus, the closest anchor to the edge is not the only one being considered.
Figure 3(a) – second anchor falling in the band
Figure 3(b) – second anchor not falling in the band
The fasteners within the scope of this bandwidth are considered within the same stress plane as the front one, thus forming an artificial anchor row. Referring to the above Figure 3(a), another anchor intersects the bandwidth marked by the red box, therefore enabling the transfer of shear loads to a larger surface marked by the blue lines. For the scenario in Figure 3(b), the clear distance between two anchors is insufficient to consider two fasteners as a single row, hence full shear load is applied to the edge through one fastener.
In conclusion, concrete edge failure is often the governing failure mode for fastenings loaded in shear. SOFA’s shear distribution approach helps the structural engineer to activate a more accurate and efficient design approach than EN 1992-4 when designing rectangular anchor layouts up to 3x3 by: (1) distributing the loads to the back row; and (2) enabling the edge failure verification with other layouts by subjecting the full shear load to the front row.
You are also welcome to ask us for support: simply leave a comment or post your question in the community, or improve your knowledge and skills via our Webinars or training sessions.
For the latest news in engineering solutions and innovations follow us on: LinkedIn, Instagram and Twitter