The naming STOP defines the sequence of controlling risk. Here’s what that means in detail:
Substitution is the elimination of the risk by using safer alternatives. By doing so the root cause of hazards can be avoided.
E.g. for some applications we recommend diamond drilling or direct fastening where possible to minimise dust and HAVS exposure.
Technical measures are machinery, tools or technologies to reduce dust in the air, to minimize the dangerous effects of dust for people.
E.g. the Hilti Dust Removal Systems (DRS) and Active Vibration reduction (AVR) are practical harmonised systems designed to reduce risk. We’ve also introduced NFC tags in our tools which talk to the Hilti Connect App allowing operatives to access safety information and training videos as well as safe exposure information at the click of a button from wherever they’re working.
Organisational measures are made possible due to different working methods and improved work organisation.
E.g. Hilti ON!Track software allows users to manage employee certifications and offers quick and easily accessible Health & Safety information such as EAVs for employees on the job
Personal protective measures are needed where risks remain. The user is exposed to this risk and without these protective measures there can be health hazards! So, PPE – personal protective equipment – is required to cover the remaining risks. The technical measures used to reduce dust in no means make PPE option. This is something we take seriously for our own employees as well as our customers.