The Hilti HUS3-H 14 screw anchor is reusable up to 100 times in fresh concrete
This adjustable screw increases productivity through less drilling and fewer operations than with conventional anchors alongside three embedment depths for maximum design flexibility. Not only this, but the HUS3-H 14’s friend, the HUS3-H 10 screw anchor, is reusable up to 40 times in fresh concrete, with the whole system being covered by DiBt approval. What’s more, the HUS3 portfolio is now ETA approved for no hole cleaning required to set the anchor. This significantly increases the speed of the screw anchor installation and minimises the exposure of harmful dust to the worker.
Earlier this year we celebrated the HUS3’s 5th anniversary by breaking a record of setting as many HUS3 anchors as possible. Don’t believe us? Watch the Hilti GB team do their part >>>