Added to cart
Added to cart
Go to shopping cart

why should I care about dust?

dust reduction

Last week, we spoke to Saskia our Services Product Manager about the benefits of investing in occupational health & safety and this time, it’s all about what some HSE experts consider as the “new asbestos in the construction industry” because of its potentially hazardous consequences on health & safety – dust.

Depending on the processed base material, size of the dust particles, concentration in the air and the duration workers are exposed, dust can lead to severe health issues as well as loss of productivity and working comfort. In addition, dust does not just stay at the construction site. It can spread easily to other areas impacting people, nature and the environment.

Before we explore the consequences let’s examine some important background information about dust.

 

what is dust?

Dust consists of tiny solid particles, is highly dispersed, and easily circulated in the air. There is inhalable dust which can be trapped in the mouth or nose, less than 100 microns in size and is usually from wood dust, whereas respirable dust penetrates deep into the lungs, is less than 10 microns and is generated from silica. Then we have thoracic dust which gets trapped in the upper part of the airway and is from cotton fibres.

Let’s put that into perspective: the average human hair is about 60 microns thick!

Fine dust is invisible to the human eye and can only be seen if there is a lot of it in the air - clouds of dust as we say. Because of its small particle size, it can stay in the air for up to 12 days. Sometimes, when we don’t see dust, we might still smell it e.g. if a room smells “like concrete”, cement can be circulating in the air.

Fine dust particles are the most dangerous because they are small enough to get into the far reaches of the respiratory system, typically the alveoli where they interfere with oxygen, and potentially cause long-term damage. Over-exposure to respirable dust that contains silica can even cause cancer, silicosis and chronic obstructive pulmonary disease (COPD).

 

how does dust arise?

Dust is generated by abrasive treatment of materials like drilling, chiselling, sawing or grinding. But dust can also occur through circulation when it is blown up by wind, by transporting dusty materials or while mixing powdery material, e.g. when preparing cement.Depending on the material processed, different types of dust occur.

Here are two of the more dangerous types of dust relevant for the construction industry:

  1. Dust with crystalline structure: generated by abrasive treatment of material that contains silica e.g. sandstone, concrete, mortar or tile. It contains respirable crystalline silica (RCS)
  2. Dust with powder structure: occurs by abrasive treatment of wood and processed wood like medium-density fiberboard (MDF). And in the UK, hard wood is classed as carcinogenic in the EH40 regulations.

 

DUST IS EVERYWHERE ON THE CONSTRUCTION SITE

It’s a fact that dust is everywhere on a construction site. It occurs at nearly every point in the construction process during drilling, sawing, breaking, grinding and transportation. It is so ubiquitous that it’s often considered as normal and nothing to worry about. But that’s a false conclusion.

Some jobs create a huge amount of dust – for example slitting bricks and installing electrical cables can produce about 17 kg of dust an hour. Demolishing concrete ceilings for post-installation can produce about 6 kg of dust per hour.

Now add up all the work done on your construction site on a normal work day – that’s a worrying amount of dust your employees must be dealing with, right? So here comes the number one reason why you should care about dust.

 

Dust is created at nearly every point in the construction process including cutting concrete

DUST CAN HAVE HAZARDOUS CONSEQUENCES TO HEALTH & SAFETY

A shockingly high number of people die each year of lung cancer caused by over-exposure to respirable silica dust. Others suffer from dust-related diseases, like COPD, so badly that they can no longer work. So, dust can have severe consequences to your workforce and the company’s finances if not tackled head-on. Several national and international organisations have realised the urgency of the issues and launched initiatives and campaigns to combat dust at the workplace.

As an employer, there’s a responsibility to monitor your workers’ health & safety on the construction site. It’s generally regulated by law but considering the consequences to individuals and their families it should be in your interest to protect your employees the best you can.

 

What are the consequences?

When the human body inhales dust, natural defence mechanisms kick in e.g. sneezing, coughing. But those human defence mechanisms are limited and for some kinds of dust, ineffective. Special care must be taken when working with materials containing silica.

Silica is a natural material. About 27% of our earth crust is covered with it. It occurs in many materials common on constructions sites like sandstone, concrete, mortar, tile, brick and more.

When processing these materials, fine dust that contains respirable crystalline silica (RCS) occurs. Over-exposure to these RSC particles can be very dangerous because they reach deep into our lungs and settle in our lungs’ air sacks (alveoli). Over time scar tissue is produced and reduces the ability to breath-in oxygen. This incurable disease is called silicosis. 

 

can breathing in silica dust cause permanent damage to the lungs?

silica dust

Dust not only affects the lungs – it can also lead to other issues like eye and skin irritation or allergic reactions. Most of these afflictions will take a longer time to develop but with high exposure to dangerous dust it can also develop quite fast and can raise drastic problems like:

·         Reducing ability to work

·         Reducing quality of life

·         Permanently damaging health

Protecting your workforce from dust will significantly impact your employees’ health & quality of life.

Understandably, most people would prefer to work in a clean environment where body, clothes and surroundings stay clean however this can have a broader impact construction industry. As long as it continues to have a reputation for dusty, dirty working conditions there’s a risk that prospective workers may not consider the sector, which is especially troubling at a time when there’s an industry wide skills shortage.

Working in clouds of dust also increases the risk of injuries due to reduced visibility and it can distract employees because of eye irritations, sneezing, coughing or nose blowing. But that’s not the only reason to take control of dust. You can significantly increase productivity and lower maintenance costs with appropriate measures against dust by:

·         Reducing preparation time: no or minimal time sealing off the area required before work starts

·         Reducing cleaning: depending on the application you can save up to 99% of cleaning time

·         Reducing damage of fixtures and fittings: like carpets, furniture and other furnishings

·         Increasing lifetime of tools: by up to 60% and of inserts by up to 20%

·         Increasing application speed: up to 20% with cleaner and sharper tools

It’s a given that dust is a topic the construction industry must address. If you want to find out more read our other artciles in the series.

 

technology and products

Technology and products

Designed with productivity, safety and the environment in mind.

Find out more
Services

Services

Increasing user health, safety and productivity.

Learn more
Our commitment to HSE

Our Commitment

See how Health, Safety and the Environment is embedded in our culture and purpose to build a better future.

Find out more

Share

We continue to support your business with free online delivery Read our COVID-19 update

CONTACT US
CONTACT US